Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Multiple Linear Regulators in a Circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 339 subscribers
  • Views 942 views
  • Users 0 members are here
  • linear regulators
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Multiple Linear Regulators in a Circuit

jeffrichley@gmail.com
jeffrichley@gmail.com over 10 years ago

I have a 24V power supply coming into my circuit and I need a 12V for a fan and 5V to run my logic.  I have 12V and 5V linear regulators that I can use to get the desired voltages.  Would it be better to run the 24V to both or the 24V to 12V and then take the 12V to the 5V?  My reasoning for the 24V -> 12V -> 5V is that the 5V would need to dissipate less power (7V vs 19V), but I didn't know if it is a bad idea to have one regulator pull from another.

 

I appreciate any input you have,

 

Jeff

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    If its just light electronics on the 5v rail, I'd just look at a different power source to provide 12v and use the linear regulator to step that down to 5v. Im not a fan of driving heavy loads like motors for long periods of time with linear regulators, it is possible but the more power you dissipate, the larger the heatsink has to be to stop it overheating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    If its just light electronics on the 5v rail, I'd just look at a different power source to provide 12v and use the linear regulator to step that down to 5v. Im not a fan of driving heavy loads like motors for long periods of time with linear regulators, it is possible but the more power you dissipate, the larger the heatsink has to be to stop it overheating.