Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Identifying parallel circuits
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 318 subscribers
  • Views 1840 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Identifying parallel circuits

salesm21
salesm21 over 9 years ago

To anyone out there,

I have a circuit for my class and am stumped on the identification of it. I cant figure out weather or not the bottom branches are in parallel or in series. Any thoughts? Any tips or tricks? I know what parallel means but I don't understand the wire that's in-between the resistors and the capacitors. Since the capacitor branch does not end at the same spot as the other capacitor does this mean its not in parallel?

 

 

 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • urkraft
    urkraft over 9 years ago +1
    R2 and R3 are in parallel and are equivalent to 720ohm, and C2 is in parallel with C3 and are equivalent to 2.2nF. This results in a circuit composed of R1 and C1 in series with the 2.2nF capacitor and…
  • urkraft
    urkraft over 9 years ago in reply to urkraft +1
    Opps, i see that i managed to submit a typo: the equivalent capacitance for the two parallel capacitors is 3.2nF, not 2.2 as i managed to write just now.
  • urkraft
    urkraft over 9 years ago in reply to salesm21 +1
    First off, you should always use a bit of logic to validate your answers. The equivalent resistance of two resistors in parallel will always be smaller than the smallest of the two resistors, and the equivalent…
Parents
  • urkraft
    urkraft over 9 years ago

    R2 and R3 are in parallel and are equivalent to 720ohm, and C2 is in parallel with C3 and are equivalent to 2.2nF. This results in a circuit composed of R1 and C1 in series with the 2.2nF capacitor and the 720 ohm resistor, which can also be reduced to one resistor and one capacitor - i leave it up to you to calculate the equivalent resistance and capacitor of the final circuit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • salesm21
    salesm21 over 9 years ago in reply to urkraft

    Raymond,

    When I try to calculate the Parallel resistance I get a weird number. The formula I use it R1R2/R1+R2. This gives me 3600Ohms which does not go with the convention that any resistors in parallel will have an Rtot that is less the smallest resistor. Also if I do the standard formula of 1/1/1.2Kohm+1/1.8Kohm I get 1800 ohms. What formula did you use to get to this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gihu
    gihu over 9 years ago in reply to salesm21

    For the equivalent resistor I agree with Raimond 720 ohm. For the equivalent capacitor I calculate 3.2nF

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gihu
    gihu over 9 years ago in reply to salesm21

    R = (1200*1800) / (1200+1800) = 2160000 / 3000 = 720

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • urkraft
    urkraft over 9 years ago in reply to salesm21

    First off, you should always use a bit of logic to validate your answers. The equivalent resistance of two resistors in parallel will always be smaller than the smallest of the two resistors, and the equivalent capacitance of two capacitors in parallel will always be greater than the largest of the two. Hope you see the logic in that. The formula you used to calculate the resistances is correct. It is equivalent to (1200 x 1800) / (1200 + 1800) = 2160000/3000 =2160/3 = 720 ohm.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • urkraft
    urkraft over 9 years ago in reply to salesm21

    First off, you should always use a bit of logic to validate your answers. The equivalent resistance of two resistors in parallel will always be smaller than the smallest of the two resistors, and the equivalent capacitance of two capacitors in parallel will always be greater than the largest of the two. Hope you see the logic in that. The formula you used to calculate the resistances is correct. It is equivalent to (1200 x 1800) / (1200 + 1800) = 2160000/3000 =2160/3 = 720 ohm.