Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need advice on Clamp Wattmeters
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 339 subscribers
  • Views 822 views
  • Users 0 members are here
  • digital multimeter
  • wattmeter
  • clamp meter
  • power meter
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need advice on Clamp Wattmeters

mudz
mudz over 9 years ago

Hi members image
I am looking for inexpensive handheld (maybe clamp) meter which can measure power factor, Power KW or HP equipment & other basic things voltage, ampere, frequency. I'm working with 3 phase motors and power so I need an equipment for the same. I cannot go beyond 250$ I know its low but I wish to know if anything is near that range?
Thank you

 

mudz

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2
    Hi Mudz, I do not believe that a Clamp Wattmeter is available. One needs potential and current to derive wattage. While the clamp meter will give you current if calibrated for a particular system it can…
Parents
  • rmwaseem
    rmwaseem over 9 years ago

    Dear Mudz

    I think you need a specialty meter we use in HVAC field which to some extent will satisfy all your requirements and still being a clamp meter it has all bells and whistle you need. Its called

    Amprobe  ACD-45PQACD-45PQ 600A Power Quality Clamp Meter with True-RMS and can be purchased through Amazon as well Here is the link https://www.amazon.com/Amprobe-ACD-45PQ-Power-Quality-True-RMS/dp/B005409S4K  and it costs around 181..$ which may fit your budget !

     

    • Digital clamp meter measures alternating current (AC) to 600 amp, direct current (DC) voltage and AC voltage to 600 volts (V), resistance to 1,000 ohms, and frequency to 500 hertz (Hz)
    • True RMS (root mean square) sensing meter provides accurate readings when measuring linear or non-linear loads, where the current or voltage has a sinusoidal or nonsinusoidal waveform
    • Transformer clamp with 1" (26 mm) jaw opening measures current without touching or interrupting the circuit
    • Measures real power, reactive power, apparent power, power factor, and kilowatt hour (kWHr) usage of single- or three-phase balanced or unbalanced power sources <--------image
    • Meets International Electrotechnical Commission (IEC) safety standard 61010 and is certified for category III installations up to 600V
    • Measurements: AC/DC Voltage up to 600V, AC current up to 600A, resistance, frequency power
    • 3 phase unbalanced load measurement - calculation of the discrete single phase measurements

     

    • Auto VA - auto selection of AC volts, DC volts or AC amps
    • Ultra slim jaws accommodate conductors up to 1.02 (26mm) in diameter
    • Optional PC interface capability (RS-232 KIT2)
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rmwaseem
    rmwaseem over 9 years ago

    Dear Mudz

    I think you need a specialty meter we use in HVAC field which to some extent will satisfy all your requirements and still being a clamp meter it has all bells and whistle you need. Its called

    Amprobe  ACD-45PQACD-45PQ 600A Power Quality Clamp Meter with True-RMS and can be purchased through Amazon as well Here is the link https://www.amazon.com/Amprobe-ACD-45PQ-Power-Quality-True-RMS/dp/B005409S4K  and it costs around 181..$ which may fit your budget !

     

    • Digital clamp meter measures alternating current (AC) to 600 amp, direct current (DC) voltage and AC voltage to 600 volts (V), resistance to 1,000 ohms, and frequency to 500 hertz (Hz)
    • True RMS (root mean square) sensing meter provides accurate readings when measuring linear or non-linear loads, where the current or voltage has a sinusoidal or nonsinusoidal waveform
    • Transformer clamp with 1" (26 mm) jaw opening measures current without touching or interrupting the circuit
    • Measures real power, reactive power, apparent power, power factor, and kilowatt hour (kWHr) usage of single- or three-phase balanced or unbalanced power sources <--------image
    • Meets International Electrotechnical Commission (IEC) safety standard 61010 and is certified for category III installations up to 600V
    • Measurements: AC/DC Voltage up to 600V, AC current up to 600A, resistance, frequency power
    • 3 phase unbalanced load measurement - calculation of the discrete single phase measurements

     

    • Auto VA - auto selection of AC volts, DC volts or AC amps
    • Ultra slim jaws accommodate conductors up to 1.02 (26mm) in diameter
    • Optional PC interface capability (RS-232 KIT2)