Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Electrical "Dead Man" Switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 321 subscribers
  • Views 1981 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Electrical "Dead Man" Switch

swankybarbecue4
swankybarbecue4 over 8 years ago

This is my circuit:

image

The voltage output from the TSOP1738 IR receiver fluctuates since it is an analog sensor; therefore, the output voltage of the 555 timer fluctuates. I want to use the output of the 555 timer to trigger a junction transistor that would then trigger a relay (the BJT is used because the relay i want to activate requires more current then the 555 timer can output). The relay would then close a circuit with a much high current.

 

My question is: Is there a circuit that exists that would pull the gate of the transistor or (if it is more efficient to remove the BJT from the equation) trigger the relay with a constant voltage and current once it detects any sort of output form the 555 timer? I would like the circuit to keep the gate of the BJT/relay high forever (this dead man circuit would pull from an external power supply obviously) once the tiniest indication of output was detected form the output of the 555 timer circuit shown above.

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +1
    If you disconnect pin 7, then a pushbutton switch from pin 6 to ground can be used to reset the internal flip-flop. It is then ready to be triggered by your sensor on pin 2. Once triggered it will stay…
Parents
  • dougw
    dougw over 8 years ago

    If you disconnect pin 7, then a pushbutton switch from pin 6 to ground can be used to reset the internal flip-flop.

    It is then ready to be triggered by your sensor on pin 2. Once triggered it will stay latched until the reset switch is pushed. The output can drive a FET or BJT if higher current is needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • swankybarbecue4
    swankybarbecue4 over 8 years ago in reply to dougw

    Sweet lord you are a genius!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • swankybarbecue4
    swankybarbecue4 over 8 years ago in reply to dougw

    Sweet lord you are a genius!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data