Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Wall Receptacle USB Charging - Switched Transformer?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 339 subscribers
  • Views 4200 views
  • Users 0 members are here
  • usb charging
  • usb power
  • receptacle
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Wall Receptacle USB Charging - Switched Transformer?

phumphries
phumphries over 8 years ago

Hi, all.

 

I was intrigued by these new receptacles with USB C charging ports, but, like every other one that I have seen, there is no information on how much current the unit draws when idle.  Ideally, the USB ports would be dead when nothing is inserted in them, but I am sure that a feature like that would be boldly trumpeted in the description. image

 

So, two questions, really:

 

  1. How much electricity is one of these units using when idle with nothing at all plugged into it?
  2. Has anyone ever seen a North American plug like this with a power switch?  (Plugs with integrated switches are pretty standard in the Middle East and parts of Europe.)

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +3
    Personally I like to see the input power switched off on all these devices. They are a switched mode supply and the components have a limited life span (usually a few thousand hours). Mark
  • mcb1
    mcb1 over 8 years ago in reply to phumphries +2
    but I can rewire it so that the USB gets its power from the switched circuit instead of the live wires? Yes although doing that for every single outlet adds time if it is more than just a simple pull-and…
  • shabaz
    shabaz over 8 years ago in reply to mcb1 +2
    Also depending on requirements that cheaper option could be a better option too, since it allows for fast-charge. It is unlikely that the in-wall versions support fast-charge methods for phones, i.e. mobile…
Parents
  • mcb1
    mcb1 over 8 years ago

    Personally I like to see the input power switched off on all these devices.

    They are a switched mode supply and the components have a limited life span (usually a few thousand hours).

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • phumphries
    phumphries over 8 years ago in reply to mcb1

    I guess that I could buy the switch / 2 USB version and wire the power to the USB ports through the switch. image

     

    In addition to my concern about the power draw, your point about wearing out the power supplies is also a significant consideration.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phumphries
    phumphries over 8 years ago in reply to mcb1

    I guess that I could buy the switch / 2 USB version and wire the power to the USB ports through the switch. image

     

    In addition to my concern about the power draw, your point about wearing out the power supplies is also a significant consideration.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 8 years ago in reply to phumphries

    I guess that I could buy the switch / 2 USB version and wire the power to the USB ports through the switch

    That is one idea, but without looking at how they have connected them, it might be the whole socket that gets swtiched.

     

    Here in NZ we have PDL/Schneider making one that can be fitted into a socket outlet.

     

    I note that they do specify the standby load (0.07w) and is able to be wired rather than be part of the sockets.

    http://www.pdlglobal.com/data/product_documents/600%20&%20800%20USB%20Charger%20Flyer.pdf

     

    They can be added to outlets that have an extra switch, or you could fit them to a switch plate without the socket.

      or imageimage

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phumphries
    phumphries over 8 years ago in reply to mcb1

    Nice products!  In the suggested configurations, they do not show a USB port with a switch.  Do you know if that can actually be configured?

     

    It seems funny to me that someone would not just make a port that connects power to the transformer when a cable end is pushed into it.  At least PDL / Schneider is up front about the stand-by draw.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to phumphries

    phumphries

    they do not show a USB port with a switch.  Do you know if that can actually be configured?

    You're quite right

    I forgot to link this which shows some suggested connections

    http://www.pdlglobal.com/data/product_documents/642M%20install%20sheet%200414%20v7.pdf

     

    The switch is connected internally to the phase of the socket, BUT having pulled one apart, they are very easy to modify.

    You simply remove the cover and add a wire, which switches off the USB with the socket.

     

     

    If you don't need/want the socket, you can use their switch range.

    PDL : Products, Domestic, 600 Series, Switches, Standard Switches

    Each switch is a unit and come is 2 - 6 apertures.

     

     

    I'm tempted to add one to where we charge our phones ...

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phumphries
    phumphries over 8 years ago in reply to mcb1

    I want something with at least one regular outlet for plugging in any AC equipment and at least one USB outlet for charging.

     

    Are you saying that the 694USB (from the configurations page in the catalogue) comes wired so that the USB ports are live all the time whilst the AC outlet is switched, but I can rewire it so that the USB gets its power from the switched circuit instead of the live wires?

     

    I do not mind a little rewiring work, although doing that for every single outlet adds time if it is more than just a simple pull-and-push move.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to phumphries

    but I can rewire it so that the USB gets its power from the switched circuit instead of the live wires?

    Yes

     

    although doing that for every single outlet adds time if it is more than just a simple pull-and-push move.

    So either put up with 0.07w power wastage, or talk with your local manufacturer of outlets and ask why they aren't doing it.

     

     

    Besides how many charging outlets are you going to do.?

    The other option (and cheaper) is simply a charger plugged into one of the two switched sockets .....

     

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    Also depending on requirements that cheaper option could be a better option too, since it allows for fast-charge. It is unlikely that the in-wall versions support fast-charge methods for phones, i.e. mobile phones will take longer to charge.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to shabaz

    since it allows for fast-charge

    definately as they say it's only a 1.2A outlet.

     

    Interestingly, some larger tablets and transformable laptops use a normal looking charger, but it bumps the voltage up when it detects the device.

    My daughter found out the hard way when she took the wrong charger ... on trip to Japan.image

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 8 years ago in reply to mcb1

    I was about to buy one here in UK, to replace an existing twin outlet which is faulty. I need to investigate whether the USB charging outlet is switched off with no cable inserted.

     

    Thanks for the heads-up on the expected lifetime of switched mode power supply components.

     

    Neil

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phumphries
    phumphries over 8 years ago in reply to mcb1

    Whilst plugging in a "wall wart" is always an option, adding USB to existing single-gang boxes seems to me like a nice upgrade.  True, it might not have the latest and greatest USB charging features, but it will be convenient for occasional use and have an integrated look, especially where the receptacle is located conveniently (not hidden behind a chair, for example).

     

    If the AC / DC components were automatically disconnected when not in use, I would put these everywhere that someone might sit down with a mobile device; so, there would be a lot of them in a typical North American house.  Some people (like my 16-year-old son) are still okay with leaving an adaptor plugged in when not in use, but many people are aware, now, that transformers use power even when "idle," which is why it strikes me as odd that manufacturers would add DC to AC receptacles without a switch, manual or automatic.

     

    As a sort of interim solution, I have added a switch to nice-looking power bars with integrated USB ports so that the transformer for the USB ports can be turned on only when needed.  By the time that I did the sixth one, it looked like the switch belonged. image