Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Electronics Novice
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 314 subscribers
  • Views 1037 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Electronics Novice

gjfield
gjfield over 7 years ago

Hello, I am trying to help a student who would like to build a LASER Harp, which sounds pretty inspiring. I know very little about LASER Diodes, but some of the components listed here seem to be able to detect signal in addition to transmit. Has anyone worked with these gadgets before - is it just a case of configuring the device differently for detection versus emission? (Data sheet suggest so, but I am not sure) - Also, 1.1mW sounds approximately Class II, so I am guessing moderately safe? Any advice gratefully received

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +5
    You would need one light sensor such as a photo diode or a photo transistor for each string. You could also have a laser emitter for each string, but if each sensor is just focused on a small area, the…
  • michaelkellett
    michaelkellett over 7 years ago +3
    If you mean this sort of thing: https://www.kromalaser.com/laser-harp Then wait until you are not a novice !!! (No idea how the audience and guy playing it are protected - looks risky to me - we wouldn…
  • beacon_dave
    beacon_dave over 7 years ago +2
    These two 'The Ben Heck Show' episodes may be of interest: Episode 253: Ben Heck’s Intel Edison Laser Harp Part 1: Design Episode Episode 254: Ben Heck’s Intel Edison Laser Harp Part 2: Assembly Episo…
Parents
  • dougw
    dougw over 7 years ago

    You would need one light sensor such as a photo diode or a photo transistor for each string.

    You could also have a laser emitter for each string, but if each sensor is just focused on a small area, the whole line of stings can have the same light source. You can make the sensor only see a small area by putting a long thin black tube in front of it. If the tube has a 1 mm inner diameter and is 100 mm long, the spot it sees 300 mm from the tube opening is only 3 mm.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago

    You would need one light sensor such as a photo diode or a photo transistor for each string.

    You could also have a laser emitter for each string, but if each sensor is just focused on a small area, the whole line of stings can have the same light source. You can make the sensor only see a small area by putting a long thin black tube in front of it. If the tube has a 1 mm inner diameter and is 100 mm long, the spot it sees 300 mm from the tube opening is only 3 mm.

    • Cancel
    • Vote Up +5 Vote Down