Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Electronics Novice
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 314 subscribers
  • Views 1034 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Electronics Novice

gjfield
gjfield over 7 years ago

Hello, I am trying to help a student who would like to build a LASER Harp, which sounds pretty inspiring. I know very little about LASER Diodes, but some of the components listed here seem to be able to detect signal in addition to transmit. Has anyone worked with these gadgets before - is it just a case of configuring the device differently for detection versus emission? (Data sheet suggest so, but I am not sure) - Also, 1.1mW sounds approximately Class II, so I am guessing moderately safe? Any advice gratefully received

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +5
    You would need one light sensor such as a photo diode or a photo transistor for each string. You could also have a laser emitter for each string, but if each sensor is just focused on a small area, the…
  • michaelkellett
    michaelkellett over 7 years ago +3
    If you mean this sort of thing: https://www.kromalaser.com/laser-harp Then wait until you are not a novice !!! (No idea how the audience and guy playing it are protected - looks risky to me - we wouldn…
  • beacon_dave
    beacon_dave over 7 years ago +2
    These two 'The Ben Heck Show' episodes may be of interest: Episode 253: Ben Heck’s Intel Edison Laser Harp Part 1: Design Episode Episode 254: Ben Heck’s Intel Edison Laser Harp Part 2: Assembly Episo…
  • dougw
    dougw over 7 years ago

    You would need one light sensor such as a photo diode or a photo transistor for each string.

    You could also have a laser emitter for each string, but if each sensor is just focused on a small area, the whole line of stings can have the same light source. You can make the sensor only see a small area by putting a long thin black tube in front of it. If the tube has a 1 mm inner diameter and is 100 mm long, the spot it sees 300 mm from the tube opening is only 3 mm.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago

    If you mean this sort of thing:

     

    https://www.kromalaser.com/laser-harp

     

    Then wait until you are not a novice !!!

     

    (No idea how the audience and guy playing it are protected - looks risky to me - we wouldn't be allowed to do this in an office or factory !)

     

    1W + lasers - please do not go there without actual training.

     

    If you want to make a miniature home use device you could use LEDs but the hard stuff will be in the optics.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago

    These two 'The Ben Heck Show' episodes may be of interest:

    Episode 253: Ben Heck’s Intel Edison Laser Harp Part 1: Design Episode

    Episode 254: Ben Heck’s Intel Edison Laser Harp Part 2: Assembly Episode

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to beacon_dave

    Also this one may be of some interest:

    LASER HARP

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago in reply to beacon_dave

    This one is based on a 375mW laser:

     

    From Wikipedia:

     

    Class IIIb

    Lasers in this class may cause damage if the beam enters the eye directly. This generally applies to lasers powered from 5–500 mW. Lasers in this category can cause permanent eye damage with exposures of 1/100th of a second or more depending on the strength of the laser. A diffuse reflection is generally not hazardous but specular reflections

    can be just as dangerous as direct exposures. Protective eyewear is recommended when direct beam viewing of Class IIIb lasers may occur. Lasers at the high power end of this class may also present a fire hazard and can lightly burn skin.

     

    If you play with matches .........

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to michaelkellett

    I seem to recall that local Trading Standards found a number of cheap import laser pointers on the market were outputting far in excess of their claimed class I or class II ratings.

     

    Also I recall that sometimes the class rating takes into account the protective enclosure, so if you remove the laser diode from its original product housing then the rating can change.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi,

     

    There are safer non-laser methods, maybe using a camera perhaps.

    If you're happy with a software solution, there is Leap Motion, that might work for this use-case. It is very responsive (several hundred frames per second) because it is intended for gaming, and provides a value in millimetres of where your hand or fingers are, in 3 dimensions.

    Some info here: Virtual Reality, Leap Motion, and Controlling Things! - Getting Started Guide

    Or if you want it to be a hardware project, then experimentation with LEDs and lenses could help, although it gets expensive fast, when it comes to optics : (

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to beacon_dave

    Cornell ECE4760 student project

    https://youtu.be/kHuugv6sa_U

     

    More info at:

    Laser Harp