Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Five robot from DIY to NASA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 3 Jun 2019 8:34 PM Date Created
  • Views 1310 views
  • Likes 8 likes
  • Comments 4 comments
  • industrial
  • mit
  • hmi
  • robotics
  • work
  • robot
  • nasa
  • on_campus
  • diy
  • cabeatwell
  • caltech
  • university
Related
Recommended

Five robot from DIY to NASA

Catwell
Catwell
3 Jun 2019

Doggo, a robot that can do acrobatics comes at an affordable price

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Doggo can walk, trot, do backflips and even jump with ease and can prop itself back up if it loses its balance. (Image Credit: Stanford University)

 

Stanford's Extreme Mobility team has developed a four-legged robot that's capable of acrobatics, like backflips and can trot, dance, hop, jump up to 3.5 feet and even walk on rough terrain. The Stanford Doggo is available to anyone who can consult about comprehensive plans, code and supply list, all of which is online. Doggo's price is estimated at less than $3,000, including shipping/manufacturing costs. Students who developed Doggo built it with replicability in mind by using supplies that were easy to obtain and by testing each part as they were created. Doggo had trouble with maneuverability at first, but after some tweaks and experimenting, Doggo can maintain a consistent gait and desired trajectory.  This is achieved with motors that detect if there is external force on the robot. It then determines the amount of force and torque that would be applied. The motors are speedy too, computing at 8,000 times a second and act similar to springs, setting Doggo in the correct position.  Extreme Mobility is also teaming up with the Robotic Exploration Lab of Zachary Manchester to run control-based experiments. The team has also developed  Stanford Woofer, which can carry up to 6kg of equipment and is twice the size of Doggo.


Bee+, a robot-like insect that flies

image

Bee+, a robot-like insect, has improved flight precision and control over actual insects. (Image Credit: Yang et. al./University of Southern California)

 

Researchers from the University of Southern California in Los Angeles developed a four-winged robot called Bee+, weighing at just 95 milligrams, the robot has the same flight agility and poise of actual insects. This was done by replacing older biomorph actuators, cantilevers constructed from two layers of piezoelectric material with a passive layer between the two, with unimorphs that contain one piezoelectric layer. All four actuators, when combined together, weigh half the size of the biomorphs at just 56 milligrams, making it lighter on the wings and improving flight control. Bee+ has the ability to avoid obstacles, perch, land and can even follow flight paths. It's also much easier to build than the previous RoboBee model, which only has two wings. The robotic insect doesn't run on batteries, but instead, it has a tether attached to its body. However, the robot's size is larger and heavier than most insects, even if it is a bit larger than a penny. Other tiny robots could benefit from the small size, making the size of Bee+ useful for different tasks like scouting areas that may have hazards and finding survivors in a disaster area, such as collapsed buildings. One of the bigger challenges with designing small robots is allowing it to carry a full payload as it fits in tight spaces.

 

 

RoboRaise could be a handy robot when lifting heavy objects

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The robotic arm mimicks muscle movement by moving up and down as the human arm does. (Image Credit: MIT CSAIL)

 

Researchers from MIT's Computer Science and Artificial Intelligence Laboratory (CSAIL) have developed a robot known as RoboRaise that helps humans lift objects by observing their muscle movements.   Using brain signals and hand gesture, the robot uses electromyography (EMG) sensors on humans biceps and triceps to monitor their muscular activity. RoboRaise then identifies the height of their arm, and from there, the robot can follow their movements as they raise and lower their arm. The system underwent experimentation by lifting and putting down mock airplane parts, with a 70% accuracy rate when responding to gestures. The approach used for humans lifting objects with robots is meant to be intuitive and similar to how one would lift objects with another person. They key to doing this is through arm movements that set instructions on how the robotic arm would lift higher or lower. Using muscle movement and signals to communicate makes the robotic arm seem like it's being controlled by the user. The team plans on installing additional sensors or reading more muscle groups in the future to improve RoboRasie's ability to carry out complex tasks. RoboRaise could be used on construction sites, manufacturing, or even as a helpful hand around the house when lifting furniture.


Spidey-sense sensorsin vehicles can prevent dangers

image

Spidey sense on the sensors could be beneficial for autonomous vehicles. (Image Credit: Taylor Gallery)

 

A team of researchers from Purdue University, Nanyang Technological University in Singapore and ETH Zurich have proposed installing sensors into autonomous machines. They would be akin to spider sense, allowing vehicles to process data faster than possible. The aim is to cut down on data load by mimicking the way spiders process information, so researchers will be developing a sensor that can achieve this feat. For example, the hairs on a spider will vibrate at a certain frequency, activating the mechanosensors whenever prey lands on its web. However, the mechanosensors don't have a reaction to the frequency whenever it senses dust has fallen onto its web. The team is designing their sensors in a way where they could either act as mechanosensors or a mechanoreceptor, the same way spider do when they switch between sensing and responding. Their sensors work by changing shape when triggered by an external force that fits a predetermined threshold. Conductive particles will be able to move together more closely due to the shape's change, allowing electricity to pass through it to create and send a signal. This lets the autonomous system know how it should react. The sensors can sense and filter things out quickly and can also compute without using a power supply. These type of sensors could help drones explore dangerous areas, and autonomous vehicles avoid danger on the road.

 

NASA's Bumble completes first hardware checkout aboard the International Space Station

image

Anne McClain performs tests on Bumble during a mission aboard the International Space Station. (Image Credit: NASA)

Robots may soon be helping take care of spacecraft. NASA's Astrobee robot, named Bumble completed its first series of tasks aboard the International Space Station during a hardware checkout. Bumble first launched to the spacecraft with Honey, another robot on April 17th aboard Northrop Grumman's eleventh commercial resupply services mission from NASA's Wallops Flight Facility in Virginia. The robots can return to Kibo, their docking station on their own to recharge when needed. Astrobee is a robot system that allows robots to float on their own and will offer a research platform for the laboratory. The system involves three robots with a docking station to recharge. Robots will aid in NASA's mission to return to the moon, along with deep space missions. Tasks will include tending to astronauts, and Astrobee's robots will be tested on how they can assist crew members. This will enable astronauts to improve their productivity and will help look after spacecraft when astronauts are not available near the Moon, Mars or other outposts in space.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • danielw
    danielw over 7 years ago +1
    Good selection of robots here! Doggo is awesome, I've found the project and the motor controller! Robo raise... The sensing technology looks great, and assistive technologies would go a long way to helping…
  • dubbie
    dubbie over 7 years ago +1
    Cabe, I was fascinated by the Doggo robot. I have not seen that type of leg before and it was very interesting. I might even try a simpler version of this leg myself, sometime, maybe. Dubbie
  • danielw
    danielw over 7 years ago in reply to dubbie +1
    Dubbie, If you do, I'll be reading. I've still got that xpider (Tobbie like) robot on my list of things to build! I've very nearly finished the mods to my 3D printer! Dan.
Parents
  • dubbie
    dubbie over 7 years ago

    Cabe,

     

    I was fascinated by the Doggo robot. I have not seen that type of leg before and it was very interesting. I might even try a simpler version of this leg myself, sometime, maybe.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago

    Cabe,

     

    I was fascinated by the Doggo robot. I have not seen that type of leg before and it was very interesting. I might even try a simpler version of this leg myself, sometime, maybe.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • danielw
    danielw over 7 years ago in reply to dubbie

    Dubbie,

    If you do, I'll be reading.  I've still got that xpider (Tobbie like) robot on my list of things to build!

    I've very nearly finished the mods to my 3D printer!

    Dan.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to danielw

    Daniel,

     

    I've still got my Tobbie sitting on my desk with it's controller removed. I had put together a protoboard controller which worked and I was transferring that to strip board - which didn't work. After several weeks, months(?) I eventually discovered that I had connected drive signals to one channel of the dual DC motor driver and the actual motor to the other! So I couldn't find anything wrong with the connections but it just didn't work. I even purchased several more dual DC motor H bridge driver PCBs to see if that was the problem. Still, I have discovered that problem now so hopefully I will be able to progress although I might need a new stripboard implementation as I have made a complete mess of the original by de-soldering and re-soldering wires and components. Still,  have finished by Picasso Design Challenge HoloPiBot now and I'm not involved in any other Element14 projects so I might take some time to progress some of my other robots.

     

    Dubbie