Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Rapid Iron-On dispenser eases the pain of creating smart clothing
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 25 Feb 2020 7:32 PM Date Created
  • Views 1455 views
  • Likes 4 likes
  • Comments 1 comment
  • clothing
  • hmi
  • manufacturing
  • diy
  • Wearable
  • embedded
  • cabeatwell
  • machine
  • Wearables
Related
Recommended

Rapid Iron-On dispenser eases the pain of creating smart clothing

Catwell
Catwell
25 Feb 2020

image

Built using 3D printed parts, the handheld dispenser is easy to use (Image credit: Interactive Media Lab)

 

There are plenty of smart devices and wearables to choose from these days, but when it comes to smart clothing, the options are still limited. They’re either in the planning stages or restricted to certain markets. Though there are machines that use rigid yarns to incorporate digital functionalities into textiles, they’re not widely accessible by makers and designers. A team of scientists hopes to make the process less painful with their new prototype known as the Rapid Iron-On (RIO).

 

The RIO is a handheld dispenser that allows you to apply different functional tapes of various lengths and patches to most textiles and fabrics. Using the device, you can map out complex circuits, custom-shaped I/O modules, and commodity textile surfaces using a variety of continuous tapes and patches comprised of a heat-activated adhesive.

 

Built with a pair of wheeled axels used to hold the spool material along with a pair of spring-loaded posts and a soldering iron, the functional tape rolled on spools can be applied directly to the fabric, similar to how you would sketch on fabric using a pen. Pushing down on the spring-loaded iron causes the adhesive to melt and hold the circuit in place. The device is even equipped with a small actuated blade to cut the tape to a specific length for any project. And since the tapes are rolled onto spools, they can be easily inserted and swapped out when needed. All the parts used to make the tool was 3D printed and protected with Teflon heat resistant fiberglass tape.

 

The tapes and patches it uses are easily ironed on, talk about a tool meant to be easy to use. This is due to its composition. Each patch or tape is made up of three layers: the adhesive layer that bonds it to a textile base, the functional layer, which can contain conductive materials, and the carrier layer that holds the layout of the functional material in place until it’s transferred to the textile.

 

It sounds pretty promising, but does it actually work? Short answer: yes. To show off its capabilities, the team created prototype smart clothing, including a smart cuff with a four-way button built in to control slide presentations for meetings. They also created a smart coat with an RFID that lets medical professionals gain access to secure locations without having to look for that pesky keycard. And if that wasn’t impressive enough, they even made a messenger bag equipped with internal lighting when opened, capacitive buttons and slider for controlling a music player, and a moisture sensor at the bottom for detecting leaks.

 

While the tests and the interviews the team conducted with fashion experts about the tool were positive, it’s still in the early stages. The team will work on improving the device and plan to run various workshops in design schools and maker spaces to see how it can be used by students and makers. Hopefully, it won’t be too long (or expensive) to get this out to makers and creators.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • dubbie
    dubbie over 6 years ago

    This looks fun, although I'm not especially a fan of smart clothing as I've never seen the interest. Most electronics nowadays is small and fits inside a pocket where it does not have to withstand the rigours of a washing machine.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    This looks fun, although I'm not especially a fan of smart clothing as I've never seen the interest. Most electronics nowadays is small and fits inside a pocket where it does not have to withstand the rigours of a washing machine.

     

    Dubbie