Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Researchers develop novel technique that prints 3D objects in seconds
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 4 Mar 2020 7:33 PM Date Created
  • Views 2961 views
  • Likes 5 likes
  • Comments 3 comments
  • 3d model
  • manufacturing
  • on_campus
  • 3D Printing
  • 3d_printing
  • cabeatwell
  • university
  • innovation
Related
Recommended

Researchers develop novel technique that prints 3D objects in seconds

Catwell
Catwell
4 Mar 2020

image

The new technique developed by EPFL researches produces a small, soft object in less than 30 seconds. (Image Credit: EPFL)

 

Traditional 3D printers are not magic… they take time. As you may know, the process, which can take hours or days to complete, involves slowly building up a 3D model one layer at a time. What if there was a way to shorten that time? Researchers at Switzerland’s EPFL have developed a new 3D printing method that takes less than 30 seconds to print high-precision objects. The team published their findings in the journal Nature Communications on February 12, 2020. 

 

This new technique involves solidifying a photosensitive resin with a laser. The researchers found inspiration in tomography techniques, the same ones used in x-rays and ultrasounds, to print a 3D model. This was achieved by illuminating a photosensitive resin from multiple angles with laser light modulated with a digital light processing (DLP) chip. The laser covers the entire build volume while the resin rotates as it’s exposed to the light. Afterward, the laser is synced up with the rotating resin, resulting in a 3D model being produced in just a matter of seconds.

 

“It’s all about the light,” explains Paul Delrot, Readily3D’s CTO. “The laser hardens the liquid through a process of polymerization. Depending on what we’re building, we use algorithms to calculate exactly where we need to aim the beams, from what angles, and at what dose.”

The new- process is capable of producing objects that measure up to 2 centimeters, with a precision of 80 micrometers. As the team improves the process and develops larger-scale printers, they could potentially build objects measuring up to 15 centimeters. The build volume of the 3D printer in EPFL’s demonstration measures 16mm x 16mm x 20mm.

 

“Conventional 3D printing techniques, known as additive manufacturing, build parts layer by layer,” explains Damien Loterie, the CEO of Readily3D. “The problem is that soft objects made that way quickly fall apart.”

 

With the speed and method of this new technique, these issues can easily be solved. The system could be used in biology and medicine fields to produce cell-laden scaffolds to create tissues or organs. Since the technique is also compatible with hydrogels and liquid polymers, it could produce soft objects like mouth guards and hearing aids. The researchers are already working with a surgeon to develop and test 3D printed arteries using this technique. It could also be used in interior and design markets since it can rapidly print acrylic or silicone parts without requiring a finish.

 

The new patent-pending technique developed by the EPFL researchers is already on its way to commercialization, through Readily3D, which will further develop and market the system.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply
  • dougw
    dougw over 2 years ago in reply to tederton

    That old SLA method is still in use, but it physically still moves the bed an hardens layer by layer. This sounds like they harden in a 3D space by focusing multiple lasers shining through the polymer concentrating enough power at the point they wish to harden to solidify the polymer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tederton
    tederton over 6 years ago

    New? I swear I saw this technology over 25 years ago at a convention. It was at least a cubic foot of resin and where the lasers crossed in it is where it catalyzed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    Sounds good. All they have to do now is make it print bigger thing, using harder materials, at a suitably low cost,then I'll want one. Someday this might happen.

     

    Dubbie