Industrial Automation
  • Technologies
  • More
Industrial Automation
Forum Do You Know the Three Types of Industrial Automation?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 285 subscribers
  • Views 10622 views
  • Users 0 members are here
Related

Do You Know the Three Types of Industrial Automation?

rscasny
rscasny over 7 years ago

In many circles, when you say the term "industrial automation," the word that comes into mind is robotics. I'll agree that robots are amazing pieces of engineering, but they are not the beginning and the end of all automation.

 

There are three types of automation:

 

  • Fixed: traditional manufacturing equipment that do one thing and only one thing. Think of a bottling line that inserts the soda and caps the bottle.
  • Programmable: this is for batch production up to a few thousand parts. Disadvantage: the automation equipment has to be re-programmed for different kinds of batches, thus there are inefficiencies inherent in this type of automation.
  • Flexible: like programmable automation but flexible automation can automate the production of different batches of products simultaneously. This is the paradigm of Industry 4.0, advanced manufacturing, etc.

 

So, where do robots fit in?

  • Sign in to reply
  • Cancel
  • hardikemamagara
    hardikemamagara over 3 years ago

    Yes, there are three types of industrial automation:

    1. Fixed Automation: This type of automation is designed for a specific task or product and is often used in mass production. The equipment and machines used in fixed automation are typically designed to perform one function or a limited set of functions, and they are not easily reprogrammable for different tasks or products. Examples of fixed automation include assembly lines, conveyors, and transfer lines.

    2. Programmable Automation: This type of automation is designed to be easily reprogrammed to perform different tasks or produce different products. Programmable automation is often used in applications where the production process must be flexible and adaptable to changing market demands. Examples of programmable automation include CNC machines, robots, and PLC-controlled machines.

    3. Flexible Automation: This type of automation combines the benefits of fixed automation and programmable automation. It is designed to handle a wide range of tasks and products, while also being reprogrammable for different tasks and products. Flexible automation is often used in applications where there is a high degree of variability in the production process or where there is a need for customization. Examples of flexible automation include robotic cells, modular machines, and flexible manufacturing systems.

    Overall, each type of industrial automation has its advantages and disadvantages, and the choice of automation type depends on the specific needs and requirements of the application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • echobatix
    echobatix over 6 years ago

    This is conceptually an interesting way to think of it, but after working in industrial automation for more than two decades I’d say no one I know of speaks in quite these terms, which seem a bit limiting.

     

    Industrial automation includes conveyors, proximity switches, rotary encoders, pull chains, machine vision, ultrasonic sensors, lifts, control networks, communication protocols, clamping jigs, PLCs, . . . (breathe, breathe, breathe) . . . safety curtains, optical comparators, thermal sensors, pill dispensers, automatic washdowns, forklifts, lights, parts bins, SPC, warehouse database systems, logistics software, coordinate measurement machines in temperature-controlled QC rooms, light stacks, paper transfer tickets, cable trays, product carriers, barcode readers, things that wrap, things that tie, and uncountable eletromechanical things that have been around for a century or more, but wouldn’t qualify as robots.

     

    And lots and lots of production workers, engineers, managers, et al., to make sure every minute that the whole enterprise doesn’t collapse.

     

    Robots by themselves don’t do much. No single piece of equipment does. Making distinctions between static, adaptable, programmable, tweakable, reconfigurable, refreshable, etc., typically only makes sense in a specific context.

     

    6-axis and 7-axis arm robots, gantry robots, and other robots are flexible and highly programmable and can “do anything” until they can’t.

    • Cancel
    • Vote Up +4 Vote Down