Industrial Automation
  • Technologies
  • More
Industrial Automation
Forum Do You Know the Three Types of Industrial Automation?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 285 subscribers
  • Views 10623 views
  • Users 0 members are here
Related

Do You Know the Three Types of Industrial Automation?

rscasny
rscasny over 7 years ago

In many circles, when you say the term "industrial automation," the word that comes into mind is robotics. I'll agree that robots are amazing pieces of engineering, but they are not the beginning and the end of all automation.

 

There are three types of automation:

 

  • Fixed: traditional manufacturing equipment that do one thing and only one thing. Think of a bottling line that inserts the soda and caps the bottle.
  • Programmable: this is for batch production up to a few thousand parts. Disadvantage: the automation equipment has to be re-programmed for different kinds of batches, thus there are inefficiencies inherent in this type of automation.
  • Flexible: like programmable automation but flexible automation can automate the production of different batches of products simultaneously. This is the paradigm of Industry 4.0, advanced manufacturing, etc.

 

So, where do robots fit in?

  • Sign in to reply
  • Cancel
Parents
  • hardikemamagara
    hardikemamagara over 3 years ago

    Yes, there are three types of industrial automation:

    1. Fixed Automation: This type of automation is designed for a specific task or product and is often used in mass production. The equipment and machines used in fixed automation are typically designed to perform one function or a limited set of functions, and they are not easily reprogrammable for different tasks or products. Examples of fixed automation include assembly lines, conveyors, and transfer lines.

    2. Programmable Automation: This type of automation is designed to be easily reprogrammed to perform different tasks or produce different products. Programmable automation is often used in applications where the production process must be flexible and adaptable to changing market demands. Examples of programmable automation include CNC machines, robots, and PLC-controlled machines.

    3. Flexible Automation: This type of automation combines the benefits of fixed automation and programmable automation. It is designed to handle a wide range of tasks and products, while also being reprogrammable for different tasks and products. Flexible automation is often used in applications where there is a high degree of variability in the production process or where there is a need for customization. Examples of flexible automation include robotic cells, modular machines, and flexible manufacturing systems.

    Overall, each type of industrial automation has its advantages and disadvantages, and the choice of automation type depends on the specific needs and requirements of the application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hardikemamagara
    hardikemamagara over 3 years ago

    Yes, there are three types of industrial automation:

    1. Fixed Automation: This type of automation is designed for a specific task or product and is often used in mass production. The equipment and machines used in fixed automation are typically designed to perform one function or a limited set of functions, and they are not easily reprogrammable for different tasks or products. Examples of fixed automation include assembly lines, conveyors, and transfer lines.

    2. Programmable Automation: This type of automation is designed to be easily reprogrammed to perform different tasks or produce different products. Programmable automation is often used in applications where the production process must be flexible and adaptable to changing market demands. Examples of programmable automation include CNC machines, robots, and PLC-controlled machines.

    3. Flexible Automation: This type of automation combines the benefits of fixed automation and programmable automation. It is designed to handle a wide range of tasks and products, while also being reprogrammable for different tasks and products. Flexible automation is often used in applications where there is a high degree of variability in the production process or where there is a need for customization. Examples of flexible automation include robotic cells, modular machines, and flexible manufacturing systems.

    Overall, each type of industrial automation has its advantages and disadvantages, and the choice of automation type depends on the specific needs and requirements of the application.