Industrial Automation
  • Technologies
  • More
Industrial Automation
Forum Need to find a "reverse" USB selector for a single computer; multiple downstream devices
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 289 subscribers
  • Views 3180 views
  • Users 0 members are here
  • selector
  • usb
Related

Need to find a "reverse" USB selector for a single computer; multiple downstream devices

aspork42
aspork42 over 6 years ago

I have a need for what appears to be a rare device. I have software that prints to a default USB printer. I cannot change the software. The problem is I have two USB printers. I want an A/B switch box that I can use to select which printer is plugged in.

 

This would be the equivalent of just unplugging one printer and plugging the other in. This is for an industrial installation with 100's of devices required. The end user isn't able to change software and doesn't want associates swapping USB cables all day long.

 

All the USB selectors that I can find just share USB devices between two computers.

 

This is the only one that I have been able to find, but am weary about offering it: https://www.newegg.com/p/36F-00D5-00007?item=9SIAK1JB676151&source=region&nm_mc=knc-googlemkp-pc&cm_mmc=knc-googlemkp-pc…

 

I was really hoping to find a name brand like IOGear or similar, but keep coming up empty. I just need a single upstream device (the computer) and two downstream devices (Printer A, Printer B).

 

image

This image is from the NewEgg listing.

 

In theory, even the normal USB selectors 'might' just work by default if they are just A/B switch the D+ and D- on the USB bus between the two ports without other active components involved.. but the problem is I don't want to have to get a bunch of different samples to test with. I want to buy something off the shelf that I know works.

 

Has anyone seen something like this before?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi James,

     

    Since it's low-cost, I think it likely just contains a multipole switch, and it is switching over (at least) the two data lines and the 5V connection, if not the ground connection too.

    It is probably fine for USB full speed perhaps, which I'm guessing is fine for printers.

    As Dave says, if such cables are available, then it's likely to work (but definitely test on one before ordering a hundred : )

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Hi James,

     

    Since it's low-cost, I think it likely just contains a multipole switch, and it is switching over (at least) the two data lines and the 5V connection, if not the ground connection too.

    It is probably fine for USB full speed perhaps, which I'm guessing is fine for printers.

    As Dave says, if such cables are available, then it's likely to work (but definitely test on one before ordering a hundred : )

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer