Industrial Automation
  • Technologies
  • More
Industrial Automation
Forum Need to find a "reverse" USB selector for a single computer; multiple downstream devices
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 289 subscribers
  • Views 3180 views
  • Users 0 members are here
  • selector
  • usb
Related

Need to find a "reverse" USB selector for a single computer; multiple downstream devices

aspork42
aspork42 over 6 years ago

I have a need for what appears to be a rare device. I have software that prints to a default USB printer. I cannot change the software. The problem is I have two USB printers. I want an A/B switch box that I can use to select which printer is plugged in.

 

This would be the equivalent of just unplugging one printer and plugging the other in. This is for an industrial installation with 100's of devices required. The end user isn't able to change software and doesn't want associates swapping USB cables all day long.

 

All the USB selectors that I can find just share USB devices between two computers.

 

This is the only one that I have been able to find, but am weary about offering it: https://www.newegg.com/p/36F-00D5-00007?item=9SIAK1JB676151&source=region&nm_mc=knc-googlemkp-pc&cm_mmc=knc-googlemkp-pc…

 

I was really hoping to find a name brand like IOGear or similar, but keep coming up empty. I just need a single upstream device (the computer) and two downstream devices (Printer A, Printer B).

 

image

This image is from the NewEgg listing.

 

In theory, even the normal USB selectors 'might' just work by default if they are just A/B switch the D+ and D- on the USB bus between the two ports without other active components involved.. but the problem is I don't want to have to get a bunch of different samples to test with. I want to buy something off the shelf that I know works.

 

Has anyone seen something like this before?

  • Sign in to reply
  • Cancel
Parents
  • rsc
    0 rsc over 6 years ago

    The problem you will run into, is that one USB1,2 Hub can service 127 devices, and there is handshaking between the devices and the computer (when it's first plugged in) to determine device type, identification for drivers and speed negotiations.  If you change the printer, it's configuration is now invalid and the new printer will not know what the configuration was/is.  USB is not like RS232, you can't just swap the data lines between devices and assume it will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rsc
    0 rsc over 6 years ago

    The problem you will run into, is that one USB1,2 Hub can service 127 devices, and there is handshaking between the devices and the computer (when it's first plugged in) to determine device type, identification for drivers and speed negotiations.  If you change the printer, it's configuration is now invalid and the new printer will not know what the configuration was/is.  USB is not like RS232, you can't just swap the data lines between devices and assume it will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer