Industrial Automation
  • Technologies
  • More
Industrial Automation
Forum E14 Community recommendation for ModBus TCP client
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 286 subscribers
  • Views 1533 views
  • Users 0 members are here
  • modbus testing
  • modbus
  • client application
Related

E14 Community recommendation for ModBus TCP client

colporteur
colporteur 4 months ago

I am looking for an application to query a ModBus TCP interface on a scale head?

image

The company I am working for has recently installed a RiceLake 1280 scale indicator with a Modbus TCP interface. The scale indicator is IP capable and resides in a network DMZ. The goal is to have a cloud vendor pull scale data over the network from the Modbus interface. I'm looking for an application that can query the Modbus interface to confirm communication with the interface. 

The scale vendor recommended an application in order to set the Modbus TCP interface IP address. I managed to get that working, proving the interface IP answers an IP ping. DMZ rules have been set in place to isolate the indicator. I want to test that the cloud vendor can get to the Modbus interface and pull the data. I'm thinking maybe there is a software tool like minicom is for serial communication, except the tool is for Modbus.

E14 has some great Modbus resources but nothing to match my search. A Modbus client query tool. I'm hoping there is a community member that has experience with Modbus TCP and that they could recommend application software to perform the task.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz 4 months ago

    Hi Sean,

    While it's not the best protocol for this (it's a bit "naked"! and the cloud app vendor ought to have come up with better proposals to be honest), but anyway, I was interested, because by coincidence I'm just getting going with Modbus RTU currently (RS-485 instead of TCP, some differences in the protocol). I got curious enough to try to find the user manual for the 1280 Modbus TCP card. I gave that to AI, and it generated the Python code attached below. It complained that the user manual was vague in places, which it is, so I told it to try to make a simulator that accepted a few different function codes, and then try to simulate the cloud side too). 

    The screenshot shows the 1280_simulator.py file running at the left side, it just sits and waits for a connection.

    On the right window, you can see the cloud_app_simulator.py file running, it makes a TCP connection to the 1280 simulator, and then tries a few function codes.

    Currently the code transmits to port 127.0.0.1 and port 1502, you'd need to modify both of those to suit your needs.

    Please don't ask me for modifications or tweaks, I don't know Modbus TCP nor what the AI did! : ) It might be ok but it might not. It might completely fail.

    I suppose one other thing worth doing is perhaps running WireShark, and examining if it successfully decodes whatever is sent by these two simulators. I didn't try that (I've not got WireShark installed currently). I only tried running the Python code on Windows, it should work with Linux but I can't be sure.

    image

    modbus_tcp_python.zip

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur 4 months ago in reply to shabaz

    Thanks S. I will it a try next week.

    I have a programmer friend that did something simulator. He had a python script running a modbus server. I couldn't buy him enough beer to make a client:(

    I figured someone here would have used a modbus client. Coming up zeros.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 4 months ago in reply to colporteur
    colporteur said:
    I figured someone here would have used a modbus client. Coming up zeros.

    "...This also required using Modbus (TCP) within a Python script to be able to send commands..."

    https://community.element14.com/challenges-projects/project14/musictime/b/blog/posts/100-year-old-player-piano-gets-an-update-music-time-via-python-and-modbus-tcp

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur 4 months ago in reply to beacon_dave

    Yeah I got excited with this find. I've considered a cut and paste to see if I can get a phthon scrpt to work. Shabaz has given me a better starting point, so I will start there first if an app search is unfruitful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur 4 months ago in reply to beacon_dave

    Yeah I got excited with this find. I've considered a cut and paste to see if I can get a phthon scrpt to work. Shabaz has given me a better starting point, so I will start there first if an app search is unfruitful.