Industrial Automation
  • Technologies
  • More
Industrial Automation
Forum Mis-using RS-485 interfaces to generate audio and visual alerts : )
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 286 subscribers
  • Views 313 views
  • Users 0 members are here
  • rs-232
  • hack
  • rs-485
  • rs485
  • rs232
Related

Mis-using RS-485 interfaces to generate audio and visual alerts : )

shabaz
shabaz 2 months ago

I did a bit of a hack today : )

I have a Pi Pico, attached to an RS-485 transceiver. As you're maybe aware, the RS-485 transceiver converts the UART signal into two signals, called A and B, or Non-Inverting and Inverting. The oscilloscope trace below explains this.

image

What's not shown is that the A and B outputs are often only enabled if requested to do so by applying a logic high on a Driver Enable (DE) pin. If the DE pin is low, then the A and B signals will no longer output a signal.

I had a request from a friend to control an LED and a little audio tone beeper from the Pi Pico. Sometimes he wanted just the LED to light, sometimes just the beeper, and sometimes both. He doesn't need RS-485. 

I initially considered opening up the device and wiring things up to spare GPIO pins internally. However, after thinking some more, I realized I could just repurpose the RS-485 connections, as shown in the video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

To get this to work, all I needed to do was a software mod, to change the Pi Pico UART Tx pin to become a normal GPIO configured as an output. Then, the logic was simple:

Driver Enable

(DE)

UART

TXD

RS-485

A,B

1 0 Low, High
1 1 High, Low
0 0 HiZ, HiZ
0 1 HiZ, HiZ

I wired the little beeper to the A connection, and the LED to the B connection (use series diodes and resistors as required to reduce the voltage or current if needed), with the other end of each connected to 0V (ground).

I cannot turn on both the LED and the beeper simultaneously, but that's not a big deal, the code can just alternate every second as shown in the video.

I'll encase this in moldable plastic (PolyDoh), that will be good enough for the particular use-case.

image

Not a very clever hack, but it did save me some effort!

Thanks for reading.

  • Sign in to reply
  • Cancel
Parents
  • kmikemoo
    kmikemoo 2 months ago

    shabaz Sounds pretty clever to me.  Simple is hard. Well done. RelaxedThumbsup

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kmikemoo
    kmikemoo 2 months ago

    shabaz Sounds pretty clever to me.  Simple is hard. Well done. RelaxedThumbsup