Internet of Things
  • Technologies
  • More
Internet of Things
Blog Anyone up for an IIOT Relay Race? (Ignoble Internet of Things)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: aspork42
  • Date Created: 12 Nov 2019 2:02 AM Date Created
  • Views 3979 views
  • Likes 18 likes
  • Comments 18 comments
  • iiot
  • design_challenge
  • ignoble internet of things relay race
  • relay race
Related
Recommended

Anyone up for an IIOT Relay Race? (Ignoble Internet of Things)

aspork42
aspork42
12 Nov 2019

My wife and I were talking about the E14 site and she asked something about doing a team project. It was a very interesting idea, but most likely we all have enough of that in our day jobs. I still liked the idea of having to work out design details and specs as part of a design challenge with people from literally all across the globe. I mulled the idea over and over and this is what I have come up with.

 

The concept is as follows:

 

Each participant must create some soft of IoT enabled device. (Not too bad, right?)

 

The device must do three things:

  1. Get some sort of input from the World Wide Internet
  2. Do something
  3. Post something else back out to the World Wide Internet.

 

Sounds pretty simple, huh?

There's a catch - this is a "relay race". That means that when Participant "A" posts something, that is the trigger for Participant B's project - which is armed and waiting for A's post. Once "B" is complete, that will trigger Participant C's project. This means that there will be an input and an output for each person that must be sequenced.

 

For Step 2, "Do something", It could be simple or complicated. It could be as basic as turning on an LED on an Arduino, display something on an LCD, calculate Pi to 'x' places, or complicated like having a MeArm waiting to manually peck at a keyboard to post something on Twitter. You could have your model train turn on and start driving until it breaks a light beam to trigger the output.

image

 

For the web interconnects, we can get creative here as well. Twitter works pretty well, but we could also use a public MQTT server (Mosquito), parse an email, or send via RF/Ham/ Morse Code / semaphore if you are close enough (and licensed) to another participant. Any API for any platform that two users are able to work together on. Users could apply in groups for highly specific interconnects, and we could have the E14 team assign the rest of the order.

 

The format would be pretty wide open - each participant will agree with their two "co-workers" on the exact interconnect methods. The Input and the Output method could be different for any given project, depending on the users (i.e. read from Twitter, then send an email when done). The project could be as simple or as complicated as the user is able to do in the allotted time. I'm thinking 30-60 day project).

 

One challenge would be the exact timing (time of day/elapsed duration) of the final run - we are a global community from all corners of the earth, so some people would have be up at late hours to record the event. Ideally each unit would complete its task in less than 1 minute (or really a few seconds for simple things), but perhaps we could build in time gaps... i.e. if you have hacked your washing machine, it would start running when it gets the trigger, and when the clothes are done some 35 minutes later, it would trigger the next person. That way, we could build in some delays.

 

So this would end up a world-wide Rube-Goldberg, but we would call it "The Ignoble Internet of Things Relay Race"

 

This made me think back to this post, but now imagine each Arduino is 1000 miles apart!

Celebrating Arduino with a Torch Relay!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

During the final run, everyone could record a video and we could edit them all together.

 

Since "success" is defined by the entire project going from start to finish, there would't necessarily be a winner, but we could vote on most creative and try to con rscasny into making up some T-Shirts.

 

Post your comments - What would some unique interconnect methods to talk to devices which are far apart? What would your project do before sending a response?

  • Sign in to reply

Top Comments

  • crisdeodates
    crisdeodates over 6 years ago +5
    Cool idea indeed. Not only this is fun, it will allow a participation globally. Everyone would be able to contribute. That's what it really make this a community.... ️
  • aspork42
    aspork42 over 6 years ago in reply to clem57 +4
    I was thinking of that - like a game of telephone; or the game you play with kids where each person takes a turn adding one sentence to a story. The hang up would be that some communications methods might…
  • Workshopshed
    Workshopshed over 6 years ago in reply to dixonselvan +4
    It the protocol e.g. MQTT is agreed then there's no reason any device can't be used and hence we can get more participants. I'm sure the Top Members would be up for helping anyone who is having trouble…
Parents
  • crisdeodates
    crisdeodates over 6 years ago

    Cool idea indeed. Not only this is fun, it will allow a participation globally. Everyone would be able to contribute. That's what it really make this a community.... Relaxed️

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • crisdeodates
    crisdeodates over 6 years ago

    Cool idea indeed. Not only this is fun, it will allow a participation globally. Everyone would be able to contribute. That's what it really make this a community.... Relaxed️

    • Cancel
    • Vote Up +5 Vote Down