Internet of Things
  • Technologies
  • More
Internet of Things
Blog Azure Sphere (MT3620)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bwilless
  • Date Created: 19 Nov 2018 3:27 PM Date Created
  • Views 2333 views
  • Likes 12 likes
  • Comments 8 comments
  • azure sphere
  • avnet
  • mt3620
  • iot
Related
Recommended

Azure Sphere (MT3620)

bwilless
bwilless
19 Nov 2018

My name is Brian Willess, I work at Avnet where I'm responsible for training Azure Sphere customers.  I wanted to advertise the MT3620 Azure Sphere device and its supporting systems to this community.  Azure Sphere has everything you need to develop and deploy a secure IoT solution quickly.

 

Azure Sphere

 

The Azure Sphere system developed by Microsoft combines a secure MCU, secure OS (Linux kernel), and the Azure Sphere Security Service (in the cloud) to deliver a highly secure IoT solution.  Just a few of the key benefits of the system are listed below:

 

  • Certificate based authentication to the cloud (Managed by Microsoft)
  • Threat monitoring (Managed by Microsoft)
  • Over the air updates (Managed by Microsoft)
    • OS updates included for 13 years
    • OEM application updates included for the agreed life of your device
  • Sphere development is integrated into the Visual Studio development environment
    • Secure connections to Azure works out of the box
    • Support for telemetry data, device twins, remote method calls are all included with the Sphere SDK
    • Remote GDB real-time debugging using Visual Studio debugger interface

 

7-Properties of a highly secure device

 

One of the fundamental design goals in the Azure Sphere ecosystem is security.  Microsoft has some experience with security; the first two generations of the XBox were both hacked within weeks of release.  Microsoft decided to do something about that and spun up a research team to solve the problem.  This team developed the 7 Properties of a Highly Secure device, white paper here.  The latest XBox system implemented the 7-Properties and has not been hacked.  (Note that the XBox does NOT use the Azure Sphere device).  These 7-Properties are all implemented in the Azure Sphere solution.

 

  • Hardware Root of Trust – The identifying cryptographic keys are embedded and protected by secure element physical hardware with a hardware firewall around it.
  • Certificate-Based Authentication – Well beyond passwords, certificates are unforgeable and prove device authenticity.
  • Small Trusted Computing Base – Only a small portion of the device firmware has access to the private cryptography keys.
  • Defense in Depth – Multiple layers of security that mitigate attacks.
  • Compartmentalization –  On-Chip Software Systems are highly compartmentalized, leaving little access from compartment to compartment.
  • Failure Reporting – Ecosystem monitoring to watch for threats, and threat methodologies.
  • Renewable Security – Let Microsoft update security systems – Just like a Windows System update.  Nice.

 

Azure Sphere Links

 

  • Azure Sphere Documentation
  • Azure Sphere Overview (Video)

 

Brian

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 7 years ago +3
    Hi bwilless the Azure Sphere is something I'm working with at the moment, you can follow along with my project on the blog. https://www.element14.com/community/people/Workshopshed/blog/tags#/?tags=azure…
  • Fred27
    Fred27 over 7 years ago +1
    Azure Sphere sounds interesting but the documentation and ecosystem seem a bit lacking right now. For instance, the examples available at the moment seem to just deploy code to one of the M4F cores. Is…
  • shabaz
    shabaz over 7 years ago +1
    Interesting device : ) Nice that it is all very integrated into a single package at 12x12mm.. impressive!
Parents
  • Fred27
    Fred27 over 7 years ago

    Azure Sphere sounds interesting but the documentation and ecosystem seem a bit lacking right now.

     

    For instance, the examples available at the moment seem to just deploy code to one of the M4F cores. Is there any more info about using both user-accessible M4F cores or the A9?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwilless
    bwilless over 7 years ago in reply to Fred27

    Hi David,

     

    Thanks for the comment.  This is a new device and a new ecosystem.  Currently user applications only run on the Arm Cortex A7 processor running at 500Mhz.  The M4 processors are not available for user applications in the current release.  Microsoft has support for user applications running on the M4 processors on the roadmap.

     

    A few of the things that make the Sphere a good solution is that most of the heavy lifting is all done for you, Over the Air Updates, Certificate based Authentication, Secure Connections to the cloud.  Developers only need to worry about their application reading sensors and sending up telemetry data.

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bwilless
    bwilless over 7 years ago in reply to Fred27

    Hi David,

     

    Thanks for the comment.  This is a new device and a new ecosystem.  Currently user applications only run on the Arm Cortex A7 processor running at 500Mhz.  The M4 processors are not available for user applications in the current release.  Microsoft has support for user applications running on the M4 processors on the roadmap.

     

    A few of the things that make the Sphere a good solution is that most of the heavy lifting is all done for you, Over the Air Updates, Certificate based Authentication, Secure Connections to the cloud.  Developers only need to worry about their application reading sensors and sending up telemetry data.

     

    Brian