Internet of Things
  • Technologies
  • More
Internet of Things
Blog Itead Studio Sonoff and Slampher: Low Cost Smart Home Solution - Review
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kas.lewis
  • Date Created: 25 Dec 2015 7:29 AM Date Created
  • Views 14646 views
  • Likes 5 likes
  • Comments 53 comments
  • internet_of_everything
  • internet_of_things
  • sonoff
  • itead_wifi_switch
  • slampher
  • iot
Related
Recommended

Itead Studio Sonoff and Slampher: Low Cost Smart Home Solution - Review

kas.lewis
kas.lewis
25 Dec 2015

sonoffslampher.jpg

 

INTRODUCTION

Itead Studio has launched a indiegogo campaign to help bring one of their new products to market. Itead Studio has been working on a WiFi enabled switch for easy home automation. They have specifically been working on two products, one that fits into a light fixture (Slampher) and one that is spliced into any cable (Sonoff). The catch behind these two products is their incredible low price (~$7 per unit) and their easy of use.

 

HOW I ARRIVED AT THIS POINT

I was contacted through one of my reviews on Element14 by Itead Studio concerning a new product they are looking to launch. I was asked if I was interested in reviewing a WiFi switch of theirs and to give them some feedback. As I have played around with passing data over WiFi (see my Plot.ly project) I was intrested how this may work to control something in a smart home, so I promptly responded YES! After a shipping delay the package of one Sonoff, one slampher and a 433 MHz remote were on my way.

 

It took a short altercation with DHL and some kind help from customs to have my package firmly in my grasp.

 

INITIAL SETUP (NO INSTRUCTIONS)

Having arrived on a Thursday I decided to wait for the weekend to try everything out as I figured it may take some time to look into everything that interested me about this product. When I did start to play with the units I decided to start without looking at any instructions, if I can get most. if not all the way through using a product then I’m willing to keep going with it. I started by downloading the app from the Google Play store and tried from there to get something started. In all to get the slampher working took 5 minutes without instructions, for some unknown reason the Sonoff took a bit longer but eventually it worked as well. The next step was to get the 433 MHz remote working. With some fiddling around the Lamphor connected to button A on the remote but there was no way I was getting the Sonoff to connect to button B. After trying various more things and figuring the unit was a bust I decided to read the instructions… It didn’t take more than 30 seconds after doing that to connect the Sonoff to the remote's button B.

 

SETUP WITH INSTRUCTIONS (THE CORRECT WAY)

The correct procedure, this time following the instructions would be:

 

If you would like to simply turn on/off your device without using the remote or app then you can quickly press the “set” button on slampher/sonoff once to do so.

 

Pair with 433Mhz RF remote controller without WiFi .

Press the “set” button on Sonoff and Slampher twice quickly and the red LED on Sonoff/Slampher will flash one time.

 

Now press button “A”, ”B”, ”C” or ”D” on the controller to pair with the remote. If you pair it with “A”, then pressing “A” will turn on/off your device.

 

If you would like to remove the pairing, press the"set" button on Sonoff/Slampher quickly 3 times.

 

APP Operation

1. Download and install the app on your smartphone

 

2. Register a new account, you’ll need to enter your phone No. and password (at least 8 letters, must contain number, lowercase and uppercase letters). A code will be sent to your phone via SMS, enter the verification code to register.

 

3. Login with your account.

 

4. Add devices.

4A. Before adding a device, you must turn on the WiFi on your phone, then press and hold the “set” button until the green LED indicator blinks quickly.

 

4B. In the app click “+” to add devices followed by “Start searching”, it will auto-search and connect the “ITEAD10000xxx” WiFi around you.

 

4C. Then select your WiFi account and enter password, click remember so that next time you don’t need to fill in again.

 

4D. Click “next” to name your device, then “next” you will add the device successfully.

 

Note: If you see the new added device is offline, please wait for a moment. If it keeps offline, please power off the device, then power it up, if everything is ok, it will become online.

 

5. Delete devices

If you would like to remove a device, you need to go to the devices list, then slide the device name from right to left. You will see the delete icon, just press it to delete your device.

 

7.Manage Group

Click the top right corner button on device list interface. You’ll see”Manage Group””Exit Account””Exit e-Welink”. Click “Manage Group” to add or delete group. After adding group, you can long press to select the device and move it under your group. If you delete a group, the devices belong to this group will still exist.

 

8.Share devices

Enter the device you want to share, click icon “share” then enter the Phone number you want to share with, this phone No. should register and login first and remain online. That number will then receive an invitation message, by accepting the invitation, that user will have the authority to control the device you share. Only the owner of the devices has right to share devices.

 

e-WeLink APP

The app packs a lot of functionality even if it may be in its initial stages of release. The first feature that is very much appreciated and may be taken for granted is the status update. Whenever the status of the device is changed, the app will reflect this change. That is, if a shared user changes the status or someone uses the remote or if someone presses the button on the device directly, any of these changes will be reflected in the app. This quickly and easily allows a user to know the status and change it and verify that change if needed.

 

Another nice feature is the timer feature, considering a basic timer will run you ~$20 this is one big deal. There are a number of timers that can be set (the exact number is untested at this point). But not only can a timer be set once or repeatedly but, there is a countdown timer as well. This is a nice feature for someone leaving their house or getting ready for bed. The timer could be set to turn off the light after a specified amount of time without the need to remember to do so once you have left the house or gone to bed.

 

As this is an app on a smartphone it would not be complete if it was not possible to share control with another user. This too has been included and is easily done. Once shared the other user can easily turn on and off the device and use it the same as the main user. For this feature it would be nice if in a future release of the app if the level of control could be chosen so that a secondary user could not remove timers or maybe could only turn on/off a device but not the other way around. 

 

Itead has definitely thought of this as a large scale project in that they are hoping that you will deploy this across many locations, to make this easier they have introduced groups A group allows a user to put all devices, say in their home, in one group so that finding the standing lamp in your dining room will be relatively easy without needing to go through all the devices at the cottage, office, etc.

 

Overall the app is intuitive and very easy to use. Itead has kept the user interface simple and clean allowing for a great user experience, and with fast update times on a device's status change the app keeps you always informed as to what your devices are doing.

 

Power Consumption

One of the things that concerns me about using a device that is always plugged in is the ongoing power consumption. The idea here is partly to reduce power consumption and potentially save money. I was therefore wondering what the power consumption of the Sonoff was. It should be noted that currently there is nothing to compare this value to but hopefully in the near future this will be added.

 

As can be seen in the graphs below the power consumption appears to be sitting below 1 Watt for half of the duration and above 1 watt for the remainder. It should be noted that the blips that exceed these values are when the unit was on and powering a fluorescent lamp.

 

image

Figure 1. Power consumption measured in watts

 

image

Figure 2. Current measured in amperes

 

image

Figure 3. Voltage measured in volts

 

The issue here is the overall cost of having a unit connected all the time if there was away for Itead to reduce the overall power consumption this would make for an even better product.

 

That being said there are two HUGE factors to take into account regarding my measurements. The first is I was using two multimeters logging at one second intervals to a laptop over bluetooth and this may not provide the best results. If the unit only wakes up every 200 ms and is on for 20 ms to listen for WiFi or 433 MHz signals the power savings would be tremendous but the multimeters would not see that and report a higher than real power consumption. The second issue is the lack of comparable data, without anything to compare my measurements too only a small fraction of the data is being shown. For this to be useful I would need to take measurements on other time switches as well as other comparable devices, such as those from Belkin. In a later post I will try look at a time switch to be able to at least give another data point.

 

P1040254.JPGP1040255.JPG

Figure 4. Setup used to measure voltage and current to arrive at power consumption

 

I am hoping to look more into the power consumption as well as some of the irregularities that can be seen in the first half of the graphs in a later blog entry. I would also like to look into what the power consumption is of both the sonoff and the slampher in relation to other timing/standby products to get a better understanding of how the efficiency of these products compares to other such products.

 

CONCERNS

After working with this product for a few days I have tried a few different things and feel I have enough basic experience to give my feedback both positive and some less so. Starting with the less so, I would say the app needs some work. Currently the network password for your home network is stored in plain text and is always available I have been assured that this will be fixed in a later release of the app and is a “known issue”. It would also be nice if I did not have to go into each individual light to see its state but rather if the entry page could display that information directly.

Screenshot_2015-12-03-01-07-14.png

Figure 5. Itead app home page

 

The next concern I have is the longevity of the unit. Since all the units only work through Itead’s servers, should this fail for some reason all the units would no longer be useable unless someone else decided to take that on or if Itead would make all their code publicly available. Currently I do not see this as an immediate issue as Itead appears to be taking this product very seriously

 

Lastly is the issue of form factor, both the slampher and sonoff could be more discreet. The slampher adds a decent amount of length to the average light bulb preventing this from being used in a closed light fixture or any fixture that may have a length limit. As for the sonoff the form factor is pretty good, but one person noted if it could be smaller it could be inserted in light or socket fixtures. Maybe the real solution to that is for Itead to increase their product range by offering a light switch or conventional plug. Overall I did not have any issue with the sonoff other than a possible missing connection point for a ground wire connection when using a three prong plug.

P1040260.JPG

Figure 6. Sonoff with two connection points



POSITIVES

For Itead’s offerings the positives outweigh the cons. Firstly it should be noted that the price point per unit for Itead’s system is significantly less than that offered by the competitors, at ~$7 per unit or ~$22 for 4 units the cost is very low.

The next positive is ease of use, the simplicity in the units setup and control make it easily usable by anyone on any level of technical knowledge. The clean interface in the app allows for easy and quick control of any device be it in your home network or in another location network. The overall system also adds a decent amount of convenience as well as security with the ability to remotely turn on lights and well as check their status remotely. This would be great for someone coming home late and would like to have their home illuminated before entering either for comfort or security. This system would also allow for light to be turned on should motion be detected somewhere or a noise heard without the need to go to that location.

 

I also found the design of both units, while maybe cumbersome in form, easy to you. The slampher simply fits into an existing light fixture and then a bulb is inserted into it. While the sonoff has two connection points and is agnostic as to how the wires are connected. This allows for anyone to connect a device by splicing the wires with only the need to ensure they keep each wire going in connected to itself at the exit. While I have not checked that both wire are disconnected when the sonoff is turned off, I would imagine that this would be so to ensure the end device (lamp, fan , etc.) is not live with only the ground wire disconnected.

 

These devices potentially also have the ability to reduce power costs as the devices can be turned off remotely. This means if a light/device was left on or may have been left on the app can be checked and if indeed the light/device was indeed left on it can be turned off remotely thus saving power and money.






MOVING FORWARD

I have chosen to further support Itead’s campaign buy buying 4 Slamphers for use around the home. I have done so for a few reasons. Firstly the level of support I have received shows that there is active development and knowledgeable people behind this development. Secondly, I have samples in hand this shows that they have something that works that is ready for feedback and lastly Itead is a functioning and thriving online store. This would imply they have both the knowledge and ability to bring this product to fruition. While there may be some concerns, overall I believe it is relatively small payout for a potentially amazing and growing product.








Indiegogo Campaign

https://www.indiegogo.com/projects/sonoff-slampher-low-cost-smart-home-solution/#/

 

Blog on standby Power

http://goughlui.com/2015/12/23/standbyno-load-power-consumption-are-we-doing-it-right/

 

Other Blogs On Itead Slampher & Sonoff Reviews (in no specific order)

http://matthewcmcmillan.blogspot.ca/2015/12/product-review-itead-studio-wifi.html?showCom

ment=1450703164942

 

http://blog.brianmoses.net/2015/12/sonoff-and-slampher-home-automation-review.html

 

http://misc.ws/2015/12/11/itead-studios-smart-home-switches/

 

http://electronicopensource.blogspot.ca/2015/11/itead-sonoff-wifi-wireless-switch.html

 

http://www.cnx-software.com/2015/12/03/sonoff-slampher-are-5-rf-and-wifi-smart-switches-and-lightbulb-adapters-crowdfunding/

 

http://nfriedly.com/techblog/2015-12-16-itead-sonoff-slampher-review/

 

https://giovanniorgantini.wordpress.com/2015/12/22/home-automation/

 





Tweet

Follow @Kazzzzzzzzzzz

Follow Kas' blog
  • Sign in to reply

Top Comments

  • kas.lewis
    kas.lewis over 10 years ago in reply to mcb1 +3
    Hello mcb1, From looking at the Indiegogo campaign (Itead has done 6 of which 3 were very successful and 3...) itcraze is a member of Itead Studio and more specifically their indiegogo campaign team (now…
  • kas.lewis
    kas.lewis over 10 years ago in reply to e14 Contributor +2
    Hello itcraze I understand that may be your preference but some of use here would maybe like to do other interesting things with this product and not be stuck with one option or may be concerned about…
  • kas.lewis
    kas.lewis over 10 years ago in reply to mcb1 +2
    mcb1 , Here is m latest exchange with the person from Itead Studio I have been dealing with: I wrote: Hello Emmy, I was wondering, what happens to all the pledges if the Indiegogo campaign is not…
  • mcb1
    mcb1 over 10 years ago in reply to Gough Lui

    Nice conversation guys.

     

    I'm more interested in the ability to safely control a Mains source.

    We struggle with many dangerous examples appearing from time to time, and at the prices mentioned there is no excuse not to use these.

     

    In many cases the 433MHz will suffice, but wireless makes it so much better.

     

     

    Power

    I'm wondering if you were to provide a small resistance in the neutral lead, you could safely measure across it with a scope.

    To be absolutely safe, an isolating transformer that powers the scope and the device would be preferable.

     

    This may allow you to measure both voltage and current and the relationship between them on the input side.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to kas.lewis

    Definitely an ethical consideration, kas.lewis, but on the whole, I tend not to worry so much because of several reasons:

    - If they do have something innovative, then they should have filed for and received the necessary protections (e.g. patents, design patents) ahead of letting the "cat out of the bag", or risk losing their competitive advantage.

    - Reverse engineering not for profit doesn't seem to be a big issue, and specifically in the case of ensuring interoperability is actually one provision made in US DMCA law (https://www.eff.org/issues/coders/reverse-engineering-faq#faq9)

    - Exposing this information may actually give the project much more exposure and give buyers more certainty as to an alternative channel of local control should the "cloud" services disappear, or a truly open solution is desired. Just think of how much the Realtek TV tuner dongles started selling like hotcakes when the SDR mode became documented and exposed. At present, many DIY 433Mhz home automation uses cheap OOK/ASK fixed-code style devices which are vulnerable to replays and may not be quite satisfactory, and this could become an alternative for them.

    - As I have come to realize, even if you put the information out there, only those knowledgeable enough would find a use for it, and regardless, anyone commercially motivated would buy one and analyze it themselves, especially because of the low price. Ultimately, security through obscurity is recognized as a weak defense.

     

    Of course, if you're being nice to them, withholding the information until later might be a good idea, but I'll leave that to you to decide. I look forward to seeing the results anyhow, even though I'll probably hold off until it actually gets released. I've been reviewing the OSRAM LIGHTIFY and Belkin WeMo Switch systems, each with their own advantages and limitations, and running more "disjoint" home automation systems would sort of defeat the whole idea of a "one stop" app to control the house image. The low price is rather tempting, although I suppose the reliability and safety/quality of the internals might be worth assessing too, and I wonder just how close to the target price they will actually launch for. In theory, these things shouldn't be too expensive given the components that are inside, but the cost of running the cloud services for the life of the system might work against them.

     

    Judging from the links you've given, it's probably some sort of rolling code chip giving enhanced security, which would be a feature but also makes 433Mhz interoperability potentially more difficult (maybe needing to hook up a "gutted" clone remote to succeed, rather than just an ASK/OOK module to a GPIO pin or the like).

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kas.lewis
    kas.lewis over 10 years ago in reply to Gough Lui

    Hey Gough Lui,

     

    I was hoping to do as much reverse engineering as possible. I was looking into understanding the WiFi side but I can look at the 433MHz side too. As for sniffing I have the RSA306 that we both did Road Tests, it would be great to put that to work image. From my digging online, all the internals are pretty much generic. The 433MHz is a SIP module (RX C6) that is $2 or so on AliExpress and the same with the remote. On the WiFi side I was hoping to sniff the internals (UART, I2C, SPI, etc.) that control the ESP8266EX but I need an isolator first just to be sure I don't fry my Logic Analyzer, I was also going to try WireShark and/or the RSA306 to see if there was anything to be pulled out from over the air transmissions but for this I was hoping for a quiet environment, hence starting with the power side as that appeared easier and simpler to start with.. I was also asking if this is ethical/right as I was given this for a review to help promote their product not knock it off.

     

    In the end I will most likely post all my findings as I believe it will be of interest and value to the E14 community.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to kas.lewis

    Thanks for the reply kas.lewis, and well understood on the power thing - to be honest, I never even got that far in my Engineering studies before I had moved over to a different stream, so a lot of my knowledge comes from self-education and observation, so it's a bit of a shame I can't explain it any more intuitively.

     

    Anyhow, I did have another thought, if you should have the equipment necessary (namely an RTL-SDR dongle, or something similar), you might want to examine how the 433Mhz transmissions actually work. Are they ASK/OOK, or FSK data? Are they rolling code or static code (i.e. vulnerable to replay)? This may have big bearings on those wishing to use 433Mhz instead for automation (e.g. the Pilight guys), or those wanting safety against neighbours causing interference or maliciously replaying captured signals to confuse your devices. I suspect the need to push the button indicates it's a rolling-code type devices (similar to those used in garage doors), in which case, knowing the chipset, or type of rolling code may make purchasing alternative "compatible" remote controls easier, although this is also up to the device to support multiple remotes (e.g. some garage doors can do up to eight, and others less).

     

    Keep up the good work image.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kas.lewis
    kas.lewis over 10 years ago in reply to Gough Lui

    Hello Gough Lui,

     

    I have read your comment a few times, to be sure I understand everything, power was not my most enjoyable subject in Uni even if it was always obviously important. I will look into other possibilities in getting more accurate measurements and if those other possibilities can be brought to fruition. I thank you for the timing of your response because I had done some measurements on a few other devices (digital timer, mechanical timer, cellphone charger) and was looking to compile that in a bit but I will reconsider for now.

     

    As for your comment on Arms, you can see the current spiking periodically with teh multimeter (I took a video of that as that was something I wanted to talk about), presumably when the WiFi is woken up. but I do hear the power factor issue and as I have mentioned I will look into a way that I may be able to get better measurements.

     

    Also for missing data, I used a spreadsheet (Excel) to look for duplicate time stamps between the two measurements and then  removed all those that were not duplicated. Then measurements from the same second (understandably not from the same moment) where used to arrive at the power. Having two data logging meters for this was usefull, but as you have pointed out it does have its limitations.

     

    Thankfully

    Kas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>