Internet of Things
  • Technologies
  • More
Internet of Things
Blog Linux commands can turn a log into structured data (turn a TTN Gatesway log into a csv)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 20 Jan 2024 9:18 PM Date Created
  • Views 3344 views
  • Likes 8 likes
  • Comments 13 comments
  • ttn
  • the_things_network
  • gateway
  • linux
Related
Recommended

Linux commands can turn a log into structured data (turn a TTN Gatesway log into a csv)

Jan Cumps
Jan Cumps
20 Jan 2024
Linux commands can turn a log into structured data (turn a TTN Gatesway log into a csv)

A bit of Linux play. How to turn an active unstructured log file into structured data.
image source: nightcafe

Like many programs, my The Things Network Gateway generates a verbose log file. A lot of information. Every so many (> 1000) lines, there is data that I want to track: when a Thing sends data to my Gateway. I want to use that data while the log is actively written to by the Gateway.
image

Line of interest (click to zoom):
image
I want to capture lines with that structure. The rest of the log (the vast majority) is not what I want to retrieve and process.

This is what I want to get out of that active log. Both on the console and in a .csv file:
image

rules

  • I only want to track Things that contact my gateway.
    I can filter relevant lines that have this unique text (bold): 
    Jan 20 19:54:22 raspberryttn lora_pkt_fwd[23528]: INFO: Received pkt from mote: 260BCF0F (fcnt=0)
  • I am interested in the red parts: date and time, Thing identifier and message counter
  • These values should be written to a .csv file, with ';' as separator. And to the console.
  • Everything else should be ignored

Here is a Linux command line that will do this. I will break it apart in this post.
Where you see BAR, it is actually var. The e14 forum does not accept slash var slash.
This is one single command. The \ allows me to show it in 4 lines and make it fit to screen.

stdbuf -o0 tail -f /BAR/log/lora_pkt_fwd.log 2> /dev/null | \
stdbuf -i0 -o0 awk '/: INFO: Received pkt from mote:/ {print $1, $2, $3, $11,$12}' | \
stdbuf -i0 -o0 cut -d ' ' -f 1,2,3,4,5 --output-delimiter=';' | \
stdbuf -i0 -o0 sed 's/(fcnt=//g' | \
stdbuf -i0 -o0 sed 's/)//g' | \
stdbuf -i0 -o0 tee output.csv

It's a pipeline:

  • tail -f keeps reading the log file as it is written. It streams every new line that's written to the log.
    The 2> /dev/null part takes care that I only forward log file content. Warnings and errors (E.g: when the log is being rotated by Linux every week) are ignored.
  • awk finds relevant lines and retrieves the fields that we need (date, time, identifier, counter). Any line that doesn't match our pattern is ignored.
  • cut changes the separator from a space to semicolon
  • sed: called twice to remove fixed text in the counter field that I don't want
  • tee sends the stream both to the standard out (console) and a csv file.
  • stdbuf -i0 -o0 (or stdbuf -o0): I disabled buffering. Used before every command in the pipeline. I want to real-time extract events as they are happening.
    If I would process a megabyte log file at once, I would not use these. But I want to get every event as it is happening.

The output is a structured (character separated values)  file. 

Jan;20;21:34:47;D3FB2208;4938
Jan;20;21:35:52;0030D318;475
Jan;20;21:45:52;0030D318;476
Jan;20;21:46:52;A6BC7955;29136
Jan;20;21:54:52;260BCF0F;1
Jan;20;21:54:52;260BCF0F;2
Jan;20;21:56:22;0030D318;477
Jan;20;21:57:22;7D42C57D;20388
Jan;20;21:58:48;0048BAB4;802
Jan;20;21:58:48;2601643B;53122
Jan;20;22:05:34;0030D318;478
Jan;20;22:16:44;0030D318;479
Jan;20;22:16:44;FF007FF8;84
Jan;20;22:21:53;179BEEF2;50279
Jan;20;22:26:23;0030D318;480
Jan;20;22:35:53;0030D318;481

A different process can pipe this output into a processor script. This could be a database writer, an mqtt publisher, or a program that flashes an LED when an upload is received.

This is performant. I'm running it on a Pi 3. And it uses virtually no resources.
image
If I replace the tail command (reading only what gets added to the log by the gateway) with a cat command (dumping a full 40 Mb log into the pipeline), it finishes in a second.

why this way?

  • non-intrusive: Every command is standard Linux
  • non-intrusive. The command accepts the log file of the Gateway as-is. No software changes.
  • non-intrusive. Does not require additional installs.
  • non-intrusive. This isn't a program, or a shell script. It's just a command.
  • non-intrusive. Can be run by a generic user. No sudo needed.
  • the output file is also streamable in other processes. It can be consumed (E.g.: by another tail command) while this command is writing to it.

image
image: one process parses the raw Gateway log. A second process monitors the structured csv file in parallel.

  • Sign in to reply
Parents
  • balajivan1995
    balajivan1995 over 2 years ago

    Hi,

    Have you tried pasting the script in GitHub gist and embedding here?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to balajivan1995

    I'd rather have e14 allow common Raspberry Pi Linux commands. Everything in this post is innocent. I raised a support request for it a few weeks ago:  forum doesn't accept post with linux commands and config content 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps

    In this post, I finally settled for posting code as bitmaps. Because I couldn't get it posted:  

     Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 3: manage the service log size 

    Again - nothing in that post was harmful. Just processing log files of a common Raspberry Pi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps

    In this post, I finally settled for posting code as bitmaps. Because I couldn't get it posted:  

     Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 3: manage the service log size 

    Again - nothing in that post was harmful. Just processing log files of a common Raspberry Pi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balajivan1995
    balajivan1995 over 2 years ago in reply to Jan Cumps

    I saw their reply about security concerns. Maybe that's why they have included the option to insert GitHub gists as well. We can't blame the devsecops team for doing their job anyway.. Although, their spam video detector does requires some improvement..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to balajivan1995

    I should be able to post any Linux command. As long as it does not harm the reader's PC when they browse and read the page.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balajivan1995
    balajivan1995 over 2 years ago in reply to Jan Cumps

    I wholeheartedly agree with you, in some cases var path also stores html content, that's why they are hesitating I guess. They are prohibiting for the same reason some special characters are not allowed in username and password.

    I am not sure what can be done about this, considering moderator explicitly stated there's no plan to fix this issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to balajivan1995

    Let's continue Linux command post issues in the bug report  forum doesn't accept post with linux commands and config content 

    I am not sure what can be done about this, considering moderator explicitly stated there's no plan to fix this issue

    It should be fixed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balajivan1995
    balajivan1995 over 2 years ago in reply to Jan Cumps

    Made a comment with GitHub gist, it went to moderation.

    I thought the mod warning was due to including the path name in gist, made one more comment about it. That also went to moderation.