Internet of Things
  • Technologies
  • More
Internet of Things
Blog Single Channel LoRa Gateway using Wio E5 LoRa and Blynk
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: vinayyn
  • Date Created: 18 Feb 2023 5:34 PM Date Created
  • Views 38760 views
  • Likes 10 likes
  • Comments 6 comments
  • LoRa E5
  • Seeed studio Wio E5
  • blynk
Related
Recommended

Single Channel LoRa Gateway using Wio E5 LoRa and Blynk

vinayyn
vinayyn
18 Feb 2023

imageimageimage

In LoRa based system we can transmit the information to Another LoRa, then we can use that information and display it on the Local LCD Display or somewhere. if we need the data to be transmitted far longer distances than the LoRa Coverage? What do we have to do?

There are two methods available here

  1. If any other networks(4G,2G,3G) are available in the particular area we can use LoRa Gateways.
  2. If there are no networks available, we can use the Another LoRa Module as Repeaters

The Above Two methods have their Respective Advantages and Disadvantages.

The LoRaWAN Gateways are Not pocket friendly and Requires Subscriptions to connect the devices and transfer data to the cloud.

The LoRa Repeaters Implementation Requires More Number Transceiver modules to Transfer the data to the Receivers. And it can’t store details on the cloud it can store the data locally.

In this Project, I am building  Single channel LoRa gateway using Seeed studio Wio-E5 Module, ESP8266, And Blynk.

Before briefly  Explaining, Let's know a few basics about LoRafollow the link to learn more about What are LoRa® and LoRaWAN®?

LoRaWAN Gateways are one of four key components of the LoRa network architecture:

  1. End Nodes– Represents edge devices or sensors
  2. Gateway – Collects or concentrates data from several end nodes
  3. Network Server – Consolidates data from gateways for upload to the application server
  4. Application Server – Processes or displays consolidated data

Let's know more about the Seeed studio Wio-E5 LoRa module.

Wio-E5 is a low-cost, ultra-low power, extremely compact, and high-performance LoRaWAN® Module designed by Seeed Technology Co., Ltd. It contains ST system-level package chip STM32WLE5JC, which is the world's first SoC integrated with the combo of LoRa® RF and MCU chip. For More detailed Information on the LoRa-E5 Visit https://www.seeedstudio.com/LoRa-E5-Wireless-Module-p-4745.html

image

This module is also embedded with ARM Cortex M4 ultra-low-power MCU and LoRa® SX126X and therefore supports (G)FSK mode and LoRa®. 62.5kHz, 125kHz, 250kHz, and 500kHz bandwidth can be used in LoRa® mode, making it suitable for the design of various IoT nodes, supporting EU868 and US915.

This Wio E5 module is designed with industrial standards, hence it's highly suitable to be used in designing industrial IoT products, with a wide working temperature at -40℃ ~ 85℃.

Features

  • Ultra-low Power Consumption: as low as 2.1uA sleep current (WOR mode)
  • Extremely Compacted Size: 12mm * 12mm * 2.5mm 28 pins SMT
  • High Performance: TXOP=22dBm@868/915MHz; -136.5dBm sensitivity for SF12 with 125KHz BW
  • Long Distance Use: 158dB link budget
  • Wireless Connectivity: Embedded LoRaWAN® protocol, AT command, support global LoRaWAN® frequency plan
  • Worldwide Compatibility: wide frequency range; EU868 / US915 / AU915 / AS923 / KR920 / IN865
  • Great Flexibility: For users who want to develop software on the MCU of the module, other GPIOs of the MCU can be easily manipulated, including UART, I2C, ADC, etc. These rich GPIO interfaces are useful for users who need to expand peripherals.

    Simple Comparisons Of LoRa E5 and RFM95

    image

Here I am using Wio-E5 Factory AT Firmware to communicate with Host Microcontroller. Let's start learning with the AT Commands.

Wio-E5 series has a built-in AT command firmware, which supports LoRaWAN® Class A/B/C protocol and a wide frequency plan: EU868/US915/AU915/AS923/KR920/IN865. With this AT command firmware, developers can easily and quickly build their prototype or application.

The AT command firmware contains a bootloader for DFU and the AT application. The "PB13/SPI_SCK/BOOT" pin is used to control Wio-E5 to stay in the bootloader or jump to the AT application. When PB13 is HIGH, the module will jump to AT application after reset, with a default baud rate of 9600. When PB13 is LOW (press the "Boot" button on Wio-E5 mini/ Wio-E5 Development Kit), the module will stay in the bootloader, and keep transmitting a "C" character every 1S at baud rate 115200.

AT Commands

All command lines must start with "AT" and end with a carriage return character. We will use <CR> to represent a carriage return character

  • The command is case insensitive
  • All commands have a response
  • Command length never exceeds a total of 528 characters
  • One valid AT Command must end with '\n', "\r\n" is also valid
  • If the command timeout feature is enabled, end '\n' will not be mandatory
  • means the newline character. means carriage return
  • UART2 configuration "9600, 8, n 1" (8 bits data, no parity, 1 stop bit);

AT Commands Symbols

 

Symbol

Meaning of the symbols In the AT mode

=

Set value for the command

?

Query

:

Start a list input parameter

+

Prefix of command

,

Separator of parameters

Space

An empty character could be used to format the command

 

AT Commands Format

All commands in this document end with<CR><LF>. To facilitate the description, all is intentionally omitted in this document.  <CR> and <LF> represent a carriage return character and a linefeed character respectively. 

 

Query Commands

query command to check LoRaWAN modem configuration, such as channel configuration, ADR status, TX power, etc.

Example:    AT+MODE=? //Querying the mode of work

Configure / Control

configure/control command to set new configuration or control transaction.

 

RETURN Data

Return data is in the format like "+CMD: RETURN DATA"

Example      +MODE: TEST

AT Commands

Command

Description

AT

Test command

HELP

Print command list

FDEFAULT

Factory data reset

RESET

Software reset

DFU

Force the bootloader to enter dfu mode

LOWPOWER

Enter sleep mode

VER

Version[Major.Minor.Patch]

MSG

LoRaWAN unconfirmed data

MSGHEX

LoRaWAN unconfirmed data IN HEX

CMSG

LoRaWAN confirmed data

CMSGHEX

LoRaWAN confirmed data in hex

PMSG

LoRaWAN proprietary

PMSGHEX

LoRaWAN proprietary in hex

CH

LoRaWAN channel frequency

DR

LoRaWAN data rate

ADR

LoRaWAN ADR control

REPT

Unconfirmed message repetition

RETRY

Confirmed message retry

POWER

LoRaWAN TX power

RXWIN2

LoRaWAN RX window2

RXWIN1

Customized RXWIN1 frequency

PORT

LoRaWAN communication port

MODE

LWABP, LWOTAA, TEST

ID

LoRaWAN DevAddr/DevEui/AppEui

KEY

Set NWKSKEY/APPSKEY/APPKEY

CLASS

Choose LoRaWAN modem class(A/B/C)

JOIN

LoRaWAN OTAA JOIN

LW

LoRaWAN misc configuration (CDR, ULDL, NET, DC, MC, THLD)

TEST

Send test serious command

UART

UART configure

REG

Control RF Chip

DELAY

RX window delay

VDD

Get VDD

RTC

RTC time get/set

EEPROM

Write/Read EEPROM

Error Codes

This error code list applies to all LoRaWAN-supported commands. Users could refer to this list to know what is happening to the LoRaWAN modem when gets errors.

Code

Description

-1

The number of parameters is invalid

-2

The content of the parameter is invalid

-3

API function returns an error when a user parameter is passed to it

-4

LoRaWAN modem can't save parameters to EEPROM

-5

The command is disabled currently

-6

Unknown error occurs

-7

There is not enough HEAP to execute user operation

-10

Command unknown

-11

The command is in the wrong format

-12

The command is unavailable in current mode (Check with "AT+MODE")

-20

Too many parameters. LoRaWAN modem support max 15 parameters

-21

The length of the command is too long (exceeds 528 bytes)

-22

Receive end symbol timeout, command must end with

-23

Invalid character received

-24

Either -21, -22 or -23

Example: The number of parameters is invalid 

AT+mode=1

+MODE: ERROR(-1)

In the above example, we are getting an Error number of -1, which means we are setting the invalid command.

How to resolve the error: in the at command, it is mentioned when the prefix command is entered respective value need to enter. In the above example, we have to select work mode, based on the work mode command we can only three values LWABP, LWOTAA, and TEST. But the entered value is 1, which means it is not a valid value

Let's enter the Correct value and what will be the Return Data

AT+mode=TEST

+MODE: TEST

AT+mode=LWABP

+MODE: LWABP

AT+mode=LWOTAA

+MODE: LWOTAA

For creating this project I am using Two Wio-E5 Development Kit

Wio E5 Development kit is based on STM32WLE5JC.

image

Wio-E5 Dev Board has a long-distance transmission range of Wio-E5 up to 10km in an open area. The sleep current of Wio-E5 modules on board is as low as 2.1 uA(WOR mode). It is designed with industrial standards with a wide working temperature at -40 ℃ ~ 85℃, high sensitivity between -116.5 dBm ~ -136 dBm, and power output up to +20.8dBm at 3.3V.

Wio-E5 Dev Board also has rich interfaces. Developed to unlock the full functionality of the Wio-E5 module, Wio-E5 Dev Board has led out the full 28 pins of Wio-E5 and provides rich interfaces including Grove connectors, RS-485 terminal, male/female pin headers for you to connect sensors and modules with different connectors and data protocols, saving your time on wire soldering. You could also easily power the board by connecting the battery holder with 2 AA batteries, enabling temporary use when lacking an external power source. It is a user-friendly board for easy testing and rapid prototyping.

Since Wio-E5 is a LoRaWAN® chip with an MCU, there are three main ways to utilize the Wio-E5 Dev Board:

1: Connect Wio-E5 Dev Board to PC via USB and control by AT commands

There is a built-in USB to UART function on board, you could just simply connect the Wio-E5 Dev Board to your PC with a USB type C cable, and use serial communication software to send AT commands and read data from the board

2: Connect Wio-E5 Dev Board to another mainboard via UART and control by AT commands

For example, connect Wio-E5 Dev Board to Seeeduino XIAO and the Expansion Board via UART, send AT commands, and read data from Seeeduino XIAO through Arduino IDE serial monitor.

3: Develop user applications by using SDK

Develop your LoRa® development board with MCU function by using STM32Cube Programmer, which is the SDK officially provided by STMicroelectronics. To download this SDK resource, please find the resources in learning and document down below.

With all the outstanding features listed above, the Wio-E5 Dev Board will be a superior choice for IoT device development, testing, prototyping, and applications in long-distance, ultra-low power consumption IoT scenarios like smart agriculture, smart office, and smart industry.

imageimage

In this project, I will explain only The AT Command which is utilized. For a detailed AT Commands description follow this link

Communicating The LoRa Modules using AT Commands

  • We need two LoRa Module Here to test the basic AT commands require to complete the project.
  • These two modules are connected to the Computer using a Type C USB connector.
  • To send and receive the data we require serial terminal software on the PC.
  • One LoRa Module Is Used as a Transmitter and Another LoRa Module Is used as a receiver to test the AT Commands

Transmitter Side

  1. Enter TEST mode:

TEST command is not like other commands, it is a serious command, and includes several sub-commands, refer to the table below. With test mode, the user could do an RF performance test quickly without any knowledge of the LoRa chip. Commands which are related to RF configuration are disabled in test mode.LWABP7, LWOTAA8, and TEST are supported. LoRaWAN modem can only work with one mode at a time. By default, LWABP is enabled, all test commands are unavailable, and LoRaWAN will return an error(-12) if it receives the test command in non-test mode.

The "AT+MODE" command will reset the LoRaWAN stack when first entering LWABP/LWOTTA mode and reset the LoRa chip when first entering test mode.LWABP/LWOTAA mode status is remembered by the LoRaWAN modem, each time the LoRaWAN modem starts, it will enter the previous working mode before resetting or repower.

Here to test the modules I will select the Test Mode

AT+MODE=TEST

+MODE: TEST  ← once the work mode is successfully configured the return data will indicate the mode we selected.

      ←LoRaWAN Modem Enter Test mode successfully

Test Sub-Command

Sub-command

Comment

HELP

Print test command help information, make LoRa transceiver to standby mode

STOP

Set LoRaWAN Modem to TEST stop mode

TXCW

Transmit continuous wave

TXCLORA

Transmit continuous LoRa signal

RFCFG

Set RF configuration in TEST mode

RXLRPKT

Continuous receive pure LoRa packet, print once there is a new packet received

TXLRPKT

Send one HEX format packet out

TXLRSTR

Send one string format packet

RSSI

Get the RSSI value of the specified channel

LWDL

Send LoRaWAN downlink packet, a useful tool to test CLASS C device

 2. Set RF Configuration: RFCFG supports set frequency, SF, bandwidth, TX preamble, RX preamble, and TX power settings.

TX and RX share all configurations except "preamble length", the user could choose a different preamble length. For LoRa communication, it is strongly recommended to set RX preamble length longer than TX's. Bandwidth only supports 125KHz / 250KHz / 500KHz. Depending on Semtech SX1276 (PA_BOOST/RFO) and the design solution of the module, the MAX output power of different band LoRaWAN modems could be different.

The syntax for RF Configuration

AT+TEST=RFCFG,[FREQUENCY],[SF],[BANDWIDTH],[TX PR],[RX PR],[TX POWER] ,[CRC],[IQ],[NET]

      Where,

                  SF: Spreading Factor

                  TX PR: TX Preamble

                  RX PR: RX Preamble

                  IQ: Inverted IQ

                  NET: Choosing Public Or Private Network

EX: AT+TEST=RFCFG,866,SF12,125,12,15,14,ON,OFF,OFF

+TEST: RFCFG F:866000000, SF12, BW125K, TXPR:12, RXPR:15, POW:14dBm, CRC: ON, IQ: OFF, NET: OFF

FREQUENCY: 866MHz

SpreadFactor: SF12

 Bandwidth: 125KHz

TX Preamble: 12

RX Preamble: 15

Power: 14dBm

3. TX LoRa Packet: After entering test mode, the user could send the LoRa packet through the "AT+TEST=TXLRPKT" sub-command. The command format is like the below:

AT+TEST=TXLRPKT, "AB"

+TEST: TXLRPKT "AB"

+TEST: TX DONE     ← when the data is sent successfully it will acknowledge  as Done              

Command sequence to send LoRa packet:

AT+MODE=TEST /// Set test mode

AT+TEST=? //// Query test mode, check RF configuration

AT+TEST=RFCFG,[FREQUENCY],[SF],[BANDWIDTH],[TXPR],[RXPR],[POW],[CRC],[IQ],[NET]// / Set RF Configuration

AT+TEST=TXLRPKT, "HEX String"// Send HEX format packet

 

Receiver side

On the receiver side, the few basic configuration commands are the same as the transmitter, I will Again List those here.

  1. Enter TEST mode
  2. Set RF Configuration
  3. RX LoRa Packet: After entering test mode, the user could enter LoRa packet continuous RX mode through the RXLRPKT subcommand (AT+TEST=RXLRPK). Like below:

                        AT+TEST=RXLRPKT

                       +TEST: RXLRPKT

            Command sequence to receive LoRa packet:

            AT+MODE=TEST // Set test mode

            AT+TEST=?// Query test mode, check RF configuration

            AT+TEST=RFCFG,866,SF12,125,12,15,14,ON,OFF,OFF//Set RF Configuration

            AT+TEST=RXLRPKT // Enter RX continuous mode

 LoRa Transmitter and Receiver AT Commands Testing

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Now I will give details of the main project, in the transmitter part I am using XIAO SAMD21 Microcontroller, Wio E5 LoRa Dev Kit, SI7051 temperature sensor, and MPU 6050 Accelerometer gyroscope sensors, along with the 2X AA Battery .in the receiver part I am using Wio E5 LoRa Dev Kit, ESP8266 NodeMCU, OLED Display.

The transmitter part collects the temperature details, accelerometer, and gyroscope sensor collects the various movements of the device. if there is a change in the Position of the transmitter, the microcontroller transfers the alert data to the receiver using LoRa along with the surrounding temperature details. The transmitter Part is powered by two AA Size batteries that can run the transmitter for up to a couple of months.

image

Fig . Transmitter Section Block Diagram

 image

Fig. Transmitter section connection diagram

In the receiver part The LoRa receives the data and the microcontroller processes the data and then displays the data in OLED Display. In Parallel transfers the details to the Blynk cloud servers using Wi-Fi to display them in the android app. The android app will display the Temperature, position of the Transmitter, RSSI, and Status of the Transmitter and Receiver connection.

image

 Fig. Receiver Block diagram

image

Fig Receiver Connection Diagram

 Project Demo Video

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Transmitter Code

#include <Arduino.h>
#include <Wire.h>
#include "ClosedCube_Si7051.h"
#include "MPU6050.h"
ClosedCube_Si7051 si7051;
MPU6050 accelgyro;
#if I2CDEV_IMPLEMENTATION == I2CDEV_ARDUINO_WIRE
#include "Wire.h"
#endif

int data1=0;
int data2=0;
int data3=0; 
int data4=0; 
int16_t ax, ay, az;
int16_t gx, gy, gz;
#define OUTPUT_READABLE_ACCELGYRO
static char recv_buf[512];
static bool is_exist = false;
int a_x,a_y,a_z;

static int at_send_check_response(char *p_ack, int timeout_ms, char *p_cmd, ...)
{
    int ch = 0;
    int index = 0;
    int startMillis = 0;
    va_list args;
    memset(recv_buf, 0, sizeof(recv_buf));
    va_start(args, p_cmd);
    Serial1.printf(p_cmd, args);
    Serial.printf(p_cmd, args);
    va_end(args);
    delay(200);
    startMillis = millis();
 
    if (p_ack == NULL)
    {
        return 0;
    }
 
    do
    {
        while (Serial1.available() > 0)
        {
            ch = Serial1.read();
            recv_buf[index++] = ch;
            Serial.print((char)ch);
            delay(2);
        }
        if (strstr(recv_buf, p_ack) != NULL)
        {
            return 1;
        }
    } while (millis() - startMillis < timeout_ms);
    return 0;
}
 
static int node_send(uint32_t timeout)
{
   
    static uint16_t count = 0;
    int ret = 0;
    char data[32];
    char cmd[128];
    
    memset(data, 0, sizeof(data));
    sprintf(data, "%04X,%04X,%04X,%04X", data1, data2, data3,data4);
    sprintf(cmd, "AT+TEST=TXLRPKT,\"5345454544%s\"\r\n", data);
    ret = at_send_check_response("TX DONE", 2000, cmd);
    if (ret == 1)
    {
        Serial.print("Sent successfully!\r\n");
    }
    else
    {
        Serial.print("Send failed!\r\n");
    }
    data1 = si7051.readTemperature();
    data2 = a_z;
    data3 = 100;
    data4 = 200;
    
    return ret;
}
 
void setup(void)
{
    Serial.begin(115200);
    si7051.begin(0x40); // default I2C address is 0x40 and 14-bit measurement resolution
    Serial1.begin(9600);
    #if I2CDEV_IMPLEMENTATION == I2CDEV_ARDUINO_WIRE
        Wire.begin();
    #elif I2CDEV_IMPLEMENTATION == I2CDEV_BUILTIN_FASTWIRE
        Fastwire::setup(400, true);
    #endif
    accelgyro.initialize();
    uint16_t error;
    char errorMessage[256];
     if (at_send_check_response("+AT: OK", 100, "AT\r\n"))
    {
        is_exist = true;
        at_send_check_response("+MODE: TEST", 1000, "AT+MODE=TEST\r\n");
        at_send_check_response("+TEST: RFCFG", 1000, "AT+TEST=RFCFG,866,SF12,125,12,15,14,ON,OFF,OFF\r\n");
        delay(200);
    }
    else
    {
        is_exist = false;
        Serial.print("No E5 module found.\r\n");
    }
     
}
 
void loop(void)
{
    accelgyro.getMotion6(&ax, &ay, &az, &gx, &gy, &gz);
    Serial.print("Sensor data");
    Serial.print(ax);
    Serial.print(",");
    Serial.print(ay);
     Serial.print(",");
     Serial.print(az);
    Serial.println();

    a_x = (ax+ay+az);
    a_y = sqrt(a_x);
    a_z = ((az)/ay);
   
    Serial.print("x:");
    Serial.print(a_z);
    Serial.println();
      
    if (is_exist)
    {
        node_send(2000);
        delay(500);    
    }
}

 Receiver Code

#include <Arduino.h>
#define BLYNK_TEMPLATE_ID "Your Blynk Template ID"
#define BLYNK_DEVICE_NAME "Your Blynk Device Name"
#define BLYNK_PRINT Serial
#include <ESP8266WiFi.h>
#include <BlynkSimpleEsp8266.h>
#include <Wire.h>
#include <Adafruit_GFX.h>
#include <Adafruit_SSD1306.h>
#include <SoftwareSerial.h>
static char recv_buf[512];
static bool is_exist = false;
int RXPin = D6;
int TXPin = D5;
SoftwareSerial E5(RXPin, TXPin);
#define SCREEN_WIDTH 128 // OLED display width, in pixels
#define SCREEN_HEIGHT 64 // OLED display height, in pixels
Adafruit_SSD1306 display(SCREEN_WIDTH, SCREEN_HEIGHT, &Wire, -1);
char auth[] = "Blynk Device authentication code";
char ssid[] = "Your Wi-Fi Name";
char pass[] = "Your Wi-Fi Password";
BlynkTimer timer;
WidgetLCD lcd(V1);
WidgetLCD lcd2(V3);
//////////////////////////////////////////////////////////////////////////////////////////
static int at_send_check_response(char *p_ack, int timeout_ms, char *p_cmd, ...)
{
int ch = 0;
int index = 0;
int startMillis = 0;
va_list args;
memset(recv_buf, 0, sizeof(recv_buf));
va_start(args, p_cmd);
E5.printf(p_cmd, args);
Serial.printf(p_cmd, args);
va_end(args);
delay(200);
startMillis = millis();

if (p_ack == NULL)
{
return 0;
}
do
{
while (E5.available() > 0)
{
ch = E5.read();
recv_buf[index++] = ch;
Serial.print((char)ch);
delay(2);
}


  
if (strstr(recv_buf, p_ack) != NULL)
{
return 1;
}
} 
while (millis() - startMillis < timeout_ms);
return 0;
}

////////////////////////////////////////////////////////////////////

static int recv_prase(void)
{
char ch;
int index = 0;
memset(recv_buf, 0, sizeof(recv_buf));
while (E5.available() > 0)
{
ch = E5.read();
recv_buf[index++] = ch;
Serial.print((char)ch);
delay(2);
}
 
if (index)
{
char *p_start = NULL;
char data[32] = {
0,
};
int rssi = 0;
int snr = 0;
p_start = strstr(recv_buf, "+TEST: RX \"5345454544");
if (p_start)
{
p_start = strstr(recv_buf, "5345454544");
if (p_start && (1 == sscanf(p_start, "5345454544%s,", data)))
{
data[16] = 0;
int data1,data2,data3,data4;
char *endptr,*endptr1,*endpt2,*endptr3;

char dataarray1[5] = {data[0], data[1],data[2], data[3]};
char dataarray2[5] = {data[4], data[5], data[6], data[7]};
char dataarray3[5] = {data[8], data[9], data[10], data[11]};
char dataarray4[5] = {data[12], data[13],data[14], data[15]};

data1 = strtol(dataarray1, &endptr, 16);
data2 = strtol(dataarray2, &endptr1, 16);
data3 = strtol(dataarray3, &endptr, 16);
data4 = strtol(dataarray4, &endptr1, 16);
lcd2.clear(); 
Serial.print("data1:");
Serial.print(data1);
Serial.println();
Serial.print("data2:");
Serial.print(data2);
Serial.println();
Serial.print("data3:");
Serial.print(data3);
Serial.println();
Serial.print("data received displaying on the wio terminal");
Serial.print("\r\n");
display.setTextSize(1);
display.setTextColor(WHITE);
display.setCursor(0, 0);
display.print("Temperature:");
display.print(data1);
display.print(" C");
Blynk.virtualWrite(V0,data1);

if(data2 <=10)
{
  display.setCursor(0,20);
  display.print("The device Position  had Changed");
  lcd.clear(); //Use it to clear the LCD Widget
  lcd.print(0, 0, "The device Posi"); // use: (position X: 0-15, position Y: 0-1, "Message you want to print")
  lcd.print(0, 1, "tion had Changed"); // use: (position X: 0-15, position Y: 0-1, "Message you want to print")  
}
else
{
  display.setCursor(0,20);
  display.print("The device is in a   constant position");
  lcd.clear(); //Use it to clear the LCD Widget
  lcd.print(0, 0, "The device is in"); // use: (position X: 0-15, position Y: 0-1, "Message you want to print")  
  lcd.print(0, 1, "constant position"); // use: (position X: 0-15, position Y: 0-1, "Message you want to print")  
}
}
p_start = strstr(recv_buf, "RSSI:");
if (p_start && (1 == sscanf(p_start, "RSSI:%d,", &rssi)))
 {
String newrssi = String(rssi);
Serial.print(rssi);
Serial.print("\r\n");
Blynk.virtualWrite(V2,newrssi);
display.setCursor(0,50);
display.print("RSSI:");
display.print(rssi);
display.print(" dB");
display.display(); 
delay(100);
display.clearDisplay();
}

 p_start = strstr(recv_buf, "SNR:");
if (p_start && (1 == sscanf(p_start, "SNR:%d", &snr)))
{
Serial.print(snr);
Serial.print("\r\n");
}
return 1;
}
}
return 0;
}
 

/////////////////////////////////////////////////////////////////////////////
static int node_recv(uint32_t timeout_ms)
{
at_send_check_response("+TEST: RXLRPKT", 1000, "AT+TEST=RXLRPKT\r\n");
int startMillis = millis();
do
{
if (recv_prase())
{
return 1;
}
} 

while (millis() - startMillis < timeout_ms);
Serial.print("No data");
Serial.println("");
display.clearDisplay();
display.setCursor(0,50);
display.print("Transmitter Not found");
display.display(); 
lcd.clear(); 
lcd2.clear(); //Use it to clear the LCD Widget
lcd2.print(0, 0, "Transmitter Not"); // use: (position X: 0-15, position Y: 0-1, "Message you want to print")
lcd2.print(0, 1, "Found"); // use: (position X: 0-15, position Y: 0-1, "Message you want to print")  
Blynk.virtualWrite(V0,0);
Blynk.virtualWrite(V2,0);
return 0;
//

}

/////////////////////////////////////////////////////////
void setup() {
Serial.begin(9600);
Blynk.begin(auth, ssid, pass);
if(!display.begin(SSD1306_SWITCHCAPVCC, 0x3C))
 {
Serial.println(F("SSD1306 allocation failed"));
for(;;);
}
delay(2000);
display.clearDisplay();
E5.begin(9600);
Serial.print("Receiver\r\n");
    
if (at_send_check_response("+AT: OK", 100, "AT\r\n"))
{
is_exist = true;
at_send_check_response("+MODE: TEST", 1000, "AT+MODE=TEST\r\n");
at_send_check_response("+TEST: RFCFG", 1000, "AT+TEST=RFCFG,866,SF12,125,12,15,14,ON,OFF,OFF\r\n");
delay(200);
}
else
 {
is_exist = false;
Serial.print("No E5 module found.\r\n");
}
}
 



void loop()
{
if (is_exist)
{
node_recv(2000);
}
Blynk.run();
timer.run();
}

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 3 years ago +1
    Hi, There's a typo: "I n this Project, I am building Single channel LoRaWAN gateway using Seeed studio Wio-E5 Module, ESP8266, And Blynk " should be replaced with: "I n this Project, I am building…
  • ralphjy
    ralphjy over 3 years ago +1
    Nice tutorial . I’ve used the Grove Wio E5 module with a Wio Terminal and it works great with my Things Network gateway. Best part is that Seeed provides the firmware to automate the setup as part of…
Parents
  • shabaz
    shabaz over 3 years ago

    Hi,

    There's a typo:

    "In this Project, I am building  Single channel LoRaWAN gateway using Seeed studio Wio-E5 Module, ESP8266, And Blynk"

    should be replaced with:

    "In this Project, I am building  Single channel LoRa gateway using Seeed studio Wio-E5 Module, ESP8266, And Blynk"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 3 years ago

    Hi,

    There's a typo:

    "In this Project, I am building  Single channel LoRaWAN gateway using Seeed studio Wio-E5 Module, ESP8266, And Blynk"

    should be replaced with:

    "In this Project, I am building  Single channel LoRa gateway using Seeed studio Wio-E5 Module, ESP8266, And Blynk"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to shabaz

    (The blog post refers to LoRaWAN frequently, but then the project proceeds to use test mode to send/receive wireless packets that are nothing to do with LoRaWAN, so it's pretty confusing).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to shabaz

    (Can't edit) It refers to LoRaWAN 42 times! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vinayyn
    vinayyn over 3 years ago in reply to shabaz

    I have changed the error