Internet of Things
  • Technologies
  • More
Internet of Things
Blog Suggestion needed for a IoT solution
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 29 Jun 2015 8:41 AM Date Created
  • Views 1629 views
  • Likes 0 likes
  • Comments 3 comments
  • sensors
  • internet_of_things
  • iot
Related
Recommended

Suggestion needed for a IoT solution

e14 Contributor
e14 Contributor
29 Jun 2015

Hello i am developing a IoT product.

basically there are lot of nodes separated by 100-200metre apart. they are battery operated by 2100mah AA alkaline battery. and i want the life to be 6-8 month on each charge cycle.

The sensor node consumes 30-50ma for getting data from the sensors, and i need to tx it for 1sec every one hour, and i need a mesh kind of network,.

It seems sub GHZ will help in this scenario, still confused on which chip i should go./

 

Found several chips from Ti,SiLabs,Freescale,Atmel.

 

Anyone suggest me a best chip-set for my application. footprint doesn't matter.

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    I have used the TI Sub 1GHz and they work very well and are reliable and well supported, you can et a pair from TI / Newark for about 20$ as Booster packs, they come with an MSP430 CPU each as well so…
Parents
  • BigG
    BigG over 11 years ago

    Assuming your 100-200m spaced nodes are not in a built-up urban environment, then suggest this little 433MHz module, which is available from seeedstudio:

    http://www.seeedstudio.com/depot/433Mhz-Wireless-Serial-Transceiver-Module-1-Kilometer-p-1733.html?cPath=19_22

    It is fairly easy to use as it communicates via UART/TTL (3V-5V) through it's embedded mcu and uses AT commands to set radio configuration options. There are 3 operating modes, one of which is a low power consumption option during TX, and has low power sleep option. Not so sure about the 1km claim, but when I used with a quarter monopole whip antenna, I was able to communicate at the +100m range (not that my tests were in way scientific).

     

    Otherwise maybe look at si4463 transceivers. Suggest searching https://www.tindie.com for some ready made modules.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • BigG
    BigG over 11 years ago

    Assuming your 100-200m spaced nodes are not in a built-up urban environment, then suggest this little 433MHz module, which is available from seeedstudio:

    http://www.seeedstudio.com/depot/433Mhz-Wireless-Serial-Transceiver-Module-1-Kilometer-p-1733.html?cPath=19_22

    It is fairly easy to use as it communicates via UART/TTL (3V-5V) through it's embedded mcu and uses AT commands to set radio configuration options. There are 3 operating modes, one of which is a low power consumption option during TX, and has low power sleep option. Not so sure about the 1km claim, but when I used with a quarter monopole whip antenna, I was able to communicate at the +100m range (not that my tests were in way scientific).

     

    Otherwise maybe look at si4463 transceivers. Suggest searching https://www.tindie.com for some ready made modules.