Internet of Things
  • Technologies
  • More
Internet of Things
Blog Texas Instruments CC11XL Wireless Connectivity Development Kit – Photos
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 27 Aug 2014 2:53 AM Date Created
  • Views 1830 views
  • Likes 0 likes
  • Comments 3 comments
  • RoadTest
  • cc110l
  • ioe
  • sub-1ghz
  • internet_of_everything
  • boosterpack
  • internet_of_things
  • sub-ghz
  • cc11xldk-868-915
  • texas_instruments
  • cc11xl
  • iot
  • wireless
  • internet_of
  • launchpad
  • ti
  • anaren
Related
Recommended

Texas Instruments CC11XL Wireless Connectivity Development Kit – Photos

shabaz
shabaz
27 Aug 2014

This blog post is part of a collection, click here for links to the entire set, and a review of the products.

Introduction

The TI CC11XL Development KitTI CC11XL Development Kit arrived today as part of an Agilent and TI roadtest, so I decided to take some photos and a quick video before examining it further.

image

 

This development kit is ideal if you want to create wireless connectivity solutions. It allows you to experiment with the transceivers, try out the built-in software with in-built sensors, and prototype your own code using the supplied programmer/debugger.

 

CC11xL Integrated Circuits

TI has a vast variety of development kits and evaluation boards, and they can be considered to be essential to enable rapid solution development. They are an opportunity to quickly try out software and hardware, and try out your own changes, while being assured that the supplied hardware and software are a high quality reference design.

 

There is lots of information to glean from the designs, and the supplied schematics and board layouts help immensely.

 

The CC11XL development kit is intended to help create solutions using TI’s CC11xL series devices and the kit comes enabled with CC110L, CC113L and CC115L devices. The first is a transceiver IC, and the other two are receiver and transmitter chips respectively.

 

Texas Instruments has a vast array of wireless connectivity devices – see www.ti.com/wireless for details. The sub-Gigahertz wireless options include a ‘Performance Line’ and a ‘Value Line’. The CC11xL products fall into the Value Line category and are intended for cost-sensitive applications such as home automation, alarm systems and remote control.

 

Development Kit

The CC11XLDK-868-915 is a full development kit, but, as a side note, there are lower-cost options to get moving with the CC10xL family if required. There are small modules by Anaren which contain the CC110L on-board. There are also ‘BoosterPack’ boards which contain the Anaren module on a PCB with 0.1 inch headers. These BoosterPack boards could be soldered onto a stripboard, or can be plugged on top of TI ‘LaunchPad’ boards which are compact microcontroller development boards much like Arduino boards. The photo below shows some of this LaunchPad and BoosterPack ecosystem.

image

 

The full development kit is still extremely good value however. It saves a huge amount of time and effort and is therefore a small price to pay for such a comprehensive kit to quickly get a project developed. We have purchased a variety of these for work, and they all contain a pair of base boards known as a Transceiver Evaluation Boards (TrxEB) which include an on-board microcontroller and LCD display (and 2xAA battery holders around the back). The development kits ship with the wireless devices on daughter cards (known as Evaluation Modules) that plug onto the TrxEB. The kit also includes an MSP430 programmer/debug tool (unfortunately it’s not the latest MSP-FET model, but still a very handy thing to have) so that you can write and debug custom programs to run on the TrxEB boards or on your own circuit boards.

 

If you want to try out a different chip, you don’t need to re-purchase an entire development kit if you feel you have enough TrxEB base boards. You can just buy individual Evaluation Modules (i.e. daughter cards).

 

Here is a photo of the front and underside of the two CC110L evaluation modules that are part of the development kit:

image

 

Close-up view of the circuitry:

image

 

This photo shows the programmer/debugger and the cables that are supplied with the kit.

image

 

A Quick Test

Finally, here is a video showing the out-of-the-box experience. There are pre-loaded demonstrations on the board. This video shows the packet error rate (PER) test.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Summary

This has just been a very brief look at the wireless connectivity development kit for the CC11xL series of integrated circuits from Texas Instruments. More to come soon.

  • Sign in to reply
Parents
  • vish
    vish over 12 years ago

    Seems like it took 2+ months for the shipment to reach youimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to vish

    https://www.youtube.com/watch?v=3K7pVYo9jM8

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 12 years ago in reply to vish

    https://www.youtube.com/watch?v=3K7pVYo9jM8

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • vish
    vish over 12 years ago in reply to shabaz