Internet of Things
  • Technologies
  • More
Internet of Things
Blog What's new in Raspberry Pi 4?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: James_Smith
  • Date Created: 19 Nov 2024 7:09 AM Date Created
  • Views 2759 views
  • Likes 2 likes
  • Comments 3 comments
  • raspberry
  • arduino ide
  • raspberry pi 4
  • raspberry_pi
  • raspberry pi
  • raspberri pi
Related
Recommended

What's new in Raspberry Pi 4?

James_Smith
James_Smith
19 Nov 2024
raspberry Pi 4. Raspberry_pi

Raspberry Pi 4 is the latest iteration of the popular single-board computer series. Packed with upgraded specifications and new features, it offers a wide range of possibilities for various applications. In this article, we will explore the impressive specs of Raspberry Pi 4, discuss how it improves upon its predecessors, and highlight the updates on Raspberry Pi OS. Whether you're a tech enthusiast or an innovator looking to develop new IoT gadgets, servers, or robots, Raspberry Pi 4 provides a cost-effective and robust solution.

Impressive Raspberry Pi 4 Specs

The Raspberry PI 4 boasts a host of impressive specifications that make it a compelling choice for various projects. Let's take a closer look at what it brings to the table:

Processing Power

  • The CPU and GPU of Raspberry Pi 4 are both clocked at 1.5 GHz, providing a significant boost in processing power compared to its predecessors.
  • It features a quad-core Broadcom BCM2711B0 chip built on 28nm technology, utilizing the Cortex-A72 microarchitecture. This architecture enables out-of-order execution and a deeper instruction pipeline, resulting in improved performance.
  • On the Linpack benchmark, Raspberry Pi 4 outperformed the previous model, Raspberry Pi 3 B+, by a staggering 413%, showcasing its enhanced processing capabilities.

Enhanced Graphics and Display

image

  • Raspberry Pi 4 features an upgraded VideoCore VI GPU with a core clock speed of 500 MHz, replacing the VideoCore IV found in Raspberry Pi 3 B.
  • The new GPU supports two displays at 4K resolution and 30 fps each or a single display at 4K and 60 fps, opening up possibilities for high-resolution multimedia applications. 

image

Increased RAM

  • Raspberry Pi 4 offers up to 8GB of DDR4 RAM, a significant improvement from the 1GB of DDR2 RAM found in Raspberry Pi 3 B+. The increased RAM capacity is especially beneficial for memory-intensive tasks such as web browsing and handling high-bandwidth applications.

Connectivity Options

  • One of the major features that makes the electronic components and devices easy to use is their connectivity option. The Raspberry Pi 4 includes multiple connectivity options, such as USB 3.0 ports, a Gigabit Ethernet port, and Bluetooth 5.0 technology. These features enable faster data transfer, improved network connectivity, and seamless integration with various peripherals.

Power and Form Factor

  • The Raspberry Pi 4 can be powered via USB Type-C, providing more efficient power delivery compared to the previous micro USB standard. It requires a minimum of 3 amps and a 5V power supply, ensuring optimal performance.
  • Despite the upgraded internals, Raspberry Pi 4 maintains the same compact form factor as its predecessors, making it compatible with existing cases and accessories.

How Raspberry Pi 4 Improves on Other Models

Raspberry Pi 4 introduces several enhancements that set it apart from its predecessors, such as Raspberry Pi 3 B+. Let's delve into the key improvements and explore how they elevate the overall performance and user experience.

image

Processing Power and Architecture

  • With its faster CPU and GPU clock speeds, Raspberry Pi 4 offers a substantial performance boost compared to Raspberry Pi 3 B+. The Cortex-A72 architecture enables more efficient processing and better power management.
  • The deeper instruction pipeline of the Cortex-A72 processors results in improved execution speed and overall system responsiveness.
  • The Linpack benchmark clearly demonstrates the significant performance gains of Raspberry Pi 4, showcasing its ability to handle demanding computational tasks effectively.

Memory and Storage

  • Raspberry Pi 4's increased RAM capacity allows for smoother multitasking, better web browsing performance, and improved application responsiveness.
  • The microSD card slot of Raspberry Pi 4 is twice as fast as that of Raspberry Pi 3 B+, providing faster data access and reducing loading times.
  • The enhanced storage capabilities of Raspberry Pi 4 make it well-suited for applications that require ample memory and quick access to data.

Connectivity and Networking

  • Raspberry Pi 4 features USB 3.0 ports, which offer faster transfer speeds compared to the USB 2.0 ports found in previous models. This enables quicker data exchange with external devices such as storage drives and peripherals.
  • The Gigabit Ethernet port in Raspberry Pi 4 supports genuine Gigabit connections, allowing for significantly faster network speeds compared to its predecessors.
  • Bluetooth 5.0 technology in Raspberry Pi 4 provides improved wireless connectivity and low-energy capabilities, making it ideal for IoT projects and wireless peripherals.

Display Capabilities

  • Raspberry Pi 4 introduces dual micro-HDMI ports, enabling the connection of two displays simultaneously. This feature is particularly beneficial for applications that require multiple screens or extended desktop setups.
  • With support for 4K resolution and higher frame rates, Raspberry Pi 4 delivers stunning visual experiences, making it suitable for multimedia projects, digital signage, and home entertainment systems.

Updates on Raspberry Pi OS

Raspberry Pi OS, the official operating system for Raspberry Pi devices, has also received notable updates to enhance the user experience and functionality. Let's explore some of the key improvements:

image

Text-Based Search

  • Raspberry Pi OS now includes a text-based search box, accessible by pressing the Windows key on some keyboards or the Raspberry key on others. This search box allows users to quickly locate programs like File Manager, OS Imager, and Image Viewer, improving overall system navigation and productivity.

Audio Input and Output

  • Raspberry Pi OS features a new icon for audio input and output. When a USB or Bluetooth audio device is connected, a microphone icon appears, providing convenient access to audio settings and configurations.

Wi-Fi and Bluetooth Menus

  • Two new keyboard shortcuts, Ctrl-Alt-W and Ctrl-Alt-B, have been introduced to launch the Wi-Fi and Bluetooth menus, respectively. These shortcuts streamline the process of managing wireless connections and settings.

NetworkManager Integration

  • Raspberry Pi OS now includes NetworkManager, a popular network management tool found in many Linux distributions. This integration offers improved Wi-Fi network management capabilities, providing a more user-friendly and efficient way to control wireless connections.

Conclusion

Raspberry Pi 4 is a game-changer in the world of single-board computers, offering significant improvements in processing power, graphics capabilities, memory, and connectivity options. Whether you're a hobbyist, educator, or innovator, the Raspberry Pi 4 provides a versatile and affordable platform for various projects, ranging from educational endeavors to IoT devices and multimedia systems. With continuous updates to Raspberry Pi OS, the user experience is further enhanced, making Raspberry Pi 4 a compelling choice for both beginners and experienced enthusiasts alike.

So, if you're looking to embark on a new tech adventure or take your existing projects to the next level, the Raspberry Pi 4 is the perfect companion to unleash your creativity and bring your ideas to life.

  • Sign in to reply
  • James_Smith
    James_Smith over 1 year ago

    This is one of my research topic assigned during my college work and I tried my best to cover all the features.

    • Cancel
    • Vote Up -1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vmate
    vmate over 1 year ago in reply to embeddedguy

    The text also feels a lot like what an AI would write

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • embeddedguy
    embeddedguy over 1 year ago

    Pi5 is out now.