Internet of Things
  • Technologies
  • More
Internet of Things
Forum Best Load Cell to Measure Medication Weight?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 523 subscribers
  • Views 1446 views
  • Users 0 members are here
Related

Best Load Cell to Measure Medication Weight?

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I am using a board that has both raspberry pi and arduino capabilities. I am looking for the best load cell to take small measurements such as that of a pill. It would have to be relatively sensitive enough to measure in grams. Anyone have suggestions on the best load cell for something like this? Don't worry if it has a complex set-up. Wiring up a circuit to accompany the cell shouldn't be an issue.

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 11 years ago

    Accurate load cells can be very expensive. You can make them from scratch, but the mechanics get very precise and tricky. I would be tempted to buy a low-cost pocket scale to obtain a sensitive sensor coupled with appropriate mechanics. I would then take it apart and tap into the sensor or electronics to get the weight signal. The built-in readout will tell you when you have your signal calibrated properly.

    Here is a typical device - but there are many similar devices available:

    500G X 0 01G 0 1G Mini Digital Pocket Jewelry Scale Calibration Weights Wfeu | eBay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to dougw

    At that price I doubt if there will be any useful accessible signals - it'll have one of those mystery black blobs on the board with everything in it.

     

    I think the idea is fine - just that OP may need to buy a few (different models) before they get one that hacks easily.

     

    These people sell high sensitivity load cells:

     

    http://www.smdsensors.com/Products/Low-Range-Force-Sensors-Grams-to-10s-of-Grams-Full-Scale/

     

    I have no idea of the price but they don't look cheap.

     

    If the OP is looking for fun and entertainment it isn't that hard to build a force balance scale to weigh pills but it's a lot more work than hacking a ready made scale.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 11 years ago in reply to dougw

    At that price I doubt if there will be any useful accessible signals - it'll have one of those mystery black blobs on the board with everything in it.

     

    I think the idea is fine - just that OP may need to buy a few (different models) before they get one that hacks easily.

     

    These people sell high sensitivity load cells:

     

    http://www.smdsensors.com/Products/Low-Range-Force-Sensors-Grams-to-10s-of-Grams-Full-Scale/

     

    I have no idea of the price but they don't look cheap.

     

    If the OP is looking for fun and entertainment it isn't that hard to build a force balance scale to weigh pills but it's a lot more work than hacking a ready made scale.

     

    MK