Internet of Things
  • Technologies
  • More
Internet of Things
Forum Flashing ESP32 by only UART port
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 517 subscribers
  • Views 3637 views
  • Users 0 members are here
  • esp32
  • flashing
  • uart
Related

Flashing ESP32 by only UART port

Chuitoto
Chuitoto over 3 years ago

Hi element 14! have anyone know can we program ESP32 with only UART connection without a USB-to-UART bridge?  

Let's say I have a Jetson nano whtch can have GPIO on the board, UART connunication can be used through 4pin (+, -, RX, TX)

Can we flash the ESP32 by ESP-IDF only by those pin without a USB-to-UART bridge?  

  • Sign in to reply
  • Cancel
Parents
  • JWx
    JWx over 3 years ago

    according to this:

    https://forums.developer.nvidia.com/t/serial-ports-uart-on-the-jetson-tx2-and-nano/117687

    Jetson serial ports are named /dev/ttyS0-3 (or ttyTHS0-3) in linux

    USB-to-Serial port is detected in Linux as any standard serial port (maybe with specific name, but device names like ttyS0 are also possible)

    if voltage levels are compatible one can verify what serial port is used in ESP-IDF util, change it to the above (/dev/ttySx or /dev/ttyTHSx) and flash it like embeddedguy mentioned (reset into download mode then flash)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 3 years ago

    according to this:

    https://forums.developer.nvidia.com/t/serial-ports-uart-on-the-jetson-tx2-and-nano/117687

    Jetson serial ports are named /dev/ttyS0-3 (or ttyTHS0-3) in linux

    USB-to-Serial port is detected in Linux as any standard serial port (maybe with specific name, but device names like ttyS0 are also possible)

    if voltage levels are compatible one can verify what serial port is used in ESP-IDF util, change it to the above (/dev/ttySx or /dev/ttyTHSx) and flash it like embeddedguy mentioned (reset into download mode then flash)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Chuitoto
    Chuitoto over 3 years ago in reply to JWx

    O greate! It's Possible to use ttySX port to flash ESP32! thank you for all your reply!