Internet of Things
  • Technologies
  • More
Internet of Things
Forum I have installed esptool. I would like to know what command to type to erase esp32 s3 flash.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 517 subscribers
  • Views 6402 views
  • Users 0 members are here
  • esp32 s3 sense
Related

I have installed esptool. I would like to know what command to type to erase esp32 s3 flash.

manojroy123
manojroy123 over 2 years ago

I have installed esptool. can anyone help me out with the command to type on the command prompt in order to erase flash of esp 32.

bellow is the command prompt display

image

  • Sign in to reply
  • Cancel

Top Replies

  • obones
    obones over 2 years ago +1
    Why do you want to call it manually? I mean, I'm only ever using it inside VSCode with the PlatformIO extension that takes care of all that tedious setup.
  • javagoza
    javagoza over 2 years ago in reply to manojroy123 +1
    I've used the esptool for the ESP8266 NodeMCU downloading esptool from github https://github.com/espressif/esptool Troubleshooting - ESP32 - — esptool.py latest documentation (espressif.com) I wrote…
Parents
  • balajivan1995
    balajivan1995 over 2 years ago

    1. You are using Linux style USB port identification (dev/ttyUSBx) instead of windows based identification (COMx)

    2. Esptool.py is not added to the path as you have just installed it in local user data, which system can't access unless you add the path to environment variables.

    3. You can actually use an executable named "esptool.exe" that is automatically installed when you install esp32 package automatically. Install "everything" software to find the location of that application and open a cmd window from there. Enter "esptool erase_flash", application will automatically scan all USB port and erase the flash memory of esp32 (assuming it is in boot mode).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balajivan1995
    balajivan1995 over 2 years ago

    1. You are using Linux style USB port identification (dev/ttyUSBx) instead of windows based identification (COMx)

    2. Esptool.py is not added to the path as you have just installed it in local user data, which system can't access unless you add the path to environment variables.

    3. You can actually use an executable named "esptool.exe" that is automatically installed when you install esp32 package automatically. Install "everything" software to find the location of that application and open a cmd window from there. Enter "esptool erase_flash", application will automatically scan all USB port and erase the flash memory of esp32 (assuming it is in boot mode).