Internet of Things
  • Technologies
  • More
Internet of Things
Forum Which devise should I use?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 522 subscribers
  • Views 1040 views
  • Users 0 members are here
Related

Which devise should I use?

e14 Contributor
e14 Contributor over 10 years ago

Hey everyone! I'm new at that page and here is my first question: I'd like to know about some devices I could use to take photos and save them in a microSD. So, I would need: 1) A device (like Arduino or Raspberry Pi), 2) a camera compatible with this device. I would like to conect the device with the caemera directly (space where i want to install the staff). For this reason I think arduino doesn't work, but I'm so noob! About Raspberry Pi, I think it could work out but I'm looking for more options! Thank you community!

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 10 years ago

    There are low-cost cameras available for arduinos but most arduinos don't have enough horsepower or memory to handle images well, much less video.

    Raspberry Pi is a good choice - it has the necessary speed and memory and because it has a built-in camera connector there are lots of examples on the net to learn from. Even the oldest RPi's were good with camera applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to dougw

    Thank you so much! However, do you know if is possible to get the same result with another device smaller?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    You can get PI like devices but smaller, the point Doug was making is that alot of the work is done for you with the PI, and this makes the whole process much more achievable

     

    You could go with a smaller device that does not have a dedicated camera connector and hook up a USB based camera for instance but then your slowed down by probably USB2 interface if you lucky, trying to find suitable drivers and them writing your won code to integrate. Also if you go much smaller then you will be losing something, probably memory, wifi, bluetooth etc so this will mean adding them back again anyway if you need them,

     

    From a pure price perspective, there are plenty of WIFI / IP cameras available ready built, if your doing this for the education etc then dont worry about size so much, if you do end up making it into a product, you can worry then image

     

    Oh, and the PI is no bigger than most Arduinos so your not saving on size there!

     

    The PI has the power required as Doug has said (Were talking about CPU performance)

     

    If as you say, your new to this then you need to walk before you can run so pick the path of less resistance for now, and add complexity later when your ready for it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    You can get PI like devices but smaller, the point Doug was making is that alot of the work is done for you with the PI, and this makes the whole process much more achievable

     

    You could go with a smaller device that does not have a dedicated camera connector and hook up a USB based camera for instance but then your slowed down by probably USB2 interface if you lucky, trying to find suitable drivers and them writing your won code to integrate. Also if you go much smaller then you will be losing something, probably memory, wifi, bluetooth etc so this will mean adding them back again anyway if you need them,

     

    From a pure price perspective, there are plenty of WIFI / IP cameras available ready built, if your doing this for the education etc then dont worry about size so much, if you do end up making it into a product, you can worry then image

     

    Oh, and the PI is no bigger than most Arduinos so your not saving on size there!

     

    The PI has the power required as Doug has said (Were talking about CPU performance)

     

    If as you say, your new to this then you need to walk before you can run so pick the path of less resistance for now, and add complexity later when your ready for it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    In the end it could be a product. I'm not in a rush and I could learn a little bit about them, so if you can tell me some of these smaller devices I'd be so glad. Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 10 years ago in reply to e14 Contributor

    some solutions to check out

    CC3200 Energia | Arduino Based Camera

    low tech: OpenMV Camera Module 

    https://www.olimex.com/Products/ARM/ST/STM32-E407/open-source-hardware

     

    Another interesting solution is to use a $9 C.H.I.P. computer - it is small, has wi-fi, runs linux, and you can add a USB camera (webcam), (images could be stored on a USB memory stick)