Internet of Things
  • Technologies
  • More
Internet of Things
Forum Which sensor to use for detection of Humans Climbing Poles
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 524 subscribers
  • Views 2246 views
  • Users 0 members are here
  • frontpage
  • proximity sensors
  • aurdino
  • ras pi 3
Related

Which sensor to use for detection of Humans Climbing Poles

davetechnosis
davetechnosis over 9 years ago

My Use Case

 

Our client is in Power Generation business. There have more than 3000 poles to transfer power from production to power grid. The distance between each pole is 400 meters. Most of the wires are having active current, but the ones at the low level are used for earthing and dont have any power supply.

 

The line passes through remotest areas of India and consequently, the locals cut the Earthing wire (no active current) and sell them in market. Motion detection camera is one of the option but that creates false alarms. I am looking for a sensor where in any human is trying to climb the pole, the camera gets active and takes snap of the user trying to climb.

 

What kind of sensor can be used for this use case? We need to detect it from the proximity of 5 meters.

 

The image of the pole is here: https://blogs-images.forbes.com/stevensalzberg/files/2014/08/670px-power_lines.jpg

  • Sign in to reply
  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 9 years ago +3
    This is already done in industry. The presence of the electric fields means the best solution will be fiber optic sensing. Fiber is immune to EMI. If you are serious about it, you can message me on here…
  • kas.lewis
    kas.lewis over 9 years ago +2
    The motion scene camera connected to image recognition to look for a person. That may be one solution. Also if you cap sense where you are looking for a signature of a human body, this would take some…
  • davetechnosis
    davetechnosis over 9 years ago in reply to dougw +2
    Ya, I wish, but the issue with IR is that it makes false alarms as even birds are routine visitors.
  • dougw
    dougw over 9 years ago in reply to DAB

    Maybe if a couple of loops of wire were strung around the structure about 4 feet apart, perhaps just above the first cross bar, the capacitance between the loops would indicate when something as big a as a person came near.

    The chip I just road tested would probably work well.

    Cutting these loops could also trigger an alarm.

    Making a big coil inductor around the structure that was part of a resonant circuit or oscillator might work as well. The resonant frequency or oscillation frequency would change when a person was near.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • volly
    volly over 9 years ago in reply to dougw

    davetechnosis.

    I like dougw's idea. Maybe incorporated with some considered recommendations made by makerj2017.

    In addition a combination deterrence barrier of sandwiched barbed wire and energised electrical fencing on both sides of the barbed wire around these pylons

    at a height of about 10 metres from ground level with a monitoring unit which will activate an overhead monitored camera as well as a warning sounder loud enough

    to veer off the perpetrator(s) when the barrier system is triggered.

    This way, the would be thieves would be deterred by the electrified barbed wire barrier and if the barrier is being tampered with, the sounder will act in two ways:

    1. one that might drive fear into them and take off;
    2. two, informing them that they have set off and alarm and that consequential action is being activated that will land them in trouble

    Also, the electrified barrier might even stop them in the act.

    The monitored camera will be used to verify and or identify the perpetrator(s) and a decision could be made to dispatch a patrol team or not.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 9 years ago

    This is already done in industry. The presence of the electric fields means the best solution will be fiber optic sensing. Fiber is immune to EMI. If you are serious about it, you can message me on here and I will put you in touch with the company I work for. We provide fiber optic sensing solutions. Fiber also allows you to measure many poles with one interrogator unit. If you put any point sensors, like the ones discussed thus far in this thread, you will have to provide power to it. Fiber has the power at the interrogator point only.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to michaelwylie

    Good point.

    Perhaps if you used a big coil, you could scavenge power from the local fields.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<