Internet of Things
  • Technologies
  • More
Internet of Things
Forum Language for IOT
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 526 subscribers
  • Views 3935 views
  • Users 0 members are here
Related

Language for IOT

nirmal2000
nirmal2000 over 7 years ago

Which language is better option for learning IOT for beginners?

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 7 years ago +6
    Well, you'll most likely be using a microcontroller so I'd say it has to be C.
  • dougw
    dougw over 7 years ago +5
    For a beginner, the learning curve includes the language, the integrated development environment (IDE), the hardware and they also need to consider the cost of all these things. As mentioned above C and…
  • shabaz
    shabaz over 7 years ago +5
    Hi, traveling so excuse typos typing on a small screen.. There's plenty of scope to learn and use multiple languages, or whatever you're familiar with, since the scope is broad. My favourites are C, C…
Parents
  • dougw
    dougw over 7 years ago

    For a beginner, the learning curve includes the language, the integrated development environment (IDE), the hardware and they also need to consider the cost of all these things. As mentioned above C and Python are two good candidates for language. Python is a little easier to learn but C is more universal. For IDEs, arduino is the most popular and pretty easy to learn, micro:bit IDEs are easier, but limited to micro:bit hardware, TI has Code Composer and Energia (which is like arduino) working together creating a lot of flexibility. I also like PSoC Creator from Cypress because it simplifies hardware as well as software. MBED is another good IDE, but I haven't used it enough to prefer it.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago

    For a beginner, the learning curve includes the language, the integrated development environment (IDE), the hardware and they also need to consider the cost of all these things. As mentioned above C and Python are two good candidates for language. Python is a little easier to learn but C is more universal. For IDEs, arduino is the most popular and pretty easy to learn, micro:bit IDEs are easier, but limited to micro:bit hardware, TI has Code Composer and Energia (which is like arduino) working together creating a lot of flexibility. I also like PSoC Creator from Cypress because it simplifies hardware as well as software. MBED is another good IDE, but I haven't used it enough to prefer it.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to dougw

    Dough, just an objection. If for micro:bit IDE you mean the blocks language, it is true. But thinking to IoT development with micro:bit this visual language is extremely reductive. It is needed to move to a more reliable IDEs, MU (easier) and Yotta (a bit more complex). With Yotta it is possible to experiment and develop using mbed that works on micro:bit as well as a considerable range of other micro controllers (if I ma not wrong some Arduino boards are included too), all C/C++ based. With MU it is interesting for developing with micro-Python; also this development platform support micro:bit as well as some other IoT oriented devices

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to balearicdynamics

    Good points. I wasn't being specific - as I think micro:bit python language/IDE is also simpler than arduino IDE.

    Any of them can be used for beginner IoT.