Internet of Things
  • Technologies
  • More
Internet of Things
Documents Sailing Auto Pilot - Competition - Ready For Tomorrow 2022
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 28 Feb 2022 8:57 AM Date Created
  • Last Updated Last Updated: 29 Nov 2022 2:03 PM
  • Views 19024 views
  • Likes 16 likes
  • Comments 61 comments
Related
Recommended

Sailing Auto Pilot - Competition - Ready For Tomorrow 2022

Farnell partners with sailor Alberto Riva to redevelop a Nautical Autopilot image

Alberto Riva is a multi-competition winning skipper who always had a passion for sailing since he was a child.

With the support of many different sponsors, he has sailed on a variety of boats from smaller centreboard boats to 70ft long flying trimarans, on board of which he competed many different regattas.i

He now has an eye on a new dream: the Mini Transat - a 4050 nautical miles solo race on the smallest offshore racing boats at only 6.50m long. A challenge that requires not only competence and resilience, but also a sound mind.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Far from being only a sailing passionate and competitor, indeed, Alberto is also a trained engineer who worked as data analyst and on-board electronics expert for the preparation of other racing boats. With a master in nanotechnologies, he also developed an auto-pilot board during his studies

.image

The auto-pilot is an element that he defines “his best friend” during sailing, as it allows him to leave the wheel and rest or focus on weather conditions especially on demanding regattas like the Transat, where one-person sailing and no phone/computer or technical support aside from tracking are the main requirements.

image

Interface for AutoPilot 

In light of all the characteristics that distinguish this challenge, such as passion, determination, performance, resilience and technology, Farnell decided to partner with Alberto and help him by opening the project up to our open-source design community to redesign his autopilot. As technologies develop further and faster, we are confident that our electronics enthusiasts could highly improve it to achieve higher performances with better cost efficiency.

image

Among the improvements Alberto would add, he would certainly focus on changing the current screen (which was an additional cost on the overall system) in favour of taking advantage of new smart phone technologies. Connecting a smart phone to the automatic navigation system could allow to cut a big part of development and budget effort, as it would allow to use the embedded characteristics of modern displays such as waterproofness and mechanical resistance, and make it further flexible and efficient.

Join Alberto in his challenge!

Auto Pilot Components

What do you need for a boat to sail its self? 

The autopilot is made by two parts: The data acquisition and the control part.
Several sensor are connected to the system to perform the vectorial calculation of the wind and gain information about the heading of the boat: IMU compass, wind sensor, boat speed sensor and a rudder sensor.

The calculated variables are used to keep the boat on a particular true wind angle or on a particular course. Two nested PID controllers allow the boat to keep the desired route moving the rudder through a linear actuator.

The first PID calculates the desired rudder angle. The second PID, thanks to the rudder angle sensor feedback, drives the motor of the actuator to the desired rudder angle.

The first controller can be set to follow a particular reference: TWA (True Wind Angle), AWA (Apparent Wind Angle), Internal Gyro Compass (preferred choice), Fixed Rudder Angle (debugging purpose).

 

Ancient mariners would tie the rudder with a rope but this could run them into rocks in their sleep. 
Alberto has used electronics to monitor the wind, position and control it all with an Arduino 

image

Components 

Learn more about the components used in this build

image image image image image
Arduino Max232 Driver Interface 12v-5v DC to DC Converter H-Bridge Motor Drivers Resistors 

Arduino

Driver Interfaces DC to DC Converters Motor Drivers Resistors

Are you ready for Tomorrow? 

Competition

Global Competition
Winner
riky_electronicmarine 
Australia and New Zealand
Winner
Gough Lui 

India
Winner
rsjawale24 

Greater China
(China, Taiwan, Hong Kong)
Closed

ASEAN
(Singapore, Malaysia, Phillipines, Vietnam, Thailand) + Korea

Winner
abyraj 
image image image image image

 

Enter our "Ready for Tomorrow" competition for a chance to win a prize from our prize pool

Multicomp Pro Handheld Oscilloscope - Hand Held Oscilloscope
Multicomp Pro PC USB Oscilloscope - USB Oscilloscope
Multicomp Pro Soldering Station - Soldering Station

Mulitcomp Pro Handheld Multimeter - Multimeter


Details of your answers and contact details can be shared with element14 Avnet Group

 

  • ReadyForTomorrow
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14phil
    e14phil over 3 years ago +2
    Congratulation to the Winners of the following Challenges: Global Competition Winner - Will win the full Global Competition Prize pool riky_electronicmarine Australia and New Zealand Winner - Will win…
  • riky_electronicmarine
    riky_electronicmarine over 4 years ago +1
    ok who won the prises?
  • rsjawale24
    rsjawale24 over 3 years ago in reply to dougw +1
    Thanks! Really excited to see what prize do I get from the pool! A handheld oscilloscope would be nice as I don't have a scope with a screen yet..I just received my USB scope as project14 prize
Parents
  • ajayvishaal
    ajayvishaal over 4 years ago

    I've already worked on ROVs and UUVs. Since this is not an under water vehicle, I've some suggestions that can be added to the existing design. So the first thing is to integrate an SBC like Nvidia Jetson Nano or Raspberry Pi. This will add good computation power to the robot. Then coming to the software architecture, my suggestion is to deploy ROS on SBC. Since I'm a ROS Engineer curently working on Autonomous UUVs, I've seen in real time that ROS is robust for making this kind of system into an intelligent machine in a cost effective manner. And next thing is sensor fusion, since the robot moves on the surface of water, we don't need to wory about buoyancy control things. So we can easily focus on sensor fusion part. For that we need an IMU sensor and GPS module and using filters like EKF we can fuse the sensor data to get the accurate pose of the drone. When coming to the obstacle detection part, we can go with 2 sensors. One is Lidars, to detect the obstacles like another boat near by the robot or some other obstacle over the surface of sea. And another one is sonars, which can be mounted under the robot to detect obsacles that is below the surface of water. So Inorder to make the system to avoid obstacles we are going to utilize the Lidar and sonar sensor and control the thruster and rudder of the bot. As far as I understand, It seems like arduino is used for controlling the actuators. So we can utilize the ROSserial communication protocol to make the SBC to talk to the Arduino. So we need to create a script by utilizing the lidar and sonar data and then make the actuators move accordingly based on the obstacle detection.Now coming to the autonomous part, we can use GPS waypoint based navigation by integrating all the features that I've mentioned previously. By this way, the system will be more robust and at the same time will be intelligent. And my final suggestion is creating a custom dashboard, with speedometer dial, battery level indicator, compass and orientaion dials. This makes the user to understand about the bot's current heading direction and all other essential informations. Hope my suggestions helps to develop the robot into a better and intelligent one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ajayvishaal
    ajayvishaal over 4 years ago

    I've already worked on ROVs and UUVs. Since this is not an under water vehicle, I've some suggestions that can be added to the existing design. So the first thing is to integrate an SBC like Nvidia Jetson Nano or Raspberry Pi. This will add good computation power to the robot. Then coming to the software architecture, my suggestion is to deploy ROS on SBC. Since I'm a ROS Engineer curently working on Autonomous UUVs, I've seen in real time that ROS is robust for making this kind of system into an intelligent machine in a cost effective manner. And next thing is sensor fusion, since the robot moves on the surface of water, we don't need to wory about buoyancy control things. So we can easily focus on sensor fusion part. For that we need an IMU sensor and GPS module and using filters like EKF we can fuse the sensor data to get the accurate pose of the drone. When coming to the obstacle detection part, we can go with 2 sensors. One is Lidars, to detect the obstacles like another boat near by the robot or some other obstacle over the surface of sea. And another one is sonars, which can be mounted under the robot to detect obsacles that is below the surface of water. So Inorder to make the system to avoid obstacles we are going to utilize the Lidar and sonar sensor and control the thruster and rudder of the bot. As far as I understand, It seems like arduino is used for controlling the actuators. So we can utilize the ROSserial communication protocol to make the SBC to talk to the Arduino. So we need to create a script by utilizing the lidar and sonar data and then make the actuators move accordingly based on the obstacle detection.Now coming to the autonomous part, we can use GPS waypoint based navigation by integrating all the features that I've mentioned previously. By this way, the system will be more robust and at the same time will be intelligent. And my final suggestion is creating a custom dashboard, with speedometer dial, battery level indicator, compass and orientaion dials. This makes the user to understand about the bot's current heading direction and all other essential informations. Hope my suggestions helps to develop the robot into a better and intelligent one.