Internet of Things
  • Technologies
  • More
Internet of Things
Documents Australia and New Zealand Entry Page - Sailing Auto Pilot - Competition - Ready For Tomorrow 2022
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 11 Aug 2022 9:17 PM Date Created
  • Last Updated Last Updated: 24 Aug 2022 1:29 PM
  • Views 1162 views
  • Likes 4 likes
  • Comments 4 comments
Related
Recommended

Australia and New Zealand Entry Page - Sailing Auto Pilot - Competition - Ready For Tomorrow 2022

image

This is the Competition entry Page for Ready For Tomorrow 2022 APAC

Ready For Tomorrow 2022 
Australia and New Zealand only

Based on Alberto's Project here: /technologies/internet-of-things/w/documents/27490/sailing-auto-pilot---competition---ready-for-tomorrow-2022
F
or other regions please visit the main document above. 

Competition

Enter our "Ready for Tomorrow APAC 2022" competition for a chance to win a prize from our prize pool

Multicomp Pro Handheld Oscilloscope - Hand Held Oscilloscope
Multicomp Pro PC USB Oscilloscope - USB Oscilloscope
Multicomp Pro Soldering Station - Soldering Station

Mulitcomp Pro Handheld Multimeter - Multimeter

image

Enter our competition by commenting your improvements to Albertos Project below

What: Comment below your suggested improvements to Alberto's project. 
When: 10th August 2022 00:01am to 30th September 2022 23:59am
Winning Criteria: Our favorite most detailed suggestions will win prizes.
Suggestions must be feasible and cost effective as this is a DIY solution. 

Who: a Member of the element14 Community based in Australia and New Zealand only
Prize: 1 set of the Prize Pool Listed Above.

Details of your answers and contact details can be shared with element14 Avnet Group

 

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to e14phil

    That is most excellent news!

    I confirm that my details are accurate and up-to-date :)

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 3 years ago

    Congratulations  Gough Lui  you are the winner of this segment.  
    We are pleased to let you know that your suggestion was selected as one of our favorites.
    You will be sent one of the prizes from the prize pool for these competitions. 

    Please make sure the address on your account is current and up to date! 

    Phil 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Electronics777
    Electronics777 over 4 years ago

    A really good thing would be integration with OpenPlotter! Ideally talk over NMEA2000 (CAN). That way it could read sensors on the network (GPS, compass heading, wind speed and direction, water speed, depth, IMU, etc...). AIS data could be used to avoid collisions with ships. And you can send it commands too.

    Modes:

    • Compass Heading
    • GPS Waypoints/paths
    • Hold  a constant wind angle (like a wind vane) for optimal sailing 

    The lower cost, but still expensive, COTS autopilots only steer a constant compass heading and therefore have their limitations. 

    Really cool project!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago

    I’ll have to admit – I’ve never sailed before, let alone been on the water much. But from my point of view, I do know a bit about electronics, so I’ll try and elaborate on some of the improvements I think may be useful.

    • Perhaps consider using FPGAs rather than microcontrollers for the PID loops as FPGAs can process inputs quickly and in parallel, this may mean better loop performance without adding complexity of having multiple microcontrollers or trying to make one microcontroller work several PID loops. Perhaps choose a more powerful microcontroller if going that route – e.g. the RP2040.
    • Use an eInk display – this would save energy as it does not require continuous refreshing and be sunlight readable. Perhaps you could also consider modifying the display to incorporate a backlight for use when it is dark, or use a front-light.
    • For communication with a smartphone, I would recommend the use of Bluetooth Low-Energy for streaming the occasional status update. This keeps power low, and with newer standards, a long-range mode is also available to overcome some of the propagation disadvantages of 2.4GHz. This could be added on, say with the use of an ESP-32-based microcontroller.
    • The use of 2.4GHz probably is not ideal, however, if long-range or penetration of solid material is necessary. As a result, I think it would be better if 900MHz LoRa-based communications is considered. This could be simply added by retrofitting an RFM9x module and would ensure robust, long-range (often several hundred meters to several kilometers) communication with a data-rate tradeoff.
    • If LoRa is used, then perhaps the smartphone is less important and a dedicated eInk-based LoRa display is probably worth building. This could be kept on your body or in several convenient places across the yacht, and all could receive the same broadcast data thus being efficiently updated. Perhaps you could also incorporate a buzzer to indicate critical alarms, so the system could wirelessly page you anywhere on the ship!
    • If the speed of data communications to your actuators and sensors are not that critical, then having them run by separate controllers on a radio link (e.g. LoRa, or 2.4GHz BLE/ESPNow) may be a convenience as this would save on wire and allow for quick replacement in case something goes wrong. Some sensors could feasibly be solar powered or battery powered with lower-energy radios and judicious use of sleep routines.
    • Consider the use of high-precision 24-bit ADCs for digitising analog signals, in case you use any strain sensors or precision potentiometers. This would provide much greater accuracy compared to the onboard analog inputs from an Arduino.
    • It would probably be nice to have a microSD card to serve as a “voyage data recorder” of sorts, as well as a set of environmental sensors (temperature, barometric pressure) to detect potential weather changes. A full-sky camera with an AI-based algorithm may also provide some information on cloud cover as well.

    Those are just some of the things that come to mind …

    - Gough