Internet of Things
  • Technologies
  • More
Internet of Things
Polls Future proofing smart city data communication infrastrucure
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Instructorman
  • Date Created: 15 Apr 2016 7:55 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 2209 views
  • Likes 1 like
  • Comments 13 comments
Related
Recommended

Future proofing smart city data communication infrastrucure

Many municipalities are interested in investing in smart city infrastructure to monitor and manage resource consumption, traffic congestion, et cetera, and to add value to urban living through intelligent analysis of data gathered from sensor networks.  The technology that enables monitoring and management on urban scales is emerging.  One issue that is holding back many municipalities is the question of what infrastructure to embed in order to allow data communication for all the anticipated sensors that may be installed in the future.

 

What do you think is the best strategy that will future proof data communication infrastructure in a smart city context?

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +3
    From a systems engineering standpoint, I would focus on the protocol and then let the technology solve the speed and volume issues. When you implement the control network, plan to change the actual media…
  • DAB
    DAB over 10 years ago +2
    This is one of those issue that there is no good answer. I remember when we designed a lab for a network only to have the technology change to fiber optics before we could implement the project. No matter…
  • tonyboubady
    tonyboubady over 10 years ago +1
    Using and expanding existing infrastructure is wise decision, we are already in 4G era which is almost enough to implement smart city network. Providers should start to categorise their data only packages…
Parents
  • rscasny
    rscasny over 10 years ago

    I looked over some research and white papers. The following condenses what vendors are discussing about Smart City infrastructure:

     

    Cisco doesn’t had clarity or a final word on the subject when it says in its “The Internet of Everything for Cities,” The communication media itself can be fairly diverse (wireless Internet connection, radio frequency, GPRS, 4G/LTE, power line communication, and IP).”

     

    Industry researcher IDC cites in its white paper called “Smart Cities and the Internet of Everything:  The Foundation for Delivering Next-Generation Citizen Services,” a plan by the city of Barcelona for its smart city. Barcelona planned that “the backbone for this is a fiber-optic and WiFi network as the platform to improve service delivery.” This paper is 3 years old, however.

     

    The City of San Jose uses the Starfish network, which is the Sliver Spring Network. I looked it up, Silver Spring says this: "Cellular providers like to brag about how great their coverage is today.  However, cellular is still a tower-based solution, which requires point-to-point connections from expensive cell towers. The price of monthly cellular charges has fallen over the last few years, but operators still have to pay a substantial bill every month for a cellular-only solution for millions of devices. Silver Spring provides a mesh-based solution that is backhaul agnostic.  Our Access Points support Ethernet and cellular backhaul, but network operators can also connect to Wi-Fi, satellite, WiMAX, fiber, or other backhaul methods from the Access Point.  Our Access Points can backhaul traffic from up to 5,000 devices, so monthly OPEX costs are greatly reduced. You can’t see around a corner with a tower-based solution, but you can mesh around a corner.  Our customers deploy mesh networks and dictate the coverage they need for their applications using our self-forming and self-healing mesh."

     

    Randall

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rscasny
    rscasny over 10 years ago

    I looked over some research and white papers. The following condenses what vendors are discussing about Smart City infrastructure:

     

    Cisco doesn’t had clarity or a final word on the subject when it says in its “The Internet of Everything for Cities,” The communication media itself can be fairly diverse (wireless Internet connection, radio frequency, GPRS, 4G/LTE, power line communication, and IP).”

     

    Industry researcher IDC cites in its white paper called “Smart Cities and the Internet of Everything:  The Foundation for Delivering Next-Generation Citizen Services,” a plan by the city of Barcelona for its smart city. Barcelona planned that “the backbone for this is a fiber-optic and WiFi network as the platform to improve service delivery.” This paper is 3 years old, however.

     

    The City of San Jose uses the Starfish network, which is the Sliver Spring Network. I looked it up, Silver Spring says this: "Cellular providers like to brag about how great their coverage is today.  However, cellular is still a tower-based solution, which requires point-to-point connections from expensive cell towers. The price of monthly cellular charges has fallen over the last few years, but operators still have to pay a substantial bill every month for a cellular-only solution for millions of devices. Silver Spring provides a mesh-based solution that is backhaul agnostic.  Our Access Points support Ethernet and cellular backhaul, but network operators can also connect to Wi-Fi, satellite, WiMAX, fiber, or other backhaul methods from the Access Point.  Our Access Points can backhaul traffic from up to 5,000 devices, so monthly OPEX costs are greatly reduced. You can’t see around a corner with a tower-based solution, but you can mesh around a corner.  Our customers deploy mesh networks and dictate the coverage they need for their applications using our self-forming and self-healing mesh."

     

    Randall