Take the Nordic Thingy:53 Quiz
This Fun Quiz to Win 1 of 5 Nordic Thingy:53s! With its wireless connectivity, multitude of sensors, and two ARM Processors, it can almost help build anything!
PIC-IoT WG Dev Board
An IoT development board that provides an MCU, encryption, and Wi-Fi, connecting embedded applications directly to the Google Cloud.
Buy NowRaspberry Pi 4
With the Dual 4K Micro-HDMI, it has the fastest running processor at 1.5GHz, dual-band 2.4Ghz/5GHz Wireless LAN, BluetoothLE 5.0, and PoE capability.