Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum choosing a motor and parts.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 76 subscribers
  • Views 1445 views
  • Users 0 members are here
Related

choosing a motor and parts.

gio_dude
gio_dude over 9 years ago

Sorry about the simple questions in advance but I'm very new to motors.

 

So I wanted to make a retractable window curtain the goes up and down and coils on to its self. So what I was thinking was bluetooth or wifi feather from adafruit with their motor driver wing (https://www.adafruit.com/product/2927 ). A  motor on a rod with the curtain hanging from it.  

 

So if I'm missing something that will make this project completely fail in my face please tell me.

 

here are my questions

 

what type of motor should choose?

I've been reading a lot about stepper motor and they look promising since I can have more precision.

 

What type of torque do i need to be looking at.

I read the post about torque and need to read it a few more times to understand it all but it doesn't sound like I need a lot of torque.

 

Motor to rod connection.

I don't know terms very well and looking at 3d printers they use a coupler to attach the motor to a rod. is there a different way i should research or a better way of doing it.

 

Dual motor

I was thinking about using a motor on each side one wired in reverse is that a good idea.

 

thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3 suggested
    Hi Giovanni, It seems that your application will need a higher torque lower speed motor if you are going to directly couple the rod to the motor shaft. Since these type motors are geared down and when…
  • 14rhb
    14rhb over 9 years ago +2 suggested
    Your ideas make good sense to me. I think what you describe is what I call a 'roller blind'. I've got a manually operated one at home. At times it can be quite hard to lift via the pull cord. You could…
  • gio_dude
    gio_dude over 9 years ago in reply to 14rhb +1
    Thank you for the reply. I will look into how toothed belt and pulleys work, but do they take up a lot of space. Thank you for your advice on the dual motors that make more sense now. Could you explain…
Parents
  • 14rhb
    0 14rhb over 9 years ago

    Your ideas make good sense to me. I think what you describe is what I call a 'roller blind'. I've got a manually operated one at home. At times it can be quite hard to lift via the pull cord.

     

    You could measure the required force to raise your curtain by winding a cord around the roller and attaching a large enough known weight to lift the curtain. Required torque for your stepper motor would then be (minimum): Roller radius(m) x Weight(Kg) x 9.8ms-2  = Torque (Newton metres or N.m )

     

    You could also increase you motor's torque using a toothed belt and pulleys (smaller pulley on motor, larger pulley on curtain roller). Like these:

    image

     

    Personally I would just try a single motor as they will be acting on the same shaft. When you see a 3D printer with two steppers for the Z axis they are pushing on separate ends of the cross beam - so there is a little give if they don't quite manage the same movement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gio_dude
    0 gio_dude over 9 years ago in reply to 14rhb

    Thank you for the reply.

     

    I will look into how toothed belt and pulleys work, but do they take up a lot of space.

     

    Thank you for your advice on the dual motors that make more sense now.

     

    Could you explain a litttle more about how you are  calculating the torque. Are you saying setup everything and see how much weight is need to turn it with out the motor then do the math.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gio_dude
    0 gio_dude over 9 years ago in reply to 14rhb

    Thank you for the reply.

     

    I will look into how toothed belt and pulleys work, but do they take up a lot of space.

     

    Thank you for your advice on the dual motors that make more sense now.

     

    Could you explain a litttle more about how you are  calculating the torque. Are you saying setup everything and see how much weight is need to turn it with out the motor then do the math.