Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum need help with a stepper driver
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 3 answers
  • Subscribers 77 subscribers
  • Views 4839 views
  • Users 0 members are here
  • help
  • stepper_motor
  • manual
  • motor_driveboard
  • instruction_manual
  • stepper_driver
  • motor_control_drive
  • instruction
  • help_required
  • division_setting_table
  • motor
  • arduino
  • motor_circuits
  • stepper_drive
Related

need help with a stepper driver

e14 Contributor
e14 Contributor over 13 years ago

imageimageimageimageimageimage

this is a 2-phase stepper motor drive by a chinese company called SCKJMOTOR with the model number SC2680MH

it can be found here in this link http://sckjmotor.com/prodetail.asp?cid=3&scid=6&id=67

i am not much experienced with electronics so i cant figure out how to use it with out an instruction manual and sadly the manual is in chinese image

so i thought maybe i can find some help here on element 14

 

you can see in the pictures  the driver has lots off ports on it they go like  + , PU, + , DR, + , MF, + ,  TM, +V, -V, +A, -A, +B, -B

 

here i think the " + " ports might be a 5V input so i guess i must give 5V in them, but why are there so many???? why do i need to give the driver 5V at 4 different ports ???   image

 

the port " PU " might be pules, i am just guessing, it might be to control the speed of the motor  

 

the port " DR " maybe direction like forward-reverse, another guess 

 

the port " MF " i have no idea, cant even guess this one   image

 

the ports " +V " and " -V" the driver says on the side " DC24-80V "  so i guess i might have to give it some thing between 24V to 80V

 

the posts  +A, -A, +B, -B  are clear i guess, i just have to find the right coil pairs of the stepper motor and connect it to these ports  image 

 

there is also some thing called a division setting table and it gives me values  1, 2, 4, 8, 16, 32, 64 and 128 , i think this must be some thing related to the step divisions of the stepper motor, need some help with that as well

 

please try to help me out with this, i am just starting to take interset in electronice and dont have any experience in this at all, just have some basic electronic knowledge since i am doing engineering and its my 1st year

 

thank you

  • Sign in to reply
  • Cancel
Parents
  • kas.lewis
    0 kas.lewis over 13 years ago

    Have you tried Google Translate? I have it built into my browser so one click and its all in english.... Ahh OK I see what you mean now, I gat all the slaes stuff in english but since they have embeded the data sheet as a picture Google won't translate that image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to kas.lewis

    exactly  image  , the useless stuff i could just Translate it all, what i want is all as pictures sadly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 13 years ago in reply to e14 Contributor

    OK, just asked someone here and this is what I could make out.

     

    MF - motor output signal or some form of feedback (Does not need to be connected)

    V+ - DC Power

    V-  - DC Power

    A  - Stepper motor phase A

    B  - Stepper motor phase B

    TM - Zero point (we think)

    Im - Current in coil

    PU - Stepper pulse (D2-on step on rising edge, D2-off step on falling egde) we think

    DR - Direction D2-off direction control signal, D2-on reverse pulse

     

    Also in teh data sheet were it says asomething then 0 - 0.5V that is the low required, 4-5V that is the high required, 2.5us is the pulse width. The PU/DR + take 5V and if >5V is applied a current limiter is needed.

     

    I think that should get you somewhat started on the understanding what is what but to get it aculy working it seems liek there is a controller that plugs into PU- and DR- as can be seen in teh picture n ttop right corner of teh data sheet.

     

    (sorry about spelling, writing this quickly while at work)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to kas.lewis

    thanks alot, appreciate ur help very much image

     

    ill have to read ur reply a few times trying to understand every bit since i am very new to this 

     

    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to kas.lewis

    thanks alot, appreciate ur help very much image

     

    ill have to read ur reply a few times trying to understand every bit since i am very new to this 

     

    thank you