Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Another BeagleBone - BeagleBone AI!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 27 Feb 2019 4:19 PM Date Created
  • Views 4099 views
  • Likes 16 likes
  • Comments 10 comments
  • bbai
  • bb-ai
  • beaglebone ai
  • bbb
  • beagleboard
Related
Recommended

Another BeagleBone - BeagleBone AI!

shabaz
shabaz
27 Feb 2019

Hopefully we'll hear more soon, but there appears to be another BeagleBone board launched at Embedded World, with the same form-factor as the BeagleBone Black.

It's called the BeagleBone AI. I'm guessing it's not a replacement and won't be anywhere near as cost-reduced as the BBB and its variants (for example there is 16GB of eMMC on-board on the BB-AI), the board looks very useful for working with image recognition or other video processing.

(Photo from the Beagleboard website, will replace with a better photo if I find one):

image

The main chip is TI's AM5729, which doesn't have a datasheet yet, but appears to be the same or very similar to AM5728. The diagram below highlights some interesting features. There are a lot of processing sub-systems.

The applications processor portion is a dual-core Cortex-A15 (dark red) running at 1.5GHz. There are 2D and dual 3D graphics processors (shown in green), plus a couple of DSPs (orange).  There is a Video Processing Engine (VPE) shown in brown, for stuff like basic image scaling.

There is still the PRU capability shown in purple (2 x dual-core PRU), but there's also a couple of dual-core Cortex-M4 processors for real-time operations too (shown in blue). This is nice, I''m guessing it allows for real-time computation, and high-speed low-level protocol handling, to be separated if desired.

 

What wasn't on the block diagram but I've added it in yellow, are four EVE embedded vision engines! These are apparently controlled via normal C programming. Open CL is possible, and some other API maybe.

Unlike the older NEON (which was a basic, general SIMD processor for doing operations on a few bytes of memory in a single instruction - some further description here: BBB, NEON and making Tintin bigger  ), EVE simplifies things so that you don't need to program in complex SIMD instructions, it handles it for you. Plus it is specially designed for video operations, for example object identification. You can get it to identify shapes or objects in real-time live video really efficiently, at low power, since the key building-blocks that the image recognition algorithms use are implemented in hardware. I can't find much info on it yet, but I have not google'd it a lot so far. It could be useful for object identification while driving, if you're designing the next Tesla.

 

Also, the BB-AI brings out USB 3.0 speeds, with a USC Type C connector. And GigEth. Plus wireless (2.4 and 5GHz) including 802.11ac! so super-high throughput hopefully. Also supports BLE as I understand.

 

image

If anyone is at Embedded World, or has more information to share, it would be great to see it!

 

Texas Instruments Deep Learning (TIDL)

There is a framework to make use of the DSP and EVE processors, if desired, for some computer vision types of scenarios.

According to a TI Deep Learning overview PDF it can be used for some popular things like classifying objects, and detecting multiple different objects and their locations.

image

Some more examples of this:

image

(The images above are from that PDF document).

It can be done in live video streams, as shown here, screenshot from video at https://e2e.ti.com/support/processors/f/791/t/710226?TDA3-Our-TIDL-car-detection-on-TDA3X-are-there-any-methods-to-incre… :

image

The main resource on learning the TIDL framework is the Processor SDK TI Deep Learning Documentation.

 

 

 

Edited 28th Feb 2019 - I'd mistyped the TI part code in the text above, it is corrected now.

Edited 3rd March 2019 - Added a bit on TI Deep Learning (TIDL)

  • Sign in to reply
  • fmilburn
    fmilburn over 7 years ago

    According to this site the cost will be ~$100 and it will be available in mid to late 2Q: https://blog.hackster.io/the-new-beaglebone-ai-b3eea55e09f2

     

    RE: AI

    BeagleBone AI makes it easy to explore how artificial intelligence (AI) can be used in everyday life via the TI C66x digital-signal-processor (DSP) cores and embedded-vision-engine (EVE) cores supported through an optimized TIDL machine learning OpenCL API with pre-installed tools.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Problemchild

    Problemchild  wrote:

     

    Which bit was the AI part then Shabaz it seems to have a unit for everything !!?

    I had the same thought. This is a versatile device. Why mark it as AI? Buzzword compliance?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 7 years ago in reply to Problemchild

    Problemchild  wrote:

     

    Which bit was the AI part then Shabaz it seems to have a unit for everything !!?

    I think the Embedded Vision Engines are the AI part.  In the USA, "AI" primarily means "self-driving vehicles" and lots of chip makers are competing for those sockets.

     

    I used to think that self-driving vehicles would be a bad thing -- how could you possibly have a computer drive safely given all the variables?  Then I started paying attention to how others were driving and decided that as long as the computer does better than the average USA driver it would be a net win.  That is not a big hurdle.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 7 years ago

    Which bit was the AI part then Shabaz it seems to have a unit for everything !!?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gecoz
    gecoz over 7 years ago

    This is one very interesting board! I hope all the goodies don't push the price too high.

     

    BTW, there is also another interesting open source board launched at Embedded World: the S7-Mini, based on the Xilinx Spartan7. I wonder if anybody has info on that one as well.

     

    Fabio

     

    image

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • More
    • Cancel
<