Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog ‘Bottoms-up’ dispenser can fill 56 pints of beer in one minute….magnetically
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ZeroSizeObject
  • Date Created: 25 Jan 2011 6:03 AM Date Created
  • Views 842 views
  • Likes 0 likes
  • Comments 1 comment
  • industrial
  • automation
  • beer
Related
Recommended

‘Bottoms-up’ dispenser can fill 56 pints of beer in one minute….magnetically

ZeroSizeObject
ZeroSizeObject
25 Jan 2011
image
 
A magnet-powered method of pouring beer from the bottom up that works nine times faster than traditional methods, further proof that great ideas can be fueled by alcohol. The cup features a small hole at the bottom, covered up by a circular magnet. Pressurized beer lifts the magnet up; filling the cup until the weight of the beer on top of the magnet pushes it back down, sealing the bottom. Josh Springer, the inventor of Bottoms-up, said by switching from traditional taps to his system, stadiums can go from using eight pourers per two cashiers to one pourer per eight cashiers. So the main problem has become that providers literally can’t collect money fast enough to keep up. Regardless, the new system certainly speeds up the time it takes to grab a brew, which means fans don’t have to miss as much of the game to quench their desire to drink beer. The Bottoms Up system also cuts costs for the provider by minimizing spillage and provides drinkers with a relatively-foamless beer. You no longer need to worry about that one guy who doesn’t know how to pour, as the system gets rid of pouring altogether. For more information please visit: http://www.grinonindustries.com/aboutgrinon.htm

Zero
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    One suggestion, rather than using the weight of the liquid to push the magnet down, use a metal disk inside, as a valve held by the magnet. when placed on the filler base, the magnet holds the cup in place, and a small tube pushes the disk up, for filling. the base retracts, the disk clamps to the magnet, creating a seal..  Otherwise, just a magnet alone, once you reach the bottom of the glass (perish the thought!) the magnet could fall away, creating a spill.

     

    Oh, one other suggestion.. Advise customers, Don't use their charge plates (credit cards) as coasters! we are talking magnets here! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 15 years ago

    One suggestion, rather than using the weight of the liquid to push the magnet down, use a metal disk inside, as a valve held by the magnet. when placed on the filler base, the magnet holds the cup in place, and a small tube pushes the disk up, for filling. the base retracts, the disk clamps to the magnet, creating a seal..  Otherwise, just a magnet alone, once you reach the bottom of the glass (perish the thought!) the magnet could fall away, creating a spill.

     

    Oh, one other suggestion.. Advise customers, Don't use their charge plates (credit cards) as coasters! we are talking magnets here! image