Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Building a Linear Power Supply Module
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 29 Oct 2017 8:49 PM Date Created
  • Views 14295 views
  • Likes 13 likes
  • Comments 10 comments
  • diy audio
  • linear_power_supply
  • power supply
  • linear power supply
  • dc power supply
  • diy
  • hifi
  • hi-fi
Related
Recommended

Building a Linear Power Supply Module

shabaz
shabaz
29 Oct 2017

Note: The project is experimental. The project is low power and low voltage, and requires a low voltage source which can be derived from a mains transformer.

However there are significant risks with building mains powered projects. For that reason, it is advised to use an external enclosed AC to low voltage mains transformer unless you’re a qualified engineer.

 

Introduction

When working with analog circuits it can help to have a linear power supply. I use a Thandar supply at home, but unfortunately it just has a single supply rail.

 

Years ago I built a cheap dual-rail supply; it used a couple of linear supply kits from a local electronics store, and was put together with a mains transformer and a couple of voltmeter display panels. I still use it, but I wanted to create “building block” types of modules for op amp experiments, hi-fi audio projects such as headphone amplifiers, working with ultra-sensitive devices and signals from sensors, and sensitive radio receivers, and for integration into all sorts of other projects where noise would cause issues otherwise.

 

So, the aim of this project was to build a reasonably general-purpose, low noise, compact linear power supply that can be embedded into larger projects or could be used standalone. It is intended to supply up to around 250mA at voltages selectable at design time, and power output can be up to 3.75W for each of dual rails, so there is enough power to drive lots of interesting projects.

 

The final PCB actually contains two designs; a dual rail supply, and also a separate single rail supply. The two sections can be cut if desired, if all three rails are not needed in a project. Multiple boards could be used for additional rails.

 

The photo here shows the dual rail portion of the board completed (the single rail part of the board is essentially just a duplicate of half of the dual-rail portion, and is not fully soldered in the photo below). Having three rails could be useful for combined analog/digital projects where (say) a +5V supply is needed for a microcontroller, but also +/-15V is needed for the analog portion. The separate single rail supply is isolated, to help keep any microcontroller noise away from the analog circuitry.

image

 

The voltage regulators are adjustable at design time through modification of component values so the PCB can be useful for various projects by altering the capacitor and resistor values, and selecting an appropriate transformer.

 

As mentioned, a typical use-case could be to have +5V and +/-15V or +/-10V. I decided to construct the dual rail portion to be +/-14V (a somewhat arbitrary value, I just needed something higher than +/- 12V for some experiments.

 

To summarise, here are the design specs, but as mentioned these values can be changed by altering component values:

Input: 110V or 220V AC

Main Output: +14V 250mA, -14V 250mA

Additional Output: +5V 200mA

 

Design Overview

The output from the mains transformer is shown here:

image

 

The flattened top and bottom is normal; the mains supply is not always a perfect sine wave, and the transformer may be introducing some harmonics too.

 

The output from the mains transformer is rectified and then any diode switching noise is filtered and the rectified output is also filtered using the large electrolytic capacitors to leave a DC waveform. Any high frequency noise is reduced using ferrite beads, which present a high resistance to such noise content.

image

The positive unregulated output from the circuit above goes to the positive linear regulator. This circuit is based around an LT3065 integrated circuit. The datasheet was followed. The voltage is set using a couple of resistors, but if you wish to make changes then please consult the datasheet because some other part values (such as capacitor C10 in the diagram below) also need to be adjusted if the desired voltage is changed.

 

Note that the output voltage with the values shown is actually 14V, not 15V. The output current is set to 250mA maximum.

image

The negative unregulated output from the bridge rectifier is fed to a LT3090 based circuit. Again the datasheet was closely followed. The output is -14V (250mA max) with the values indicated.

image

 

The portion of the PCB that contains the single rail power supply reuses the same design as for the positive rail. The values are changed though, because I desired to set this output to 5V. The current limit for the 5V output was set to 200mA with resistor R1.

image

Building It

The render here shows what the PCB looks like for the dual rail design. The transformer output is connected on the left side.

 

The circular arrangement was originally intended to allow screwing directly over the center of the toroidal transformer for a very small footprint supply block, but toward the end of the PCB design layout I decided to just fit it alongside the transformer with screw holes on the corners of the PCB instead. The top half of this design implements the negative supply rail, and the bottom half implements the positive supply rail.

image

The single rail output PCB design is near-identical to the bottom half of the dual-rail PCB design.

 

The CAD files are attached to the blog post, they can be sent to any PCB manufacturer. Once the boards arrive, the first task is to solder the linear regulator integrated circuits. They have an exposed pad on the underside; one procedure on how to solder underside pads using a normal soldering iron is shown here.

 

After they have been soldered, continue soldering the smallest parts and end with the largest, i.e. the electrolytic capacitors and the connectors.

 

Attaching the Transformer

Molex Ultra-Fit connectors were used for the transformer secondary wires. A low-cost PA-09 crimp tool was used.

image

 

When inserting the crimped ends into the plastic shell, orient the crimp such that the side of the crimp that was open is facing upwards, if the clip side of the plastic shell is also facing upwards. The photo below shows the correct orientation of the metal crimps in the center of the photo, open side facing upwards, to match the orientation of the plastic shell on the right side of the photo, which has its clip facing upwards.

image

 

Initial Tests

The bulk of the testing will be saved for part 2, but for now the transformer was powered up, and the output voltage from the dual rails was observed initially with no load. Noise was not measurable with the oscilloscope, other techniques will be used for this.

 

The voltage was also measured with a multimeter and the prototype output was measured to be +14.06V and -13.99V. Load and dynamic testing will be carried out in Part 2.

 

Getting a Third, Isolated Rail

In order to get the third rail to be fully isolated, one could use another transformer. However, it is more practical to use the same transformer and add another winding.

 

Note: The information in this section is explicitly for the specific 15VA 2x12V transformer15VA 2x12V transformer from Farnell, and is only appropriate if the dual rails set for +/-15V or lower, at up to 250mA on each rail, and if the third rail is set to be at +5V at up to 200mA.

The information will not apply to any other model transformer, even if the ratings appear identical. This also applies to all other materials (such as the wires and tape) mentioned in this section. Only the part numbers specified must be used, and they must come from a traceable source. There is a very high risk of damage or electrocution or fire if this is not followed.

Also, please use responsible mains wiring, not bad mains wiring as often seen.

 

The steps are extremely simple, there is not much that can go wrong, provided you use the correct, identical materials and follow the procedures. The actual mains wiring and final assembly will not be described in this blog post, it will come in part 2. This blog post will only describe how to obtain the extra supply rail using the transformer.

There are four main steps.

 

Step 1: Winding the Enamelled Wire

Take a 7 metre length of 180 degrees C rated 24 or 25 AWG enamelled copper wire, and wind 82 turns of it around the transformer. To do this, it is easier to start in the middle, at 3.5 metres into the wire, and wind 41 turns from each 3.5 metre length. One turn is basically one pass through the center of the transformer. Once you’re done, it should look like the photo below:

image

 

Step 2: Attaching the PVC Wire Leads

Use a small piece of Kapton tape (if you've not used it before, it is a very heat tolerant adhesive tape that can be used as an insulating layer) to hold the first and last windings in place, and then attach PVC insulated wires to the ends. This process will involve scraping off the enamel (use a small piece of sand paper or the edge of a blade). The photo here shows a blue PVC insulated wire soldered onto the enamelled copper wire. The insulated wire must be 22AWG, 105 degrees C rated.

image

 

Step 3: Securing the Wire Leads

Bend back the enamelled wire and place some tape across the blue wire, and then fold over the blue wire into a ‘U’ shape and secure it with more Kapton tape, such that there is some strain relief. The Kapton tape is placed across the wire, but also another piece is taped through the transformer, on both sides of the blue wire, so that it is held in place securely. The result of this should look like in the photo below:

image

Here is the birds eye view of it all so far; you can see the Kapton tape has been wrapped through the transformer, on both sides of the blue wire, for both ends of the winding:

image

 

Step 4: Insulating the Winding

Wind Kapton tape around the transformer, to cover all of the enamelled copper wire. This won’t be possible with a single long length of Kapton tape, so you’ll have to do it with shorter (say 30cm) lengths. Start at the other side of the blue wire, so that at least 10mm prior to the enamelled copper wire is covered, and overlap the Kapton tape by half of its width, so that by the time the tape has been wound around to the other end blue wire (and cover a further 10mm), there is effectively a double-layer thickness of Kapton tape everywhere over the 5V winding, due to the overlap. It will look like the photo below:

image

 

That’s it! Now you have a transformer with an additional winding suitable for providing the +5V rail.

 

In summary the modifications listed have made the transformer suitable for providing the +/-15V rails at up to 250mA, and +5V at 200mA. This capability should be sufficient for many of the projects mentioned in the introduction!

 

The specific parts that must be used are listed here:

15VA 2x12V Transformer15VA 2x12V Transformer

24 AWG enamelled wire24 AWG enamelled wire

22 AWG PVC insulated wire22 AWG PVC insulated wire

Kapton Polyimide tapeKapton Polyimide tape

 

Summary

A dual rail (or triple rail) power supply module design has been constructed for low noise projects. Although tests still need to be done, I thought it was worth writing up this part 1 now, in case others wish to construct this project too. The parts list is below and board files are attached to this blog post too, ready for sending to any PCB factory (e.g. Elecrow, iTead).

 

Parts List

Transformer, Enamelled Wire and Tape:

See above

 

Unregulated Supply Section:

C1,C2,C3,C4,C5,C6 3300uF 25V  EEUFK1E332SEEUFK1E332S Farnell 1744955 18MMDIA 7.5MM PITCH Panasonic Capacitor FK Series

C15   1u 100V 1210 Capacitor Kemet C1210C105K1RACTU Farnell 1793831 

R8 100R 0805 Resistor  CR0805-FX-1000ELFCR0805-FX-1000ELF Farnell 2008370

D1,D2,D3,D4  PMEG10020AELRPMEG10020AELR Farnell 2498546 SOD123W 100 V 2 A low leakage current Schottky barrier rectifier

FB1,FB2  FBMH3225HM102NT Farnell 1651731   Ferrite Bead 1210  

J1 Molex  172286-1204172286-1204 Farnell 2494350 ULTRA-FIT-4-VERT Connector

 

Dual Rail Section Plugs and Crimp terminals:

J1-PLUG J2-PLUG Molex  172256-1004172256-1004 Farnell 2494339 Ultra-Fit 4-way Connector Housing

CRIMP-SOCKETS (qty 8 needed) Molex 172253-3111 Farnell 2494336 Ultra-Fit 20AWG

 

Dual Rail Section Positive Output:

C7 10uF 25V Panasonic  EEEHD1E100AREEEHD1E100AR Farnell 1714735 case'C SMD Aluminium Electrolytic capacitor

C8 10n   0603 Capacitor Kemet C0603C103K1RACTU Farnell 1865545  

C9 22n   0603 Capacitor Kemet C0603C223K1RACTU Farnell 1865548  

C10   56n   0603 Capacitor Kemet C0603C563K3RACTU Farnell 2522421

C11   10uF 35V AVX TPSD106K035R0300  Farnell 1432608 Tantalum D size (7.3mmx4.3mm) Band marks '+'

R1 1.2k 0603 Resistor(sets the current limit to 250mA  CR0603-FX-1201ELFCR0603-FX-1201ELF Farnell 2333528

R2 270k  1% 0603 Resistor (sets the output voltage to 14V) ERJ3EKF2703V Farnell 2303262  

R3 12k   1% 0603 Resistor (sets the output voltage to 14V) CR0603-FX-1202ELF Farnell 2333583 

R4 470k 0603 Resistor  CR0603-FX-4703ELFCR0603-FX-4703ELF Farnell 2333613

U1 LT3065EMSE or LT3065IMSE  Farnell 2396654 LDO Positive Voltage Regulator  

J2 Molex  172286-1204172286-1204 Farnell 2494350 ULTRA-FIT-4-VERT Connector

 

Dual Rail Section Negative Output:

C12 10uF 25V Panasonic  EEEHD1E100AREEEHD1E100AR Farnell 1714735 case'C SMD Aluminium Electrolytic capacitor

C13   100p  0603 Capacitor Kemet C0603C101J1GACTU Farnell 1414602

C14   10uF 35V AVX TPSD106K035R0300  Farnell 1432608 Tantalum D size (7.3mmx4.3mm) Band marks '+'

R5 40.2k 1 0603 Resistor(sets the current limit to 250mA  ERJ3EKF4022VERJ3EKF4022V Farnell 2059463

R6 280k 1 0603 Resistor(sets the output voltage to-14V  ERJ3EKF2803VERJ3EKF2803V Farnell 2059515

R7 470k 0603 Resistor  CR0603-FX-4703ELFCR0603-FX-4703ELF Farnell 2333613

U2 LT3090EMSE or LT3090IMSE or LT3090MPMSE Farnell 2365998 Negative Voltage Regulator

 

Third Rail Section Plugs and Crimp terminals:

J1-PLUG,J2-PLUG Molex  172256-1002172256-1002 Farnell 2494337 Ultra-Fit 2-way Connector Housing

CRIMP-SOCKETS (qty 4 needed) Molex 172253-3111 Farnell 2494336 Ultra-Fit 20AWG

 

Third Rail Section (Positive 5V Regulator):

D1,D2,D3,D4  PMEG10020AELRPMEG10020AELR Farnell 2498546 SOD123W 100 V 2 A low leakage current Schottky barrier rectifier

FB1  FBMH3225HM102NT Farnell 1651731   Ferrite Bead 1210

C1 1u 100V 1210 Capacitor Kemet C1210C105K1RACTU Farnell 1793831

C2,C3 5600uF 16V  EEUFK1C562EEUFK1C562 Farnell 1744932 16MMDIA 7.5MM PITCH Panasonic Capacitor FK Series

C4 10uF 25V Panasonic  EEEHD1E100AREEEHD1E100AR Farnell 1714735 case'C SMD Aluminium Electrolytic capacitor

C5 10n  0603 Capacitor       

C6 22n  0603 Capacitor       

C7 15n  0603 Capacitor       

C8 10uF 35V AVX TPSD106K035R0300  Farnell 1432608 Tantalum D size (7.3mmx4.3mm) Band marks '+'       

R1 1.5k 0603 Resistor(sets the current limit to 200mA  CR0603-FX-1501ELFCR0603-FX-1501ELF Farnell 2333563

R2 432k 1% 0603 Resistor (sets the output voltage to 5V) ERJ3EKF4323V Farnell 2303286       

R3 59k  1% 0603 Resistor (sets the output voltage to 5V) CRCW060359K0FKEA Farnell 1652892       

R4 470k 0603 Resistor  CR0603-FX-4703ELFCR0603-FX-4703ELF Farnell 2333613

R8 100R 0805 Resistor  CR0805-FX-1000ELFCR0805-FX-1000ELF Farnell 2008370

U1 LT3065EMSE or LT3065IMSE  Farnell 2396654 LDO Positive Voltage Regulator       

J1,J2 Molex  172286-1202172286-1202 Farnell 2494346 ULTRA-FIT-2-VERT Connector

Attachments:
export-psu-4.zip
  • Sign in to reply
  • michaelkellett
    michaelkellett over 8 years ago in reply to shabaz

    Hello Shabaz,

     

    Thanks for the info - I'll be interested to see what your tests find - and I understand the reason for the diodes now .

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to michaelkellett

    Hi Michael,

     

    Thanks for checking it out! Unfortunately I messed up there : ( I did not realise I'd placed the RC across the bridge rectifier output, I'd meant it across the input : ( To try to reduce that HF noise generated by the rectifier diodes and the inductance on that secondary side. I would not have spotted it so soon, I'm glad you pointed it out. Time for the bodge wiring to resolve this : (

    The Schottky diodes are an experiment, but I hoped it would work out because I was not sure I would reach the goal of allowing up to +-15V to be achieved (since I was using an off-the-shelf transformer with the 12V secondary rating, and I had not physically prototyped those tiny LDOs to see what the measured dropout was, and the headroom from the calculations was not a lot - I have quite a high voltage mains supply, but others may not) - so I configured the output to +-14V initially, with the option to go to +-15V later if it worked out, or revert to normal rectifier diodes and a possibly lower configurable output if it didn't.

    I could not find much info on using Schottky diodes in a bridge rectifier for PSU application, now I'm wondering if it could be worth comparing it with IN400x diodes, to see which results in more noise (or which noise is easier to suppress). Since I have a some spare PCBs, I will try to run that test, with nothing but the bridge rectifiers and some reservoir capacitance, and a resistor as a load.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago

    Hello Shabaz,

    Thanks for going to th trouble of posting all this.

     

    I have two questions,

    1) what is R8, C15 path for ?

    2) why schottky diodes in the rectifier, I've always felt that they are less rugged than simple low speed rectifier diodes and more likely to cause hf problems - although now I think about it I haven't got any hard evidence to prove it.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to learnerjohn

    Hi John,

    I've now added a parts list to the blog post, and a file called 'export-psu-4.zip'. To obtain the PCB, the cheapest way is to use a manufacturer for example Elecrow or iTead (there are many others too).

    To do this, download the export-psu-4.zip file and then on the PCB manufacturer website you can select the board size to be 100x90mm (or 100x100mm if it doesn't allow specifying it exactly), 2-layer board, and then check-out, and upload the file. It will cost approximately $10 for 5-10 boards (i.e. $0.50-$1 per board), so you will have some spare. Shipping is about $10-$20 total. It takes about a week for the boards to be made (and then some time depending on destination/shipping option selected).

     

    The board has all three outputs (dual rail plus the third isolated rail), you can hacksaw off the third rail if not needed for a project).

    image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • learnerjohn
    learnerjohn over 8 years ago

    Hello my name is John and I am new on Element 14,

     

    This linear power supply has my attention to use with various devices.

    How can the PCB be purchased, to support a build.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>