Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Fake and Re-used Electronic Parts and Components
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 15 Jun 2017 1:18 AM Date Created
  • Views 4456 views
  • Likes 10 likes
  • Comments 14 comments
  • fake
  • ebay
Related
Recommended

Fake and Re-used Electronic Parts and Components

shabaz
shabaz
15 Jun 2017

I thought it would be good to have a discussion about peoples experiences with fake and recycled components, and share photos so that others can be aware.

 

As an introduction, it should be clear to most that if it a component deal seems too good to be true then it probably is fake : )

I generally avoid using ebay for components, although I have used it for a few parts in the past for hobby projects. One particular area of risk seems to be integrated circuits, especially audio op-amps and RF chips. These can cost a lot, and I once saw a fake Analog Devices part which clearly was a cheaper IC with the markings sanded off and a new marking inscribed on top. A genuine AD part would not have such poor quality finish.

 

LEDs are another area of concern; a while back I picked up a few Cree LEDs, but I also purchased some from Farnell.

The difference is quite interesting, this is a photo of the underside of the LEDs:

image

The one purchased through ebay came in a plastic component carrier tape, just like the genuine parts from Farnell. However, upon opening the tape and examining the underside, it can be seen that the part has been recycled; someone has unsoldered it from a PCB and polished off the solder, revealing the copper underneath the plated exterior that the genuine part should have.

LEDs have a limited life and this one has likely been used in the past, and will have a lower brightness and time to failure compared to a new LED. The LED does light up (I tested with a multimeter), it just won't perform as well as the new part. It may not be the same part either; the genuine LEDs are correctly binned for brightness matching.

 

I don't purchase from ebay often enough to have more examples, but it would be interesting to see and read about other fakes/recycled parts other people have experienced.

  • Sign in to reply
Parents
  • rachaelp
    rachaelp over 9 years ago

    I once bought what was supposed to be an Arduino compatible Nano v3 which allegedly had a genuine FTDI chip on it. It was suspiciously cheap and I could never get communication to work properly so I suspect it was not actually a genuine FTDI chip at all. I did check out all the connections and make sure everything was connected to where it should, it just didn't work.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rachaelp
    rachaelp over 9 years ago

    I once bought what was supposed to be an Arduino compatible Nano v3 which allegedly had a genuine FTDI chip on it. It was suspiciously cheap and I could never get communication to work properly so I suspect it was not actually a genuine FTDI chip at all. I did check out all the connections and make sure everything was connected to where it should, it just didn't work.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 9 years ago in reply to rachaelp

    Hi Rachael,

     

    That's a good point, those USB-to-UART chips could have been fake. Also USB-to-RS232 adapters have had that issue in the past! There was a famous Prolific PL2303 'Error code 10' issue.

    • Cancel
    • Vote Up +3 Vote Down