Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog ODROID-GO Handheld Gaming Kit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 27 Jun 2018 8:52 PM Date Created
  • Views 5525 views
  • Likes 12 likes
  • Comments 29 comments
  • educational
  • retro gaming
  • odroid
  • gaming
  • educational kit
  • retro gaming console
  • odroid-go
Related
Recommended

ODROID-GO Handheld Gaming Kit

shabaz
shabaz
27 Jun 2018

Introduction

Thanks to Problemchild he advised me about a simple gaming kit called ODROID-GO, and it was fairly low cost (£38 including delivery to the UK) for such a device, so I was tempted to purchase it. (Note: that there will be duty of approx. £7 to pay, plus £12 handling charge by FedEx, so that makes it less attractive : (

 

The ODROID-GO is a very compact (approx 120x75x13mm) device that internally features an ESP32 (ESP32 PDF datasheet) based module (this contains a microcontroller and 2.4GHz WLAN and Bluetooth Classic and Bluetooth LE capabilities), and rechargeable battery built-in too. There is also a microSD socket and what is especially awesome is a 0.1 inch SIL header socket at the top end of the case, for custom hardware expansion : )

 

image

(image source: ODROID website)

 

It comes with a microUSB cable for charging and USB UART for connecting into the ESP32 module. All that is additionally required is a microSD card, and a small Philips screwdriver to assemble it!

The device comes from ODROID, who manufacture some really nice single board computers and accessories.

 

It arrived today, and although I'd initially thought it was a kit to be soldered, it actually is pre-soldered. I think a child could easily assemble it with just a little supervision. It looks really great, and I'm tempted to purchase another, so both my nephews can have one.

 

This short blog post is a quick introduction to the ODROID-GO, I have not explored it much yet.

 

What's in the Box

This is everything you get in the box (the micro USB cable is also supplied but not shown in the photo):

image

 

What Can it be Used For?

The project is open source, and there is an ODROID-GO github repository with the schematic and source code.

However no programming knowledge is needed to use it just for gaming. For gaming some files are downloadable from the ODROID website that need to be transferred to a microSD card, along with games ROMs. It can play ROMs for various historical consoles like Nintendo GameBoy, and Sega GameGear and so on. I've not explored (nor assembled!) it yet. ODROID-GO assembly steps are online.

 

More interestingly, since it is open source, the possibility exists to create your own games or applications, and connect your own hardware. The expansion port appears to have SPI and a few general purpose input/output connections and 3.3V available. Perhaps it could become a debug tool : )

 

Some More Pics..

The enclosure looks to be of reasonable quality, injection-moulded, perhaps 1mm thick. It could crack perhaps if mishandled; it looks like the same plastic that CD case covers were made of. It is custom-designed and has the ODROID legend on the front. The lower half of the shell has a slot for inserting the microSD card, but I didn't like that such a delicate card is exposed. It would have been better to have a plastic cover for it. Other than that, I didn't have any complaints, but I still need to assemble it to explore further. There are four black rubber buttons (the enclosure has them labelled as Menu, Volume, Select and Start), and also a directional pad and a couple of buttons labelled A and B, suitable for games. There is a slide switch on the right of the ODROID-GO, for power on/off. The hard LCD cover is adhesive, so once the LCD is fitted, it may be awkward to remove. Anyway, the LCD it is unlikely to go faulty. The PCB can still be removed by disconnecting the LCD.

image

The pre-assembled circuit board looks nicely made, it is a 1.6mm fiberglass board so it is fairly rugged.

image

 

Everything looks easy to maintain and debug, there are lots of test points on the circuit board. The holes where the screws should go are marked; three screws secure the PCB to the inside of the front shell of the enclosure, and then six screws will secure the rear half of the enclosure.

image

 

That's it for this short blog post. To be continued..

  • Sign in to reply

Top Comments

  • Problemchild
    Problemchild over 7 years ago in reply to shabaz +4
    I want to do a copy of defender!!
  • shabaz
    shabaz over 7 years ago in reply to genebren +3
    Oh! that's great : ) Like you I had to use PayPal, that bank transfer charge was unattractive! although it worked for me from their website.
  • Problemchild
    Problemchild over 7 years ago in reply to genebren +3
    I notice the PAypal Button is next to the transfer button I clicked that then entered the address(Same as Paypal) and also selected the invoice address to be the same and that all worked it just sent me…
  • Problemchild
    Problemchild over 7 years ago in reply to genebren

    Cheers ...seem to be unavailable at the moment though ;-(

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to Problemchild

    John,

     

    Not quite sure what URL your are looking for.  But here is the Amazon link: https://www.amazon.com/ODROID-GO-source-console-No-Operating-System/dp/B07FFZVWMC

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to Problemchild

    John,

     

    I did the exact same thing.  I think that their site, while attempting to verify the City, State and Postal code ran into a glitch and prevented my transaction from going through to PayPal.  I re-tried, re-checked and try again, but I could not get into the PayPal site.

     

    Thanks for your suggestion, but problem solved I found it on Amazon.

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 7 years ago in reply to shabaz

    I want to do a copy of defender!!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to Problemchild

    Hehe, that's excellent, we can share hi-scores on Chuckie Egg: )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>