Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum CNC Interface Board discussion
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 329 subscribers
  • Views 9108 views
  • Users 0 members are here
  • linuxcnc
  • engraver
  • cnc
  • bbb
  • machinekit
  • BeagleBone Black
Related

CNC Interface Board discussion

shabaz
shabaz over 7 years ago

This is a thread to discuss ideas for controlling low-cost hardware (machines), for the purposes of cutting or engraving for example. It was created due to the interest in ralphjy project to assemble such a device.

There are several ways to do this, typically the 'brains' are a normal desktop or laptop PC, or a single board computer (SBC), and then there is some interface board, that then ultimately connects via high-power drivers, to the motors. There are some other bits of functionality too, like feedback (e.g. limit switches) for detecting end stops.

 

In terms of motors, in industry servomotors will be used, but for home use stepper motors are a lot more popular due to lower cost. For controlling the tool, a 'spindle motor' may be a brushless motor, or alternatively a brushed permanent magnet DC motor (i.e. BLDC or PMDC motor respectively).

 

The PC connection to the interface board can typically be a parallel interface, or USB. When using a SBC then its on-board general-purpose input/output (GPIO) can be used.

 

The BeagleBone Black (BBB) is worth considering I think, since it has been the first popular Linux product to be integrated into machines, providing functionality for 3D printers and small CNC machines. Commercial manufacturing products have been launched with the BeagleBone inside, such as the PocketCNC. There are also third party add-on boards that act as interface boards (and some that integrate motor drivers too). The BBB is old now, but there is a BeagleBone-AI that could in future be used as an upgrade.

 

Partly the reason the BBB has been useful is because it contains some programmable real-time units (PRU) internally, and they can override some GPIO pins, for direct control without needing to go through the Linux system. So, the Linux system can push code to execute on the PRU, and the PRU will control the pins. This means high speeds, and no unexpected delays or jitter, since the PRUs are simpler devices that do not run an operating system that could have a task preempted.

 

To control the interface cards, PCs have a wider choice of software, and popular choices are Mach 3 and LinuxCNC. For the BBB, the software all the boards seem to use is called Machinekit, which is a fork of LinuxCNC.

 

Using it for BBB is not documented well unfortunately. When I first started looking a while back, it was hard to tell which information works, and which information is old. I wanted to automate a simple XY table I'd bought.

However, there is a fairly recent blog article with useful pointers.  It too discusses that information is spread out.

 

It would be nice to develop hardware (or to at least consider it first), and any software or configurations, documented, that would allow low-cost control of machines, and to bound it a little, to only consider home-grade machines using stepper motors, not servomotors. I think there is value in a new open source design, to collect up the wisdom of the various CNC users here, so we can all have low-cost home robots to make things for us!

After some initial thinking, these sketches were a couple of ideas: They are based around the thought that the BBB could be a plug-on daughter card on a larger interface board, that uses something like RJ45-style connectors (because it would be nice to use off-the-shelf cables where possible, to reduce wiring effort, otherwise there are a lot of wires to connect).

image

 

image

After some further discussions with balearicdynamics, it was suggested that scenario 1 could be more practical since it can handle more motors (low power and high power). I too like that idea, since it is one less board to make.

Edge connectors or some other connection location could still be left on the board, for those who do want to have a custom board for add-ons (e.g. to control a 3D printer instead, where they may need outputs for say a heater).

 

More input to any of this, including the practicality of it all, and board design (physical as well as functionality), and connector choices, is welcome. Meanwhile, I've been looking at the existing boards that are supported by Machinekit, to see what pins they use of the BBB, and why. I'll have to install Machinekit to better understand it. So far, I've looked at boards (or Machinekit configs) called CRAMPS, Replicape, and BeBoPr-Bridge and all use different pin mappings. I need to figure out which of these configs are using the PRU, and if so, which pins to allocate for that. I like the CRAMPS pin mapping so far, because it avoids eMMC and HDMI clashes (the BBB has these brought out to its connectors, and some interface boards tend to use these, which rules out using eMMC or HDMI as a result).

 

The pin mappings are in text files, but not easy to compare, so I've put them in a spreadsheet, I'll attach that as soon as it is complete.

The pin mapping text files are: CRAMPS.hal,  replicape.hal, BeBoPr-Bridge.hal  (I'll look at a few more too, and put them in the spreadsheet).

The mappings are numbers like 817, which means header P8 on the BBB, pin number 17.

 

EDIT: I'd hoped to daisy-chain the supplies, but looking at the user docs of a random one, it recommends against this practice:

image

So, the in/out connectors may not be a good idea, and a single power connector on each motor driver could be preferred.

I'm still looking for a suitable connector, but thinking it may as well be another RJ45-style, since I cannot think of another high power cheap alternative. Ethernet will carry lots of current safely, if wires are paralleled. There is the risk of accidentally plugging it into the wrong socket, but they could be color coded.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 7 years ago +7
    shabaz wrote: ... some programmable real-time units (PRU) internally, and they can override some GPIO pins, for direct control without needing to go through the Linux system. So, the Linux system can push…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to genebren +6
    ... another good reason to use a proper stepper driver is that it generates stepper friendly currents. A half bridge design, controlled by a pulse signal, will try (and succeed) to run the motor with square…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz +5
    Good idea of opening a separate thread. Enrico
Parents
  • shabaz
    shabaz over 7 years ago

    Final update for the day; it turns out there is a pre-built Xenomai kernel, so no need to try to build it from scratch. I added it to my BBB, but after it boots, it hangs! (perhaps 20 seconds after it the login prompt - I can log in during that time and use it). I cannot tell what is causing it (I cannot find a pattern to it, from the log files so far). In any case, on a hunch, I tried a normal BBB (well, a BBB-Industrial), rather than the BBB-Wireless. Then it worked : )

    To test the kernel, I need to install some user-space Xenomai stuff, and then run a test program. That's for another day!

    There is still the option of trying the pre-built Linux Machinekit image too, so it is still a 2-pronged approach, to see what works best.

    I worry just one avenue could be shut somewhere further down, so better to have two (or more) for now.

    But in conclusion, I think for BBB CNC stuff, it may be better to go for the standard BBB (or BBB-Industrial, since it is the closest to the original) rather than the others, simply because the real-time kernel patches may have been tested more on that.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    What I was wondering about: “Why the need for RT in Linux if the time critical (and jitter sensitive) functions are done in the PRUs?”

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 7 years ago in reply to Jan Cumps

    This is something I was wondering too, if there is a large enough buffer between "linux" and the pru then there shouldn't be a problem.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to bwelsby

    bwelsby  wrote:

     

    This is something I was wondering too, if there is a large enough buffer between "linux" and the pru then there shouldn't be a problem.

    There's not that much data that needs to be shared.

    Per stepper motor and per movement command:

    • Direction (1 bit),
    • number of steps,
    • requested speed (steps per second)
    • start speed (steps per second),
    • acceleration.

    Other movements in a CNC (spindle motor, ?) don't seem to be that time critical. They could be managed from Linux.

    If you work with a predefined acceleration profile and speed, you could either program that fixed in the PRU or set it once before the first step command is given. In that case it would only be dir and steps.

     

    Things like end switches and fault/stall detection are hardware signals and could directly be handled by the PRU.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to Jan Cumps

    Hi!

     

    I'm guessing (not sure) that as soon as any curve is cut, the Linux process is sending lots of events to the PRU, to change directions, until the curve is complete. Or maybe it pushes many trajectories into PRU-accessible memory like a list instead, and then the PRU then handles them sequentially, but the implemented code might not be that clever - not sure. I will scrutinize the code, to understand what amounts of work are done with the PRU.

    With a manual machine, I only make linear movements, but if I do not control the feed to be smooth, then I see ripples in the edge (since the tool heats the edge unevenly). I've no grasp though of the effect of several msec of jitter where (maybe?) hundreds of modifications may be made to the direction and speed, in order to cut curves (if these really are individual events to the PRU instead of written to PRU-accessible memory area as a list.

    And at some point it will be good seeing the real-world difference in cutting/engraving, using these different configurations.

    The several msec of jitter is reduced to 0.4msec of jitter with PREEMPT RT from initial observation, but I've yet to try Xenomai (I installed it, but it didn't work, because I have to add a certain flag in one of the commands during install.. the instructions on two BBB websites both appear incorrect).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago in reply to Jan Cumps

    Hi!

     

    I'm guessing (not sure) that as soon as any curve is cut, the Linux process is sending lots of events to the PRU, to change directions, until the curve is complete. Or maybe it pushes many trajectories into PRU-accessible memory like a list instead, and then the PRU then handles them sequentially, but the implemented code might not be that clever - not sure. I will scrutinize the code, to understand what amounts of work are done with the PRU.

    With a manual machine, I only make linear movements, but if I do not control the feed to be smooth, then I see ripples in the edge (since the tool heats the edge unevenly). I've no grasp though of the effect of several msec of jitter where (maybe?) hundreds of modifications may be made to the direction and speed, in order to cut curves (if these really are individual events to the PRU instead of written to PRU-accessible memory area as a list.

    And at some point it will be good seeing the real-world difference in cutting/engraving, using these different configurations.

    The several msec of jitter is reduced to 0.4msec of jitter with PREEMPT RT from initial observation, but I've yet to try Xenomai (I installed it, but it didn't work, because I have to add a certain flag in one of the commands during install.. the instructions on two BBB websites both appear incorrect).