Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum CNC Interface Board discussion
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 329 subscribers
  • Views 9119 views
  • Users 0 members are here
  • linuxcnc
  • engraver
  • cnc
  • bbb
  • machinekit
  • BeagleBone Black
Related

CNC Interface Board discussion

shabaz
shabaz over 7 years ago

This is a thread to discuss ideas for controlling low-cost hardware (machines), for the purposes of cutting or engraving for example. It was created due to the interest in ralphjy project to assemble such a device.

There are several ways to do this, typically the 'brains' are a normal desktop or laptop PC, or a single board computer (SBC), and then there is some interface board, that then ultimately connects via high-power drivers, to the motors. There are some other bits of functionality too, like feedback (e.g. limit switches) for detecting end stops.

 

In terms of motors, in industry servomotors will be used, but for home use stepper motors are a lot more popular due to lower cost. For controlling the tool, a 'spindle motor' may be a brushless motor, or alternatively a brushed permanent magnet DC motor (i.e. BLDC or PMDC motor respectively).

 

The PC connection to the interface board can typically be a parallel interface, or USB. When using a SBC then its on-board general-purpose input/output (GPIO) can be used.

 

The BeagleBone Black (BBB) is worth considering I think, since it has been the first popular Linux product to be integrated into machines, providing functionality for 3D printers and small CNC machines. Commercial manufacturing products have been launched with the BeagleBone inside, such as the PocketCNC. There are also third party add-on boards that act as interface boards (and some that integrate motor drivers too). The BBB is old now, but there is a BeagleBone-AI that could in future be used as an upgrade.

 

Partly the reason the BBB has been useful is because it contains some programmable real-time units (PRU) internally, and they can override some GPIO pins, for direct control without needing to go through the Linux system. So, the Linux system can push code to execute on the PRU, and the PRU will control the pins. This means high speeds, and no unexpected delays or jitter, since the PRUs are simpler devices that do not run an operating system that could have a task preempted.

 

To control the interface cards, PCs have a wider choice of software, and popular choices are Mach 3 and LinuxCNC. For the BBB, the software all the boards seem to use is called Machinekit, which is a fork of LinuxCNC.

 

Using it for BBB is not documented well unfortunately. When I first started looking a while back, it was hard to tell which information works, and which information is old. I wanted to automate a simple XY table I'd bought.

However, there is a fairly recent blog article with useful pointers.  It too discusses that information is spread out.

 

It would be nice to develop hardware (or to at least consider it first), and any software or configurations, documented, that would allow low-cost control of machines, and to bound it a little, to only consider home-grade machines using stepper motors, not servomotors. I think there is value in a new open source design, to collect up the wisdom of the various CNC users here, so we can all have low-cost home robots to make things for us!

After some initial thinking, these sketches were a couple of ideas: They are based around the thought that the BBB could be a plug-on daughter card on a larger interface board, that uses something like RJ45-style connectors (because it would be nice to use off-the-shelf cables where possible, to reduce wiring effort, otherwise there are a lot of wires to connect).

image

 

image

After some further discussions with balearicdynamics, it was suggested that scenario 1 could be more practical since it can handle more motors (low power and high power). I too like that idea, since it is one less board to make.

Edge connectors or some other connection location could still be left on the board, for those who do want to have a custom board for add-ons (e.g. to control a 3D printer instead, where they may need outputs for say a heater).

 

More input to any of this, including the practicality of it all, and board design (physical as well as functionality), and connector choices, is welcome. Meanwhile, I've been looking at the existing boards that are supported by Machinekit, to see what pins they use of the BBB, and why. I'll have to install Machinekit to better understand it. So far, I've looked at boards (or Machinekit configs) called CRAMPS, Replicape, and BeBoPr-Bridge and all use different pin mappings. I need to figure out which of these configs are using the PRU, and if so, which pins to allocate for that. I like the CRAMPS pin mapping so far, because it avoids eMMC and HDMI clashes (the BBB has these brought out to its connectors, and some interface boards tend to use these, which rules out using eMMC or HDMI as a result).

 

The pin mappings are in text files, but not easy to compare, so I've put them in a spreadsheet, I'll attach that as soon as it is complete.

The pin mapping text files are: CRAMPS.hal,  replicape.hal, BeBoPr-Bridge.hal  (I'll look at a few more too, and put them in the spreadsheet).

The mappings are numbers like 817, which means header P8 on the BBB, pin number 17.

 

EDIT: I'd hoped to daisy-chain the supplies, but looking at the user docs of a random one, it recommends against this practice:

image

So, the in/out connectors may not be a good idea, and a single power connector on each motor driver could be preferred.

I'm still looking for a suitable connector, but thinking it may as well be another RJ45-style, since I cannot think of another high power cheap alternative. Ethernet will carry lots of current safely, if wires are paralleled. There is the risk of accidentally plugging it into the wrong socket, but they could be color coded.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 7 years ago +7
    shabaz wrote: ... some programmable real-time units (PRU) internally, and they can override some GPIO pins, for direct control without needing to go through the Linux system. So, the Linux system can push…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to genebren +6
    ... another good reason to use a proper stepper driver is that it generates stepper friendly currents. A half bridge design, controlled by a pulse signal, will try (and succeed) to run the motor with square…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz +5
    Good idea of opening a separate thread. Enrico
Parents
  • Jan Cumps
    Jan Cumps over 7 years ago

    I have virtually no experience with running CNC, 3D printers and laser cutters. Looking for info on how they combine axis movements.

    Do the stepper motors ever run truly real-time at the same time?

    What is the sequence (commands generated) when  a 90° movement is made?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to Jan Cumps

    Yes. Steppers are often changing speed independently. Imagine moving in a circle. The X stepper will be receiving pulses at a frequency which plotted would form a sine curve. At the same time the Y stepper pulse frequency would form a cosine.

     

    Things get more complicated when you start considering limiting acceleration. Moving in an L shape would in theory be a fixed stream of pulses on X followed by a similar stream of pulses on Y. In practice this would attempt to turn a very sharp corner at speed. You might get away with this for a 3D printer or a laser, but a heavy spindle would give you a very large clunk, the whole machine would vibrate and you might even miss steps. Should you round the corner slightly? Should you slow but turn sharply? A bit of both? Slowing might work for a mill, but what about a laser which will burn more material if moved more slowly. You get the idea. It starts simple but soon gets complicated.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Fred27

    Fred27  wrote:

     

    ... It starts simple but soon gets complicated.

    Yes, I lost an important part of the skills needed - over time, because not needed in my string of jobs - my math and geometry skill (decent at school time) virtually evaporated.

    I can control a stepper motor, acceleration and deceleration, and torque.

    I also think that, if I don't have to create a smooth path and just run steppers at a constant speed, I'd be able to calculate a path for X and Y to run simultaneously.

    Doing that with taking in account acceleration of both axises (axes?) interfering with each other is beyond the number of active brain cells left image.

    For some reasons, I've vastly improved my analysis skills since leaving school, but at the cost of math.

    I tried to bump it op again  by following MOOC calculus training, but to no avail.

    For some odd reasons, other courses go perfectly fine. I can pass some exams with two fingers in my nose and one hand tied behind my back. But not math and calculus.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 7 years ago in reply to Jan Cumps

    Lets not forget also Z changing for CNC work, so that would be 3 steppers / Servos to track and calc for, no simple task im sure, like you the grey matter is lacking in this regard.

     

    For 3D printing this is simplified by the fact they print 1 layer at a time so only 2 axis to worry about. also a lot of apps will not handle curves and in fact will break them up in to a set of straight lines approximating a curve (Actually a setting in Fusion 360 CNC output tools), if you were to also include curves as is used in more expensive CAM programs then the math is way more complex yet again.....

     

    The hardware is the easy part lol

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 7 years ago in reply to Jan Cumps

    Lets not forget also Z changing for CNC work, so that would be 3 steppers / Servos to track and calc for, no simple task im sure, like you the grey matter is lacking in this regard.

     

    For 3D printing this is simplified by the fact they print 1 layer at a time so only 2 axis to worry about. also a lot of apps will not handle curves and in fact will break them up in to a set of straight lines approximating a curve (Actually a setting in Fusion 360 CNC output tools), if you were to also include curves as is used in more expensive CAM programs then the math is way more complex yet again.....

     

    The hardware is the easy part lol

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 7 years ago in reply to Robert Peter Oakes

    I just realized... 3d printing still has the 3 axis to worry about.

    XX, Y and E. the extruder is feeding the filament and needs to dynamically adjust all the time to ensure a consistent layer thickness at any speed or direction and would be integral to any acceleration / deceleration needed

     

    Ah well image

    • Cancel
    • Vote Up +3 Vote Down