Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum CNC Interface Board discussion
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 329 subscribers
  • Views 9121 views
  • Users 0 members are here
  • linuxcnc
  • engraver
  • cnc
  • bbb
  • machinekit
  • BeagleBone Black
Related

CNC Interface Board discussion

shabaz
shabaz over 7 years ago

This is a thread to discuss ideas for controlling low-cost hardware (machines), for the purposes of cutting or engraving for example. It was created due to the interest in ralphjy project to assemble such a device.

There are several ways to do this, typically the 'brains' are a normal desktop or laptop PC, or a single board computer (SBC), and then there is some interface board, that then ultimately connects via high-power drivers, to the motors. There are some other bits of functionality too, like feedback (e.g. limit switches) for detecting end stops.

 

In terms of motors, in industry servomotors will be used, but for home use stepper motors are a lot more popular due to lower cost. For controlling the tool, a 'spindle motor' may be a brushless motor, or alternatively a brushed permanent magnet DC motor (i.e. BLDC or PMDC motor respectively).

 

The PC connection to the interface board can typically be a parallel interface, or USB. When using a SBC then its on-board general-purpose input/output (GPIO) can be used.

 

The BeagleBone Black (BBB) is worth considering I think, since it has been the first popular Linux product to be integrated into machines, providing functionality for 3D printers and small CNC machines. Commercial manufacturing products have been launched with the BeagleBone inside, such as the PocketCNC. There are also third party add-on boards that act as interface boards (and some that integrate motor drivers too). The BBB is old now, but there is a BeagleBone-AI that could in future be used as an upgrade.

 

Partly the reason the BBB has been useful is because it contains some programmable real-time units (PRU) internally, and they can override some GPIO pins, for direct control without needing to go through the Linux system. So, the Linux system can push code to execute on the PRU, and the PRU will control the pins. This means high speeds, and no unexpected delays or jitter, since the PRUs are simpler devices that do not run an operating system that could have a task preempted.

 

To control the interface cards, PCs have a wider choice of software, and popular choices are Mach 3 and LinuxCNC. For the BBB, the software all the boards seem to use is called Machinekit, which is a fork of LinuxCNC.

 

Using it for BBB is not documented well unfortunately. When I first started looking a while back, it was hard to tell which information works, and which information is old. I wanted to automate a simple XY table I'd bought.

However, there is a fairly recent blog article with useful pointers.  It too discusses that information is spread out.

 

It would be nice to develop hardware (or to at least consider it first), and any software or configurations, documented, that would allow low-cost control of machines, and to bound it a little, to only consider home-grade machines using stepper motors, not servomotors. I think there is value in a new open source design, to collect up the wisdom of the various CNC users here, so we can all have low-cost home robots to make things for us!

After some initial thinking, these sketches were a couple of ideas: They are based around the thought that the BBB could be a plug-on daughter card on a larger interface board, that uses something like RJ45-style connectors (because it would be nice to use off-the-shelf cables where possible, to reduce wiring effort, otherwise there are a lot of wires to connect).

image

 

image

After some further discussions with balearicdynamics, it was suggested that scenario 1 could be more practical since it can handle more motors (low power and high power). I too like that idea, since it is one less board to make.

Edge connectors or some other connection location could still be left on the board, for those who do want to have a custom board for add-ons (e.g. to control a 3D printer instead, where they may need outputs for say a heater).

 

More input to any of this, including the practicality of it all, and board design (physical as well as functionality), and connector choices, is welcome. Meanwhile, I've been looking at the existing boards that are supported by Machinekit, to see what pins they use of the BBB, and why. I'll have to install Machinekit to better understand it. So far, I've looked at boards (or Machinekit configs) called CRAMPS, Replicape, and BeBoPr-Bridge and all use different pin mappings. I need to figure out which of these configs are using the PRU, and if so, which pins to allocate for that. I like the CRAMPS pin mapping so far, because it avoids eMMC and HDMI clashes (the BBB has these brought out to its connectors, and some interface boards tend to use these, which rules out using eMMC or HDMI as a result).

 

The pin mappings are in text files, but not easy to compare, so I've put them in a spreadsheet, I'll attach that as soon as it is complete.

The pin mapping text files are: CRAMPS.hal,  replicape.hal, BeBoPr-Bridge.hal  (I'll look at a few more too, and put them in the spreadsheet).

The mappings are numbers like 817, which means header P8 on the BBB, pin number 17.

 

EDIT: I'd hoped to daisy-chain the supplies, but looking at the user docs of a random one, it recommends against this practice:

image

So, the in/out connectors may not be a good idea, and a single power connector on each motor driver could be preferred.

I'm still looking for a suitable connector, but thinking it may as well be another RJ45-style, since I cannot think of another high power cheap alternative. Ethernet will carry lots of current safely, if wires are paralleled. There is the risk of accidentally plugging it into the wrong socket, but they could be color coded.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 7 years ago +7
    shabaz wrote: ... some programmable real-time units (PRU) internally, and they can override some GPIO pins, for direct control without needing to go through the Linux system. So, the Linux system can push…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to genebren +6
    ... another good reason to use a proper stepper driver is that it generates stepper friendly currents. A half bridge design, controlled by a pulse signal, will try (and succeed) to run the motor with square…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz +5
    Good idea of opening a separate thread. Enrico
Parents
  • shabaz
    shabaz over 7 years ago

    I made some steps forward today (and always some backward of course : ).

    Looking more deeply at some of stuff on the Internet, it seems most guides for installing Machinekit are for PREEMPT RT on Beaglebone, and not Xenomai. That's disappointing, but I figured I'd get back to that once I have a bit more understanding of how Machinekit works. So, I put aside the Xenomai stuff, and burned a new micro SD card with a ready-made Linux image already containing Machinekit. It is available here: https://elinux.org/Beagleboard:BeagleBoneBlack_Debian  (search for the text machinekit on that page). It gets installed just like a standard BBB Linux image, except the default user isn't debian, but is a user called machinekit (with the password machinekit too).

     

    So, once that was installed, I searched around, and found almost nowhere that describes what to do next image It's incredible how unfriendly the documentation out there is for beginners to CNC, even on the official sites. However, this link has nice simple steps for beginners: https://jetforme.org/2018/04/machinekit-on-bbb/

     

    Anyway, although I'll write it up properly once there is more progress and a good path chosen, (currently it is still stabbing in the dark) here are the steps I did so far:

     

    After installing as described above, I used VNC to be able to run graphical applications (another hurdle - nothing is straightforward : ) because the usual tightvnc steps for Linux didn't work, so I had to do this:

     

    apt-get update
    apt-get remove xrdp vnc4server tightvncserver
    apt-get install xrdp tigervnc-standalone-server
    edit /etc/xrdp/xrdp.ini and move the entire Xvnc section above the Xorg section.
    systemctl restart xrdp
    usermod -a -G xrdp machinekit

     

    Then, using Remote Desktop Connection from Windows 10 and connecting to the BBB, in the black screen that appears, right-click to see a pop-up menu and select Terminal Emulator.

    In that window, type machinekit and a configuration menu launches! It has a list of configs displayed, so I scrolled down to ARM->BeagleBone, and chose one.

    image

     

    I've decided to explore the CRAMPS config for now, because I think (not sure) it should be using PRU, and also because it doesn't clash with pins on BBB used for HDMI.

     

    Once selected and saved, a GUI automatically appears to control the (imaginary as yet) CNC machine attached to the BBB (From the GUI it looks like it thinks it is a 3D printer, but other user interfaces are possible - I'm only using this one to experiment).

    The analog pins on the BBB are being used incidentally, because if I put fingers around the end of P9 connector (where the analog inputs reside) the green bar graph readings on the top-right of the screenshot below, move around.

    Anyway, from the GUI, it is possible to power up the imaginary CNC machine, and make it manually move an axis (see red circled areas of the GUI).

    image

    In an earlier comment the file locations was mentioned where the pin numbers are stored. I'm still working on creating a table of them all, it isn't complete, but here's the bit covering the three axes stepper motors for some of them so far:

    image

    According to that, the X-axis stepper motor should be controlled with pulses sent to connector P8 pin 13. This is odd, because if it is using PRU then that pin should not be possible. The PRU is not wired to that pin internally. So, that still needs investigating too (I've seen where in the config the PRU driver code is specified, so I just need to dig a bit deeper). Anyway, for now here's a 'scope trace of what happens to that pin, when the '+' button in the screenshot above is pressed (to try to manually advance the X stepper motor by 1 'unit').

    As can be seen, it is accelerating and decelerating as we would have expected. Longer movement tests will be needed to examine what jitter occurs.

    image

    This is exciting, and gives me more confidence now there is light at the end of the tunnel, and a PCB design can be worked on soon too (after figuring out the PRU stuff, and working on the pin mappings and interfaces).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    With the latest PRU drivers, this command can reveal what firmware is loaded to the PRU0:

    cat /sys/class/remoteproc/remoteproc1/firmware

     

    That firmware - or a symbolic link, is located in /lib/firmware/

    ls -l /lib/firmware/ | grep [firmware filename]

     

     

    ... and this one shows the state (started or stopped)

    cat /sys/class/remoteproc/remoteproc1/state

     

     

    In my case, where I use loaded my own custom firmware to PRU0 and used a symbolic link in /lib/firmware/ instead of copying the binary to that directory:

     

    debian@beaglebone:~/bin$ cat /sys/class/remoteproc/remoteproc1/firmware
    am335x-pru0-fw
    debian@beaglebone:~/bin$ ls -l /lib/firmware/ | grep am335x-pru0-fw
    lrwxrwxrwx  1 root root             35 Aug 17 20:38 am335x-pru0-fw -> /home/debian/bin/bb_PRU_STEPPER.out
    debian@beaglebone:~/bin$ cat /sys/class/remoteproc/remoteproc1/state
    running

     

    By replacing  remoteproc1 with  remoteproc2, you get the status of PRU1.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    With the latest PRU drivers, this command can reveal what firmware is loaded to the PRU0:

    cat /sys/class/remoteproc/remoteproc1/firmware

     

    That firmware - or a symbolic link, is located in /lib/firmware/

    ls -l /lib/firmware/ | grep [firmware filename]

     

     

    ... and this one shows the state (started or stopped)

    cat /sys/class/remoteproc/remoteproc1/state

     

     

    In my case, where I use loaded my own custom firmware to PRU0 and used a symbolic link in /lib/firmware/ instead of copying the binary to that directory:

     

    debian@beaglebone:~/bin$ cat /sys/class/remoteproc/remoteproc1/firmware
    am335x-pru0-fw
    debian@beaglebone:~/bin$ ls -l /lib/firmware/ | grep am335x-pru0-fw
    lrwxrwxrwx  1 root root             35 Aug 17 20:38 am335x-pru0-fw -> /home/debian/bin/bb_PRU_STEPPER.out
    debian@beaglebone:~/bin$ cat /sys/class/remoteproc/remoteproc1/state
    running

     

    By replacing  remoteproc1 with  remoteproc2, you get the status of PRU1.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 7 years ago in reply to Jan Cumps

    Hi Jan,

     

    Thanks for this! That will be helpful for this troubleshooting. When running I don't see any remoteproc1 or 2, just a remoteproc0 running some power management stuff (am335x-pm-firmware.elf), so it seems neither PRU is being used currently : ( However references to PRU are in the initialization file for the config I'm using (it refers to a PRU bin file) so I'll try to debug that later today, see why it isn't being used, and what the code should have done.