Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Allwinner R8 in CHIP: now easier to solder
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 332 subscribers
  • Views 8027 views
  • Users 0 members are here
  • open_source
  • chip
  • oshw
  • open_hardware
  • linux
Related

Allwinner R8 in CHIP: now easier to solder

fustini
fustini over 10 years ago

image

I was excited to see the final production design of the CHIP by Next Thing Co is now using a TQFP package of the Allwinner R8 processor module:

https://www.kickstarter.com/projects/1598272670/chip-the-worlds-first-9-computer/posts/1428989

We've made a change from the smaller R8m (our Alpha C.H.I.P. processor) to the larger R8, which are functionally identical. Because of sourcing complications and repackaging costs for the R8m, we've chosen to move forward with the R8 to remain on time and on budget.

 

Here's what the Alpha CHIP board looked like with the smaller R8 package:

image

 

A big reason that I am a fan of CHIP is that it is Open Source Hardware.  I think the larger R8 package will make it easier for people to design and assemble derivatives.

 

Finally, it's great to see that Linux kernel developer Maxime Ripard of Free Electrons is visitng Next Thing Co.  I'm very encouraged by their progress in getting CHIP supported by the mainline Linux kernel.

https://www.kickstarter.com/projects/1598272670/chip-the-worlds-first-9-computer/posts/1412368

Building an operating system for C.H.I.P. requires some heavy duty driver work. Maxime Ripard from Free Electrons abandoned the French countryside and joined us in sunny Oakland, CA to make sure we’re on-time and feature rich.

 

cheers,

drew

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 10 years ago in reply to gdstew +3
    Gary Stewart wrote: I stand by my original statement, you can't have "open hardware" with closed hardware inside it. GPUs are a particular problem in the ARM SoC world... The official definition…
  • fustini
    fustini over 10 years ago in reply to gdstew +2
    CHIP is Open Source Hardware as the Schematics, Board Layout and Bill of Material are released under an Open Source license . Next Thing Co has written about their approach to Open Source development:…
  • johnbeetem
    johnbeetem over 10 years ago +2
    Glad to see them using TQFP. I really mistrust BGAs. One of my favorite chips was the IBM PPC401GF, a 32-bit PowerPC in an 80-pin PQFP with multiplexed address/data bus. Delightful little easy-to-probe…
Parents
  • gdstew
    gdstew over 10 years ago

    "A big reason that I am a fan of CHIP is that it is Open Source Hardware"

     

    No, the GPU in the R8 is proprietary so you can't use it for anything that the closed drivers don't allow even though the

    compute power of the GPU could be useful for several things other than video output. This violates a basic tenant of

    open source hardware.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 10 years ago in reply to gdstew

    CHIP is Open Source Hardware as the Schematics, Board Layout and Bill of Material are released under an Open Source license.

     

    Next Thing Co has written about their approach to Open Source development:

         https://www.kickstarter.com/projects/1598272670/chip-the-worlds-first-9-computer/posts/1247188

    [We] will be working very closely with Free Electrons and the C.H.I.P. Kernel Hacker backers over the next 6 months to make sure C.H.I.P.'s software is open, standard and most importantly FREE.

     

    Ultimately, our goal is to have as few binary blobs present in the source tree required to use C.H.I.P. as possible. Presently, binary blobs are required for 3 parts of the R8 SoC software stack:

    • ARM Mali 400 Driver (3D graphics acceleration)
    • C2D (2D acceleration)
    • CedarX (Video Hardware Encoding/Decoding)

     

    Our plan is to mainline support for user-space drivers for these binary blobs. But we're also actively exploring ways that we can eliminate the need for these binary blobs altogether. We will also provide Chipsters who want a completely FOSS C.H.I.P. OS builds that are blob-free!

     

    Free Electrons is adding support to the mainline Linux kernel for CHIP including the Allwinner R8: [PATCH 0/5] ARM: sunxi: Introduce CHIP support

     

    They are also upstreaming U-Boot (the bootloader) support: [U-Boot] [PATCH 0/6] ARM: sunxi: Introduce CHIP support

     

    Free Electrons engineer Maxime Ripard posted: "Debian 8 and XFCE running on the CHIP, on top of the DRM / KMS driver!"

    image

     

    For reference:

    • Linux kernel: https://github.com/NextThingCo/CHIP-linux
    • U-Boot: https://github.com/NextThingCo/CHIP-u-boot
    • HW Design Files: https://github.com/NextThingCo/CHIP-Hardware
    • Docs: http://docs.nextthing.co/

     

    cheers,

    drew

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 10 years ago in reply to Problemchild

    The CHIP's Allwinner R8 has a ARM Mali 400 GPU.  Open Source drivers for Mali has been a disappointment thus far.  There is the Lima project but that appears to have lost momentum: http://limadriver.org/

     

    I've heard rumors from Embedded Linux Conf that ARM themselves might make an effort... but who knows if that will happen.

     

    The community wiki for Allwinner SoC notes:

         Linux mainlining effort
         https://linux-sunxi.org/Linux_mainlining_effort#Unlikely

    These are too far off the track third party drivers making it unlikely they will ever get accepted mainline.

    • Mali driver (will not happen unless libv gets a proper lima driver out)

     

    Linux kernel engineer Maxime Ripard replied to me yesterday on Google Plus regarding the DRM / KMS driver:

     

         https://plus.google.com/u/0/107357811086496166266/posts/Bu4VSsKSPuC

    no it doesn't require any blob in userspace, and yeah, it's a pristine Debian Jessie with xfce installed, without any additional configuration
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 10 years ago in reply to fustini

    To followup, Maxime Ripard of Free Electrons commented yesterday about the DRM / KMS driver for CHIP:

    no, it doesn't require any blob in userspace, and yeah, it's a pristine Debian Jessie with xfce installed, without any additional configuration


    For those interested, Maxime previously posted about his Allwinner display driver work:

    I just published my initial work on a DRM/KMS driver for the display engine used on most Allwinner SoCs


    This is his patch set:


        [PATCH 00/19] drm: Add Allwinner A10 display engine support

    The Allwinner SoCs (except for the very latest ones) all share the same set of controllers, loosely coupled together to form the display pipeline.

     

    Depending on the SoC, the number of instances of the controller will change (2 instances of each in the A10, only one in the A13, for example), and the output availables will change too (HDMI, composite, VGA on the A20, none of them on the A13).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 10 years ago in reply to johnbeetem

    Good explanation, johnbeetem.

     

    The Open Source Hardware Certification Version 1 announced in September by OSHWA considers the level of abstraction issue:

    many well-known open source hardware projects and products strive towards openness but, by necessity, incorporate non-open components. The open source hardware definition recognizes this reality, and provides guidance on how best to handle non-open components in the context of open source hardware.

     

    It goes on to state:

    For the purposes of the certification, openness will be determined by the openness of the contribution made by the creators of the project.  A certified project will be required to share its entire contribution (including the contribution of affiliated corporate entities, if appropriate) in accordance with the open source hardware definition, but not expected to avoid third party closed components beyond its control.

     

    The certification was introduced by OSHWA President Michael Weinberg at the Open Hardware Summit 2015.

    Skip to 1h18m in the video:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    My long term hope is that we will someday have Open Source Hardware at the silicon level from efforts like lowRISC and J Core.

     

    This does also remind me of a very interesting talk from John Sarik & Haig Norian of Columbia University at OHS 2012:

    Open Sourcing the Integrated Circuit [PDF]

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • pettitda
    pettitda over 10 years ago in reply to fustini

    I have to agree with @gdstew.  It's not open source hardware if it includes proprietary hardware components.  After all, what good is the hardware if you can't write software to run on it!  You can define OSHW any way you please, but in the end the plain English meaning rules in my opinion. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 10 years ago in reply to pettitda

    David Pettit wrote:

     

    I have to agree with @gdstew.  It's not open source hardware if it includes proprietary hardware components.  After all, what good is the hardware if you can't write software to run on it!  You can define OSHW any way you please, but in the end the plain English meaning rules in my opinion.

     

    There is a specific definition for Open Source Hardware.  This OSHWA blog post sheds light on how that defination was developed by a community of people creating Open Source Hardware:


        Brief History of Open Source Hardware Organizations and Definitions

        http://www.oshwa.org/research/brief-history-of-open-source-hardware-organizations-and-definitions/

     

    All Open Source Hardware projects and products that I know of include proprietary hardware components: Arduino uses Atmel AVR microcontroller; BeagleBone uses TI Sitara SoC; MinnowBoard uses Intel Atom processor; etc.  I hope that lowRISC will someday provide a physical Open Source processor.

     

    The TI Sitara AM3358 SoC in the BeagleBone Black also has a GPU with no Open Source drivers (Powever SGX).  This is a bummer but I've never actually needed GPU acceleration on the BBB.  The BBB works fine with U-Boot and mainline Linux kernel.

     

    I think that CHIP is in the same situation.  Free Electron engineers along with the Sunxi community are upstreaming CHIP support to U-Boot and mainline Linux kernel.  It would be great to have Mali-400 drivers, but the GPU is not essential to the system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 10 years ago in reply to fustini

    Closed is not open

    War is not peace

    ...

     

    As I said they ignore the obvious in their definition because otherwise nothing using ARM SoCs is truly open hardware. They can define it (or hide it away) any way they want,

    that does not make it open hardware. And it clearly violates the most basic principle of real open hardware.

     

    The AVR hardware is fully documented. A lot of the TI Sitara SoC is fully documented, part of it (the closed hardware GPU part) as you so obviously get is not.

     

    As I stated in the first post, the processing power of GPUs can be used for purposes other than just graphics acceleration but only if they are fully documented. Image processing,

    especially in robotics where you don't need video output and could use the fully capable hardware acceleration in the GPU if only it were open, and fast FFTs (it has been done

    with RPi since it has an open GPU) are two examples. I am sure that there are more and that there are more than a few people, myself included that do not share your very

    limited ideas as to what is and what is not essential hardware in their designs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 10 years ago in reply to gdstew

    A key concept of Open Source Hardware  is the ability to create derivatives.  This is possible with an OSHW board like the BeagleBoard as the schematics, board layout and BOM are published with an Open Source license.  It was also designed to use components that are available in single quantity.  This has resulted in an ecosystem of derivatives including Seeed's BeagleBone Green, Autodesk's Ember, Outernet's Latern and SanCloud.

     

    This discussion though does remind me of the Free Software Foundation's  "Respects Your Freedom" certification program:

    All the product software must be free software. The product software includes all software that the seller includes in the product, or provides with the product, or recommends for use in conjunction with the product, or steers users towards installation in the product.

    The goal is ensure user freedom and is not concerned with whether the hardware is proprietary.  In fact, the list of certified hardware includes only one product that is Open Source Hardware (Lulzbot TAZ 3d printer).  The only products in the list with GPUs are laptops with integrated Intel graphics, for which there is Open Source GPU driver.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to fustini

    Hi Drew,

     

    I interview to this discussion because I think it is interesting for those who reads without creating a new one. If the arguments become more complex I will open later, but I think you should be involved as per your knowledge in the OSHF. As I mentioned in many other posts the project Meditech is coming to be a "product" aiming to be entirely open for a lot of reasons, first of all the kind of usage. How do you think it is possible to release a product, that is also the result of an integration of different ones, some commercial and some other custom, making it open but maintaining the same sustainable market approach the I have initially provided? Are there specific links between the marketing aspects and the fact that the product is open? You can build, make (maybe) derivatives but you must sell and distribute it at certain specific conditions.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to gdstew

    Gary Stewart wrote:

     

    As I stated in the first post, the processing power of GPUs can be used for purposes other than just graphics acceleration but only if they are fully documented. Image processing, especially in robotics where you don't need video output and could use the fully capable hardware acceleration in the GPU if only it were open, and fast FFTs (it has been done with RPi since it has an open GPU) are two examples. I am sure that there are more and that there are more than a few people, myself included that do not share your very limited ideas as to what is and what is not essential hardware in their designs.

    It's terrific that Broadcom has released documentation for the VideoCore IV GPU in RasPi's BCM2835/36.  That's great for open-source software, but on the other hand you can't buy BCM2835/36 chips in small quantities so you can't design small-scale projects that use BCM2835/36 chips -- you have to incorporate a RasPi as a module.  This is a typical quandry in the open-source world: you can get open-source software or open-source hardware, but not both at the same time.

     

    In an ideal world, you would have a choice of fully-documented GPUs and FPGAs.  However, what is documented is up to the silicon vendors which means reality is not ideal and creators of FLOSS and OSHW need to be pragmatic and take advantage of what open-ness can be achieved.  There are many excellent FLOSS and OSHW products out there that are useful even if they're not 100% open.  Using them helps move us up the long road towards the 100% ideal.

     

    Meanwhile, IMO it's important to define clearly what it means to be FLOSS and OSHW today.  Complaining that the definitions aren't "truly open" isn't very helpful IMO, since there aren't "truly open" products available in important sectors.  The established definitions clearly state what users and developers can do with FLOSS and OSHW, and IMO that's very useful.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 10 years ago in reply to fustini

    Thanks for not addressing any of my points in any way with your reply.

     

    The ability to create derivatives is easily available with only a schematic which is why, along with debugging, I call them an essential part of open hardware.

    I have never seen any derivative product (there may be a few out there) that actually uses the board layout of the original because they usually try to

    differentiate themselves from the original in some way. The BeagleBone Green along with most Aurduino derivatives, many of which do not even use the

    AVR processor, are excellent examples. A BOM is a nice time saver but hardly essential in creating a derivative product.

     

    As you point out the definition of open hardware by the OSHW mostly helps those that may be interested in creating derivative products. Other than requiring

    that schematics be provided (which some products that are not OSHW "approved" also do) it does not provide any advantage to people that want to use the

    product and yet it is constantly used in a way that infers, and sometimes outright claims that it does.

     

    The freedom to use any original or derivative hardware in a way in which may or may not be envisioned by the creator of a product does require that all the

    hardware be open. Calling anything else open hardware as if it is an advantage to the user is deceptive at best.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 10 years ago in reply to fustini

    Thanks for not addressing any of my points in any way with your reply.

     

    The ability to create derivatives is easily available with only a schematic which is why, along with debugging, I call them an essential part of open hardware.

    I have never seen any derivative product (there may be a few out there) that actually uses the board layout of the original because they usually try to

    differentiate themselves from the original in some way. The BeagleBone Green along with most Aurduino derivatives, many of which do not even use the

    AVR processor, are excellent examples. A BOM is a nice time saver but hardly essential in creating a derivative product.

     

    As you point out the definition of open hardware by the OSHW mostly helps those that may be interested in creating derivative products. Other than requiring

    that schematics be provided (which some products that are not OSHW "approved" also do) it does not provide any advantage to people that want to use the

    product and yet it is constantly used in a way that infers, and sometimes outright claims that it does.

     

    The freedom to use any original or derivative hardware in a way in which may or may not be envisioned by the creator of a product does require that all the

    hardware be open. Calling anything else open hardware as if it is an advantage to the user is deceptive at best.