• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56074 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • fmilburn
    fmilburn over 6 years ago

    Hi Ken,

     

    This is a very interesting project with great comments from Michael and Shabaz  I did not realize how low the soil resistance typically is.  Wikipedia gives the usual values to be from 10 up to 1000 (Ω-m) though sometimes higher.

     

    https://en.wikipedia.org/wiki/Soil_resistivity

     

    I am jumping ahead but assuming the typical user would be an enthusiast building this themselves as a diy project, open source.  If so, that would influence the choice of components, complexity and cost. Can you describe in a bit more detail your thoughts on that?


    Frank

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to fmilburn

    Hi Frank

    yes as you have guessed I am an enthusiast building this for myself. I belong to an amateur archaeology group and we do have access to an RM Frobisher unit, although this is somewhat restricted. We quite often carry out surveys for other groups who don’t have access to equipment, mainly because of cost. The RM Frobisher unit is in the region of £3000 currently, and that’s about the going price for this sort of equipment. To my mind it’s heavily overpriced for what it is. You will see that the ball park cost figure put in on the article by Robert Beck is about £50.00, but that was 1997. I reckon on today’s prices I could put that at maybe £150 to £200. In use the RM Frobisher unit is fairly automatic. Place the probes at C1 R1 and it takes a reading and beeps to let you know, then lift the probes and place them in C1 R2 and so on up to 20. At the end of the row there is a double beep and you would swing round and put the probe in C2 R20 and come back down. At the end of the grid there is long beep, the unit then saves all the readings to sd card and shuts down. There is facility in the software to mark trees and other obstructions as dummy readings. The one criticism I have is the menus in the software are poorly written.
    The biggest shortfall in the current offerings is not having a live view. A simple on screen grid that would be populated as readings are taken. We currently have to post process usually that evening so you have no idea what you have until then. Sometimes on a grid you will have an area of interest. With these we would go back over that section, but increase the number of readings to every half a meter to improve the resolution. Easier to do when your all set up. Anyway this should hopefully give you a flavour of what’s required. The majority requirement will be in the software I guess, but I can play at that. I don’t think the electronics are that sophisticated, but they could certainly do with being updated.
    Ken

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett

    @Frank Milburn

     

    The example I had wasn't so helpful when I looked at it so I'll go through the numbers using the AD7195. I'll assume we use a software DDS running on a STM32F4xx using the on chip DAC.

     

    We want operating frequencies of 20Hz - 200Hz, ideally with 1Hz or better precision for the test signal - we'll call this frequency Fts

     

    We want a sampling rate of about 1000 samples per second for ADC and DAC (so we can use one antialiasing filter for all operating frequencies).

     

    The ADC samples at: Fadc = Fclk/(1024 × FS[9:0]) - so we could set Fclk at 4096000 Hz and FS[9:0} (which is a register in the ADC) to 4.

    We don't expect to make measurements over only one test signal cycle, the more we include the narrower the bandwidth we will detect.

    Let's say we sample N cycles in each test period and that there are S samples per test.

    We want an integer number of cycles in each test period (this is less important when N gets very large)

    So we can say Fts = Fadc * N / S

    Fadc = 1000

     

    So Fts = 1000N / S

     

    Since we can set N over quite a wide range there are many possibilities - if we set N = 100 we can get within about 0.2Hz at 200Hz and better at lower frequencies.

     

    Probably a 409600 Hz clock is a bad idea, because we shall want to make it an integer fraction of the processor clock - so 4.00 MHz is fine, it does mean that can't set

    exactly 200Hz  but we can get very close.

     

    AN STM32L4R5VGT6 looks like a good bet for the processor - this can run at a core speed of 120MHz so it can easily provide a 4.0 MHz timer signal for a clock.

    It has dual 12 bit DACs which can produce the DDS test signal under DMA control.

    The system needs a single clock for the processor and everything is synched from this.

    The ADC on the micro isn't used - it may well be possible to interface the AD7195 without an FPGA - I haven't checked that (yet).

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to michaelkellett

    Hi Michael Not sure about the frequencies in use. Is this the frequency of the square wave to generate pseudo AC. If so the original article talks about 137Hz  being the ideal, because of possible interference from 50/60Hz mains hum, and the need to filter out these frequencies later.
    Not sure if i’m right or talking rubbish. Slap my wrists if I am.
    I’ve also seen talk of LTSpice for simulation. I have used this, but quite a while ago. I’ll download it again and try to follow what you are doing.

    All very interesting and once again thank you.

    Ken

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    This is the test signal but it really should not be a square wave but a sine wave - the design I'm suggesting uses sine waves and decodes the measured signal by multiplying by sin and cos rather than +/- 1.

     

    (I know that the DIY design uses a square wave and possibly some commercial devices do but it is a very bad idea. - with modern processors and electronics there really is no justification for not using a sine wave.

    A square wave generator and rectangular de- modulator is sensitive to odd harmonics of the operating frequency - which makes it much harder to pick a good operating frequency.)

     

    There is no perfect frequency -  the best to use depends on local interference conditions so I'm suggesting be able to set the frequency in the range 20Hz to 200Hz which more than covers the range that most commercial devices offer.

     

    Re. the FPGA - it may not be necessary image

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to michaelkellett

    Thanks Michael, good explanation. I get it now.  Simpler than I thought.


    EDIT:  that is, simpler except for the FPGA :-). I’ve never used FPGAs.


    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to fmilburn

    I'm hoping this application can avoid an FPGA, the ADC can talk directly to the processor - it'll need an interrupt every 1ms but the 120MHz STM32l4xxxx can cope with that.

     

    But happy to help put an FPGA in just for the fun of it image

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hehe my vote is stick the FPGA in : )

    It could be nice to offload that portion, gets people more interested in FPGA, plus the processor code will be slightly simplified and more portable for future people to use different or less performance devices or experiment/modify. In theory since then there's very little timing concern for the processor, some people could rip out the processor and use a Pi and a process on Linux (not that I'm suggesting it is a good idea, but technically possible) to prototype code enhancements too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    A nice little Lattice FPGA would be OK, not expensive, they only need about 100k of flash in the processor to hold the map, so no extra flash chips required.

    The tools are much easier than Xilinx.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    I downloaded the Lattice software last night, and tested putting the default blinky LED bitstream onto the ICEstick board, now planning to run through a tutorial to get some practice with the tools : )

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to michaelkellett

    Oh well... another shiny object to distract me image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to fmilburn

    I’m just trying hard to keep up.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kltm
    kltm over 6 years ago in reply to fmilburn

    I’m just trying hard to keep up.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    I think the best FPGA would be the ICE40UP5K - 48 pin QFN package so home solderable. £4.80 from Mouser , supported by Radiant software, has RAM blocks, 1Mbit SRAM and multipliers on chip.

    And even better I've used them before image

     

    Are enough people interested in this to get together and buy some boards ?

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    I'd happily do so for a set of boards, and help in areas where I can contribute. The technical challenge is interesting..

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to michaelkellett

    I am in - sounds like a good learning opportunity and I will help where I can.  I just did a search for the ICE40HX1K-STICK-EVNICE40HX1K-STICK-EVN and can’t find it in stock in the usual places - Newark, Digikey, Mouser.  I was thinking to order the STM NUCLEO-L4R5ZI as well so as to have dev boards to play with.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to michaelkellett

    I’ll certainly like to try with the boards, I’ve got a lot of learning to do.