• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56232 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • kltm
    kltm over 6 years ago

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to kltm

    Hi Michael,

     

    I had these initial thoughts, but I've not had time to think things through (I have some time late Wednesday to do that):

    There was mention of more sense probes, but maybe the expansion interface is sufficient for that, since one could drive (say) a latching relay via that. Or maybe space for on-board relay?

    A minor point was, for the USB UART, for MCP2221 I already have Android code. But FTDI is totally fine too, i.e. if you've already got the schematic entered for that portion then it's quicker for me to just hunt for demo code for FTDI, if you let me know the chip number. Below is the the schematic I've used previously for the MCP2221 (it needs an external 3.3V regulator which probably the FTDI device doesn't, and has 4kV protection which likely isn't enough, I didn't place any additional ESD protection on this schematic).

     

    One other thought was for a test facility, if there was were four jumpers or four DIP switches on the board which would connect a potential divider across the source (two switches for that) and two switches to connect the sense wires to the divider. Maybe jumpers are easier. But probably there will be test points on the board for easy soldering of a mini test harness during software development anyway.

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Hello, I had a bit of time left at the end of today and installed the MbedStudio I had downloaded.

    That was the good bit, then I tried to run it - OMG - what a disapointment !

    It flouts all the usual windows standards of look and feel so I found it a total pig to navigate, It doesn't have functional Help in the usual way.

    There is a help itme in the menu bar but it doesn't provide a normal Help facility at all.

    I got it to load up the "bare metal blinky" example - which is still a .cpp file relying on an OS. It included masses of odd files (including things like CAN drivers).

    And worst of all it doesn't build - there are errors relating to some deprecated legacy file (writing from home now so  I don't have it in front of me.)

    That's when the lack of Help really bit - I couldn't work out how to close the current project and open a new example file - aargh - then it was time to go home.

     

    This evening I downloaded the ST CubeIDE.

    I am familiar with the Cube thing for setting up pins  and clocks. The clock thing is actually quite useful. The way the ST tools "organise" the generated code is disgusting,

    But that's OK - you just put things somewhere sensible.

    The generated code compiles witout errors.

    And of course the IDE is Eclipse so looks and behaves like we've all got used to.

    The Help still isn't a patch on Keil's but it does a good bit more then the Mbed.

     

    So on the basis of this very quick and quite unfair test - I'm going to play more with the ST tools.

     

    I'm very keen to hear if you can get the Blinky to work on Mbed.

    (Is there a way of keeping it to C or Mbed fundamentally C++)

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to michaelkellett

    I compiled the blinky for OS6 on mbed studio for your board and it compiled correctly. See small screen capture I posted above.

     

    I too prefer the Eclipse way of working more than MBED Studio. But not that much more that it would decide a way forward.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

     

    I've not used MbedStudio, but Mbed capability is also a bunch of Python scripts replacing the usual Makefile. I've used that (on Linux, but in theory workable with Windows), i.e. using any text editor (e.g. Visual Code) and then using the command line to run the script to build the project, and another command to program the board. It's possible to create a script, i.e. type something like ./install in order to flash the device. Visual Code allows the command line to be dispensed with, but it's just a preference thing.

     

    The language when working with Mbed is partially C++, the main benefit is the libraries are nice (they're high-level, since the same APIs have to work with other manufacturer devices too). Some of the APIs use C++ functionality however, so typing in pure C is not possible.

     

    I'm currently writing some ideas on paper, at first thought there seems to be about 8 'work areas' a user might want to get involved with, and each seems to be separate so that can make things easier, i.e. launch into any work area based on user input or otherwise. But I'll probably focus on the core area first (calling it Survey for now) since by trying to design that (on paper) it will force me to concentrate on the important bits of the main functionality, so that code for testing bits of hardware is quicker to be done.

    Also, if you know which Flash chip you want to use, I can order that too, so I can play with getting some basic file method to meet all the workflow areas to the extent of being enough for a prototype.

    The ideas so far are (not really user stories, just very brief half-baked brainstorming, I've only spent 10 mins on it so far : )

    image

    image

     

    EDIT:  From Jan's screenshot it looks like ARM have implemented MbedStudio on top of a modification of Microsoft Visual Code, the icons and layout look very similar.

    I wasn't originally a fan of Visual Code, but it's flexible to a lot of coding tasks, and so many coders use it now, that it's likely to remain around for ages. I like that it's extremely expandable, but there's definitely a learning curve to it - lots is unconventional with it : (

    I used to use the paid 'UltraEdit' but it offers low value now that Visual Code is around.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to Jan Cumps

    Thanks for note.

    Here's a bit of the Mbed console output during compile:

    Building project mbed-os-example-blinky-baremetal (NUCLEO_L4R5ZI, ARMC6)
    Scan: mbed-os-example-blinky-baremetal
    Compile [  0.4%]: mbed_tz_context.c
    Compile [  0.8%]: AnalogOut.cpp
    Compile [  1.2%]: AnalogIn.cpp
    
    ABOUT 240 other compiled files skipped !!!!!!!
    
    Compile [ 99.2%]: USBPhy_STM32.cpp
    Compile [ 99.6%]: trng_api.c
    Compile [100.0%]: watchdog_api.c
    Link: mbed-os-example-blinky-baremetal
    [Warning] @0,0: L3912W: Option 'legacyalign' is deprecated.
    [Error] @0,0: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Base (referred from BUILD/NUCLEO_L4R5ZI/ARMC6/mbed-os/platform/source/mbed_sdk_boot.o).
    [Error] @0,0: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Limit (referred from c:\ProgramData\Mbed Studio\mbed-studio-tools\ac6\bin\..\lib\armlib\mc_w.l(malloc2.o)).
    [Error] @0,0: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Length (referred from BUILD/NUCLEO_L4R5ZI/ARMC6/mbed-os/platform/source/mbed_sdk_boot.o).
    Warning: L3912W: Option 'legacyalign' is deprecated.
    Error: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Base (referred from BUILD/NUCLEO_L4R5ZI/ARMC6/mbed-os/platform/source/mbed_sdk_boot.o).
    Error: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Limit (referred from c:\ProgramData\Mbed Studio\mbed-studio-tools\ac6\bin\..\lib\armlib\mc_w.l(malloc2.o)).
    Error: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Length (referred from BUILD/NUCLEO_L4R5ZI/ARMC6/mbed-os/platform/source/mbed_sdk_boot.o).
    Finished: 0 information, 1 warning and 3 error messages.
    [ERROR] Warning: L3912W: Option 'legacyalign' is deprecated.
    Error: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Base (referred from BUILD/NUCLEO_L4R5ZI/ARMC6/mbed-os/platform/source/mbed_sdk_boot.o).
    Error: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Limit (referred from c:\ProgramData\Mbed Studio\mbed-studio-tools\ac6\bin\..\lib\armlib\mc_w.l(malloc2.o)).
    Error: L6218E: Undefined symbol Image$$ARM_LIB_HEAP$$ZI$$Length (referred from BUILD/NUCLEO_L4R5ZI/ARMC6/mbed-os/platform/source/mbed_sdk_boot.o).
    Finished: 0 information, 1 warning and 3 error messages.

     

    Notice that this "bare metal" blinky compiles more than 240 files !!!

     

    The actual Blinky is this:

     

    /* mbed Microcontroller Library
     * Copyright (c) 2019 ARM Limited
     * SPDX-License-Identifier: Apache-2.0
     */
    
    #include "mbed.h"
    
    #define WAIT_TIME_MS 500 
    DigitalOut led1(LED1);
    
    int main()
    {
        printf("This is the bare metal blinky example running on Mbed OS %d.%d.%d.\n", MBED_MAJOR_VERSION, MBED_MINOR_VERSION, MBED_PATCH_VERSION);
    
        while (true)
        {
            led1 = !led1;
            thread_sleep_for(WAIT_TIME_MS);
        }
    }

     

    I have about a million problems with this but the main ones are:

     

    Even a simple project is dependent on literally hundreds of unknown files - an error in any one of them will break it.

     

    Its typical of what I would call 2nd decade code - everything slowly percolates down to the hardware though layer upon layer of abstraction (obfuscation !).

     

    The error is typical of this approach - I have no idea why we need to build mbed_sk_boot or what legacyalign was meant to do, (or how it can be wrong in example code) !

     

     

    I come from a hardware for mass production/ high reliability back ground and I aim for:

     

    • Every line of code should be embedded in the project itself, so it can be rebuilt, byte accurate, 10 or 20 years later.
    • Every line of code should be traceable to a requirement in the specification (rarely met except in aerospace but a good goal).
    • There should be no dead code.
    • The code should be as simple as possible, for example timers should be set up by direct control register writes, rather than through some opaque API call
    • which has stuff to work 100 timer features not present on the hardware you are working.

    It seems to me that the Mbed approach is aiming for a sort of baby Linux on embedded processors - there will be places where that is a good thing but it's not the route I would choose for this project.

     

    Having said that, if others really want to go that way, I won't throw my toys out of the pram.

     

    The core code on the processor needs to be able to set up some circular buffers for data from its own and the external ADCs and DACs and DMA for SPI to the FPGA and for the internal ADCs and DACs.

     

    It will have to support regular maintenance of these buffers - probably at a faster rate than a typical OS tick rate.

     

    I'm assuming that the  Mbed OS will support this (although a super loop would do it better and more transparently image) so I can't see why the thing shouldn't work in Mbed.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to michaelkellett

    Michael, I think you will like the CubeIDE approach more (or dislike less image ).

    There's still a HAL above the register layer, but a more traditional one.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to Jan Cumps

    Yes, you are quite right.

     

    And although I don't like the HAL I know it well - so I use it but mostly as a reference, but sometimes as intended.

     

    There is a lightweight HAL but I don't think you can make the Cube tools generate a project based on it.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael and Rob,

     

    Sorry you had a bad experience with this.

    My current status is to try the code design as a paper exercise, and then some skeleton using the ST dev environment, but I'll simultaneously get code running on Mbed too if I can, just in case.

     

    The architecture can be nicer with the OS, but I'll use a more traditional implementation with the ST dev environment.

     

    Two bits of reference code could be a benefit, I cannot tell how large and how many features could be desired for later add-on. 

    Mbed is C/C++, so direct writing to registers etc isn't an issue. The Mbed benefits are the diverse libraries for adding new features and the task handling (and it works well with interrupt handling) that is available.

     

    I've been involved with bare-metal mil-customer projects too, custom-written RTOS, and Linux+huge middleware+C++ (which suits a very different sized project). I am excited about (say) one day add-ons (such as sending data in real-time via a network, or adding different tasks) then Mbed has got a lot covered, but it's unnecessary for the core functions.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    That's a weird error, the output shows that MbedStudio is defaulting to an ARM-supplied compiler. With Linux, I can default to GCC with Mbed.

    Bad that MbedStudio didn't work by default though.

     

    I tried to compile the blinky on Linux with Mbed with GCC, and the particular errors in your comment refers to symbols in particular files, but the GCC-made version of the file I checked doesn't contain that symbol at all.

     

    Regarding unwanted code, it is possible to delete some of it (for instance unused peripheral code), but by default Mbed will add it.

    This is output for the blinky project on the command line with Linux, it's interesting to see which things took the code space (there is a normal map output too, this is just the summary output on the command line after the build).

    The output shows the C library used almost half the total code, and about 13 kbytes was used for the basic peripherals (mbed-os/targets entry), OS consumed 6 kbyte, and the user-typed blinky code took 80 bytes, etc. I think this is reasonable (and no messing about having to struggle with 'lighter' versions with reduced printf formatting etc., but is a shift from only having code in there that is known to execute (but as you say that's rare to accomplish).

     

    | Module           |         .text |       .data |        .bss |
    |------------------|---------------|-------------|-------------|
    | [fill]           |     102(+102) |       8(+8) |     19(+19) |
    | [lib]/c.a        | 27372(+27372) | 2472(+2472) |     89(+89) |
    | [lib]/gcc.a      |   3116(+3116) |       0(+0) |       0(+0) |
    | [lib]/misc       |     180(+180) |       4(+4) |     28(+28) |
    | mbed-os/drivers  |     174(+174) |       0(+0) |       0(+0) |
    | mbed-os/hal      |   1672(+1672) |       8(+8) |   130(+130) |
    | mbed-os/platform |   4228(+4228) |   260(+260) |   280(+280) |
    | mbed-os/rtos     |   6880(+6880) |   168(+168) | 6228(+6228) |
    | mbed-os/targets  | 13320(+13320) |       8(+8) | 1078(+1078) |
    | test.o           |       80(+80) |       0(+0) |     28(+28) |
    | Subtotals        | 57124(+57124) | 2928(+2928) | 7880(+7880) |
    Total Static RAM memory (data + bss): 10808(+10808) bytes
    Total Flash memory (text + data): 60052(+60052) bytes
    
    
    Image: ./BUILD/NUCLEO_L4R5ZI/GCC_ARM/testprog.bin

     

    Anyway, I'll concentrate on the high-level code design, this was just out of curiosity to check the ST-targetted Mbed can work on linux.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    I built the bare metal one on a windows box and got the same errors as Michael:

    image

     

    It's a brand new MBED Studio install from last weekend, not fiddled with any settings.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to Jan Cumps

    Nice to know it's not just me !

     

    I have my Nucleo board so I'll see if it will play with the ST tools.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 6 years ago in reply to Jan Cumps

    Nice to know it's not just me !

     

    I have my Nucleo board so I'll see if it will play with the ST tools.

     

    MK