• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56245 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • kltm
    kltm over 6 years ago

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to kltm

    Hi Michael,

     

    I had these initial thoughts, but I've not had time to think things through (I have some time late Wednesday to do that):

    There was mention of more sense probes, but maybe the expansion interface is sufficient for that, since one could drive (say) a latching relay via that. Or maybe space for on-board relay?

    A minor point was, for the USB UART, for MCP2221 I already have Android code. But FTDI is totally fine too, i.e. if you've already got the schematic entered for that portion then it's quicker for me to just hunt for demo code for FTDI, if you let me know the chip number. Below is the the schematic I've used previously for the MCP2221 (it needs an external 3.3V regulator which probably the FTDI device doesn't, and has 4kV protection which likely isn't enough, I didn't place any additional ESD protection on this schematic).

     

    One other thought was for a test facility, if there was were four jumpers or four DIP switches on the board which would connect a potential divider across the source (two switches for that) and two switches to connect the sense wires to the divider. Maybe jumpers are easier. But probably there will be test points on the board for easy soldering of a mini test harness during software development anyway.

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to shabaz

    I don't have the Nucleo board just yet (ordered it today), but I had a F746G board (quite powerful too!) and out of curiosity I tried running a filter. It was unfortunately unrealistic (I pretended to sample at 10kHz, which was a typo, I'd wanted 1 kHz) but the results were nice.. with 255 coefficients though!

    This was the expected result (simulating 5Hz wanted in red (would be zero Hz wanted of course), and 82 Hz unwanted, with a cut-off at 10 Hz (unrealistic amplitudes too, since the wanted signal could be much smaller than the unwanted):

    :image

    and this was the result with mbed-dsp (guessing is just a wrapper of CMSIS DSP functions, so should be identical to doing it on the ST environment, I just have not investigated that yet). This was with printf to output the values to a serial terminal, and then put them in matlab to plot them) - blue is output, and green was the expected result, I didn't plot them aligned:

    image

    I didn't get any timing since this was just a late-night coding experiment, but it's extremely impressive how much processing power these devices have. To think this wasn't possible with low-power microcontrollers maybe just a decade ago.

     

    It will be better to use Matlab tools I guess for designing the filter (I'm not knowledgeable on filter design at all) and for now the filter was calculated using a Python program found online (can write that up). Anyway this is all premature coding experimentation, but does give comfort that ARM DSP capabilities are nice!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    There has been an ominous silence since I published the input amplifier design a couple of weeks ago.

     

    (You can find it by searching the armp tag.)

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to michaelkellett

    Hi Michael I think it’s back to the problem of us requiring a group. There is certainly a lot of work in there thank you. I will try and set it up in LT Spice.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 6 years ago in reply to kltm

    Content marked with the tag is also highlighted on the overview page of this group, it'll show up to 20 items, at the moment there's about.. 5.

     

    Shabaz has also discussed with the developers on how to follow tags: Tags function issue/change request to list all content with a tag which should help.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

     

    Sorry for the feedback delay.

    I saw the post, and wished to look at it, but have not had as much time as hoped this week.

    However, I get a lot more free from tomorrow evening, so I will look through it then!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    That's OK, I just need to feel that there is enough enthusiasm to carry the thing forward.

     

    kltm, it'll be hard to model exactly in LT spice because the amplifiers are TI parts, they won't make much difference so use an AD part that looks close (or the Universal Op Amp model)

     

    I've got an LT Spice of some of it which I've added here.

     

    Version 4
    SHEET 1 1916 864
    WIRE 224 -160 80 -160
    WIRE 224 -128 224 -160
    WIRE 192 -112 -160 -112
    WIRE 304 -96 256 -96
    WIRE 400 -96 304 -96
    WIRE 528 -96 480 -96
    WIRE 560 -96 528 -96
    WIRE 192 -80 144 -80
    WIRE 304 -48 304 -96
    WIRE 224 -32 224 -64
    WIRE 224 -32 64 -32
    WIRE 144 64 144 -80
    WIRE 304 64 304 32
    WIRE 304 64 144 64
    WIRE 1280 112 1024 112
    WIRE 80 144 80 -160
    WIRE 656 144 80 144
    WIRE 656 176 656 144
    WIRE 528 192 528 -96
    WIRE 624 192 528 192
    WIRE 832 192 768 192
    WIRE 960 192 912 192
    WIRE 1072 192 960 192
    WIRE 1200 192 1152 192
    WIRE 768 208 768 192
    WIRE 768 208 688 208
    WIRE 624 224 528 224
    WIRE 1024 240 1024 112
    WIRE 64 272 64 -32
    WIRE 656 272 656 240
    WIRE 656 272 64 272
    WIRE 960 288 960 192
    WIRE 992 288 960 288
    WIRE 1200 288 1200 192
    WIRE 1200 288 1152 288
    WIRE 992 320 928 320
    WIRE 560 336 560 -96
    WIRE 304 352 144 352
    WIRE 992 352 960 352
    WIRE 1200 352 1152 352
    WIRE 304 384 304 352
    WIRE 64 416 64 272
    WIRE 224 416 64 416
    WIRE 832 448 816 448
    WIRE 960 448 960 352
    WIRE 960 448 912 448
    WIRE 1072 448 960 448
    WIRE 1200 448 1200 352
    WIRE 1200 448 1152 448
    WIRE 224 464 224 416
    WIRE 144 480 144 352
    WIRE 192 480 144 480
    WIRE 304 496 304 464
    WIRE 304 496 256 496
    WIRE 400 496 304 496
    WIRE 528 496 528 224
    WIRE 528 496 480 496
    WIRE 624 496 528 496
    WIRE 768 496 768 208
    WIRE 768 496 704 496
    WIRE 192 512 -48 512
    WIRE -160 544 -160 -112
    WIRE -48 544 -48 512
    WIRE 80 560 80 144
    WIRE 224 560 224 528
    WIRE 224 560 80 560
    WIRE 928 576 928 320
    WIRE 560 592 560 416
    WIRE 64 608 64 416
    WIRE 224 608 224 560
    WIRE 1280 608 1280 112
    WIRE -160 640 -160 624
    WIRE -112 640 -160 640
    WIRE -48 640 -48 624
    WIRE -48 640 -112 640
    WIRE -112 656 -112 640
    WIRE -112 752 -112 736
    WIRE -112 752 -160 752
    WIRE 64 752 64 688
    WIRE 64 752 -112 752
    WIRE 224 752 224 688
    WIRE 224 752 64 752
    WIRE 352 752 224 752
    WIRE 560 752 560 672
    WIRE 560 752 352 752
    WIRE 816 752 816 448
    WIRE 816 752 560 752
    WIRE 928 752 928 640
    WIRE 928 752 816 752
    WIRE 1024 752 1024 400
    WIRE 1024 752 928 752
    WIRE 1280 752 1280 688
    WIRE 1280 752 1024 752
    WIRE 352 784 352 752
    FLAG 352 784 0
    SYMBOL Opamps\\UniversalOpamp2 224 -96 M180
    SYMATTR InstName U1
    SYMBOL Opamps\\UniversalOpamp2 224 496 R0
    SYMATTR InstName U2
    SYMBOL res 496 -112 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R3
    SYMATTR Value 6K
    SYMBOL res 496 480 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R4
    SYMATTR Value 6K
    SYMBOL res 288 368 R0
    SYMATTR InstName R8
    SYMATTR Value 1k
    SYMBOL res 288 -64 R0
    SYMATTR InstName R9
    SYMATTR Value 1k
    SYMBOL voltage 64 592 R0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V2
    SYMATTR Value 16
    SYMBOL voltage 224 592 R0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V3
    SYMATTR Value -16
    SYMBOL voltage -48 528 R0
    WINDOW 3 -130 -53 Left 2
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR Value SINE(0 15 100 0 0 180)
    SYMATTR InstName V4
    SYMBOL voltage -160 528 R0
    WINDOW 3 -182 -3 Left 2
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR Value SINE(0 15 100)
    SYMATTR InstName V5
    SYMBOL voltage -112 640 R0
    WINDOW 3 -182 -3 Left 2
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR Value SINE(0 .01 2)
    SYMATTR InstName V8
    SYMBOL Opamps\\UniversalOpamp2 656 208 M180
    SYMATTR InstName U3
    SYMBOL res 720 480 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R1
    SYMATTR Value 1K
    SYMBOL res 544 320 R0
    WINDOW 3 47 73 Left 2
    SYMATTR InstName R2
    SYMATTR Value 1K
    SYMBOL voltage 560 576 R0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V1
    SYMATTR Value 0
    SYMBOL Opamps\\LTC6362 1056 320 R0
    SYMATTR InstName U4
    SYMBOL res 1168 432 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R5
    SYMATTR Value 1K
    SYMBOL res 1168 176 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R6
    SYMATTR Value 1K
    SYMBOL res 928 176 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R7
    SYMATTR Value 1K
    SYMBOL res 928 432 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R10
    SYMATTR Value 1K
    SYMBOL voltage 1280 592 R0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V6
    SYMATTR Value 5
    SYMBOL cap 912 576 R0
    SYMATTR InstName C1
    SYMATTR Value 0.1µ
    TEXT -312 832 Left 2 !.tran 0 1 0 10e-6

     

     

    cstanton The tag and group thing seems to work OK once you get used to it !

    Thanks.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to michaelkellett

    Hi Michael,

     

    I think this is one of the more exciting projects I have seen in a while but I will be following rather than contributing to the analog part as it is over my head and I don't have the background.  Somewhere in the boxes from my recent move is a NUCLEO-L4R5ZI board and I need to get that going.  The FPGA is going to be a learning experience as well.  I appreciate greatly the work that you and Shabaz are putting into this.

     

    Frank

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to fmilburn

    Nice to hear from you, is your house moving all done now ?

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 6 years ago in reply to michaelkellett

    I think a lot of people are contemplating a build.

     

    Until you have the circuit connected to the sensors and see how it performs you are kind of at an impasse.

    It would be awesome if someone who uses this system did a side by side comparison of its capabilities.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to michaelkellett

    All my things are in the house and though it is the same size as the old house the layout is different with little built-in storage and I am finding my things don't fit well.  So unopened boxes are waiting for me to create storage and shelving.  And it hasn't been lived in for several months so I am also having to whack the garden back into shape.  It is a nice house in a great area though....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fmilburn
    fmilburn over 6 years ago in reply to michaelkellett

    All my things are in the house and though it is the same size as the old house the layout is different with little built-in storage and I am finding my things don't fit well.  So unopened boxes are waiting for me to create storage and shelving.  And it hasn't been lived in for several months so I am also having to whack the garden back into shape.  It is a nice house in a great area though....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kltm
    kltm over 6 years ago in reply to fmilburn

    All takes time Frank. I guess it’ll take a few months to sort. Good luck

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to fmilburn

    fmilburn Frank it never ends I moved about 1.5 years ago I have 40-50 boxes in the storage, plus my garage is getting full. Consider this, I have a DB one table, LOL where all my boxes are numbered as well as what room they came from and what's in them as well as the type of box.  GRON I still have stuff from my kitchen mia, and I can't find a DVM as well as my hot air solder station. LOL

    ~~Cris

    BTW i started with over 160 boxes.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to phoenixcomm

    I started putting in shelving today :-)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to fmilburn

    fmilburn Good luck, frank I'm still putting up shelving! Lots of Elfa top mounting rails, and standards. Rubbermaid etc (Home Depot) for the brackets (cheaper price). And sometimes I buy them from my Goodwill outlet store where it's only $1.50 a pound. image I also have some Metro wire shelves, and some HomeDeopt plastic shelves. In my garage, I put together a bunch blue of 2x4x6 used shelves with nuts and bolts ( image pain in the ass!) so have about 20 feet of that stuff. And I still need to put together a workbench down there as well. for a drill press and other things. Currently building a 12' long clothes rack, from 2x4s and two uprights from the blue shelves. Not quite a 3-foot base but all the way to the ceiling made like two right triangles. And its bolted together, with a cross brace near the top to rest the steel on. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to phoenixcomm

    phoenixcomm Yep, I'm started with some metal wire shelving that is quick to put up in the garage and then building some 2x4 made to fit next.  I almost spent more time opening boxes to find the necessary tools than putting up shelves.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to fmilburn

    fmilburn " I almost spent more time opening boxes to find the necessary tools than putting up shelves." sounds very familiar!

    • Cancel
    • Vote Up +3 Vote Down