• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56100 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • genebren
    genebren over 6 years ago

    Interesting ideas so far.  I meant to chime in earlier, but things have been pretty busy for me lately (building a deck and entertaining my Grandchildren again).

     

    Several years ago, I was asked to sit in with some friends of my sister that work at a geotech company.  They were looking to build impedance measurement devices for soil surveys.  I came across this amazing looking chip from Analog Devices that looked like a great way to measure impedance (including a complex component).

     

    Here is a snippet from the specification:

     

    The AD5934 is a high precision impedance converter system solution that combines an on-board frequency generator with a 12-bit, 250 kSPS, analog-to-digital converter (ADC). The frequency generator allows an external complex impedance to be excited with a known frequency. The response signal from the impedance is sampled by the on-board ADC and a discrete Fourier transform (DFT) is processed by an on-board DSP engine. The DFT algorithm returns a real (R) and imaginary (I) data-word at each output frequency.Once calibrated, the magnitude of the impedance and relative phase of the impedance at each frequency point along the sweep is easily calculated using the following two equations:Magnitude = 22IR+Phase = tan−1(I/R) A similar device, available from Analog Devices, Inc., is the AD5933, which is a 2.7 V to 5.5 V, 1 MSPS, 12-bit impedance converter, with an internal temperature sensor, available in a  16-lead SSOP.

     

     

    This might be of some help in your planning.

     

    Good luck and let me know if you need any help on this project.

     

     

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to genebren

    Hi Gene,

     

    It's a super-interesting chip, I was keen to use it a few years ago for plant soil purposes, and for hydroponics - to try to see if the soil or liquid has nutrients. The idea being to have a signature of known good soil or water by sweeping through the spectrum. I never got to try it though sadly, the project moved on to something else.

    It was felt that it could have had a lot of merit because then you could publish the signature, so others could try to replicate a yield (it wasn't going to be for farmers, more for home use), and to not waste nutrient. But, I have no idea in practice if the result would have been usable, or too inconsistent/variable.

    I wish I'd done some work on it at the time, since it could have been useful for other purposes too.

     

    The proposed design so far is one half of the impedance measuring system, but with digital processing. In theory it could be converted to an impedance measuring system with no additional hardware change, just a software upgrade, since the frequency will be know, and there will be some sync pulse from the FPGA, we just need to internally multiply with a 90 degree out of phase signal from that sync pulse too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • paul_d_arch
    paul_d_arch over 6 years ago in reply to shabaz

    Shabaz,

     

    I have changed your outline. In the UK two of the probes are 'fixed' and can be in the same position for the day (or longer)

     

    The QGIS team have vast experience to call on in displaying this type of data  Many groups in the UK use QGIS and some run training days in Python.

     

    You can have a table and power at P2C2 and use existing equipment (including a tea and coffee facilities - YES most groups have a tent that could be pitched close to the 'fixed' probes if needed) My editing of your original is very bad, sorry.

     

    When I said "What about a Pi" I meant "QGIS would be good. it runs on Laptops and a Pi"

     

    Paul D

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to paul_d_arch

    Hi Paul,

     

    I've updated it to incorporate your comments regarding the probes and software. One underlying difference (won't make a difference to the user apart from a major improvement hopefully!) is that the older existing designs use analog circuitry for most of the signal generation and processing. In this design however, more of that is done digitally, and so needs precise timing and regular fast calculations, which would be an overhead for the Pi, so all that underlying processing needs a microcontroller (and an FPGA), hence the separation between that and the Pi. The Pi has full control via USB Serial, which is a key difference to Snuffler. The Pi can instruct the desired frequency, start/stop measurements and acquire the data in real-time, i.e. the Pi is in full control using Python, C or any desired language. Also, the interface can still work with existing software in real-time (I've run Snuffler to examine what data is expects), so I've listed those in the diagram now.

    For those who want to use a laptop, they will find it equally seamless with Windows and existing software, it's just more convenient to use USB rather than have the older RS232 DB9 connector. Just like with the Pi, they can have full control using any programming language if desired.

    For those who want to use Android, initially there could be just a simple skeleton app which doesn't do much but provides some basic visuals, or just collects up the data to e-mail it.

     

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • paul_d_arch
    paul_d_arch over 6 years ago in reply to shabaz

    Shabaz,

     

    What software are you using to create your drawings? They are great.

     

    Paul D

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to paul_d_arch

    Hi Paul,

     

    Thanks! I'm using Powerpoint. I've used it a lot and so already had things like the Pi and display ready to use.

    For items like the phone graphic, I usually google search for (say) 'phone transparent png' and then it finds stuff with the transparent background.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to michaelkellett

    michaelkellett I do agree with you, but

    1. The Pi4 can support Debian (Linux)
    2. I disagree with Shabaz about using USB between PI and control head, As said before CAN bus is robust and you don't have to write the protocol.
    3. I disagree with Shabaz about  using WiFi ( sucks power)
    4. If you go with the Pi, then with a USB3 to SATA adapter (this is what my VOIP server is running on) and run a notebook drive, for the OS and Data The Pi can be set not to boot from the SD card if you wish.
    5. if you use a tablet, that's overkill + you would have to write an app.
    6. if you use a small control box (operator panel) you could put Arduino in it. The would drive the CAN bus communications,  4xx20 I2C display, and keyboard, plus and switches etc.
    7. So if you go with my suggestion you need two cables in the waterproof cover.
      1. (5 Volts and Ground)
      2. two-wire shielded twisted-pair (50-ohm stuff works fine.

    ~~ Cris

    .

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to phoenixcomm

    michaelkellett  and of course the PI would handle the GPS.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • paul_d_arch
    paul_d_arch over 6 years ago in reply to shabaz

    Oh, sometimes the oldies are the best!

     

    Paul D

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to phoenixcomm

    Hi Cris,

     

    The existing visualization/archeology software doesn't use CAN, it uses serial (either RS232 or USB serial, either will work with them). If CAN is used between Pi and the main unit could you approximately sketch or list what modules etc will do the translation to RS232, or will appear like /dev/ttySerial to the software? (and appear like a Serial interface to the PC too, otherwise people cannot use the existing Snuffler software, which only runs on Windows).

     

    Just to clarify although it says USB, really the underlying communication is traditional 9600 or 115200 etc baud serial, i.e. easily swapped to RS232 or any long distance, robust method. If anyone wants these methods, they would be very easy to convert, and no code changes are required because there's no USB protocol being coded, there is a UART-to-USB chip (which could be unsoldered and replaced with UART-to-RS232 or to any other desired method). If anyone knows what hardware to use for wiring CAN to Pi and write some code for it, then it can be easily wired in, because there's no USB from the microcontroller, it's two-wire UART Tx and Rx. That detail will appear on the block diagram that Ken is drafting.

    image

     

    I agree regarding WiFi, I don't see the need for those comfortable with the other methods, but it's an option for those who feel more comfortable programming for an ESP chip. It's just to accommodate them, so they can contribute too if they want to. I don't know how to use the ESP, and it is labelled as an option for anyone else (if they want to) to contribute.

    The tablet/phone is a low-priority option, it is enabled for zero additional hardware cost since it uses the same connection (USB Serial). Using it would give some free advantages (by free I mean no hardware cost, beyond owning a phone) such as the potential to grab positioning data, or sending data using cellular. For those more comfortable doing it with the Pi and GPS module, that's totally fine.

    I'm self-encouraged to write a simple mobile app if anyone sees an advantage in it. I did some brief testing last night to confirm for myself that I'm not over-promising by putting the tablet in the diagram and then subsequently discovering it is impossible. If no-one wishes it, that's fine, the time wasn't wasted because I can use that for a different project one day. It could be a really poor solution, for instance if the mobile battery dies etc. I don't know.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to shabaz

    shabaz  ok no matter what you do you will need 2 CPUs.

    • one controlling the probes, etc most likely a PI, I would also have the GPS module there as well, and a CAN Module for talking to the control panel.
    • the control panel could be an Arduino mega, 4x20 LED I2C display, a keyboard, and maybe some switches.

    Please refer to my Bolg Adventures In CANaerospace (the hardware is the same as CANbus).

    All you would do is take msgs off the CAN bus and put them on the display. You can also transmit messages the same way. easy peasy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    I thought it might be helpful to explain my reasoning for some of my suggestions.

     

    My concept was to end up with an instrument that can be made cheaply and be competitive with the commercial offerings in performance.

    It has to make good measurements and never lose data.

    That rather means that the data must be stored in simple on board media. My solution is a soldered in flash chip. With a little care you will never lose

    more than the pending reading, no matter how the processor is stopped. None of the big OSs can do this without great difficulty or special hardware,

    usually both.

    Having got the data safely stored it has to be transferred to a computer with a screen and suitable software (which all demands a big OS) - we have logic level UART,

    UART over USB, Bluetooth and possibly WiFi which covers a lot of bases. Almost everything has USB, the others add to the possibilities.

    We have a flexible SPI display interface which can support displays from 2 lines character up to 800 x 480 with touch screen.

    Several reviews of exsiting hardware comment on it being difficult to control  - my solution is to offer the option of two rotary encoder type controls with additional buttons.

    Menu based character display interfaces with a rotary control are not too bad to operate - gives quite a lot of bang for not many bucks.

     

    To be reliable implies a single board design - or as close as we can get.

    The processor is a low power ARM Cortex M4 which clocks at 120MHz - enough welly to cope with any forseeable data collection load but only needing about 50mA at 3.3V.

    In that package you get 640k of RAM, fast ADCs for overload monitoring, 3 hardware SPI ports  etc, several UARTS and other stuff.

    The only way you can get close to using all the resources in modern processors is have flexibility with pin allocation which only happens if you solder the chip to your own board.

     

    As I explained in an earlier post I'm expecting the instrument to controllable by a simple serial protocol which can be used internally between the human interface

    and the measuring core or by external devices. Such protocols must be easy to code to and debug, which implies human readability.  CAN does not easily lend itself to this

    because it is small packet (8 bytes max unless you use FD) based. Of course you can send text streams over CAN but it's messy. The strong features of CAN (non destructive

    arbitration and the abilty to exist with many equal status nodes) don't do us any good in this application since we only envisage exactly 2 nodes in the network.

    (For clarification, the "measuring core" is the hardware and code that does the actual measuring, hard real time control and safe data storage.)

     

    The processor does have a CAN port  - so it could be done.

     

    As far as I can tell from a quick scan of the web the ESP module will average about 150mA from 3.3V when WiFi is on and connected, maybe less.

    No problem at all for transferring a few Mbytes of data but less good for continuous operation.

    The output driver will use about 900mW max when actually measuring, call that 1W when psu losses are added in.

    The rest of the works will need about 500mW (very roughly, a pretty display would double that).

    The battery  will need to be capable of at least 15 W hrs, continuous WiFi would take that up to 20W hrs,  well within reasonable lithium ion range.

    Shabaz's mega camera battery is about 40W hrs.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    I thought it might be helpful to explain my reasoning for some of my suggestions.

     

    My concept was to end up with an instrument that can be made cheaply and be competitive with the commercial offerings in performance.

    It has to make good measurements and never lose data.

    That rather means that the data must be stored in simple on board media. My solution is a soldered in flash chip. With a little care you will never lose

    more than the pending reading, no matter how the processor is stopped. None of the big OSs can do this without great difficulty or special hardware,

    usually both.

    Having got the data safely stored it has to be transferred to a computer with a screen and suitable software (which all demands a big OS) - we have logic level UART,

    UART over USB, Bluetooth and possibly WiFi which covers a lot of bases. Almost everything has USB, the others add to the possibilities.

    We have a flexible SPI display interface which can support displays from 2 lines character up to 800 x 480 with touch screen.

    Several reviews of exsiting hardware comment on it being difficult to control  - my solution is to offer the option of two rotary encoder type controls with additional buttons.

    Menu based character display interfaces with a rotary control are not too bad to operate - gives quite a lot of bang for not many bucks.

     

    To be reliable implies a single board design - or as close as we can get.

    The processor is a low power ARM Cortex M4 which clocks at 120MHz - enough welly to cope with any forseeable data collection load but only needing about 50mA at 3.3V.

    In that package you get 640k of RAM, fast ADCs for overload monitoring, 3 hardware SPI ports  etc, several UARTS and other stuff.

    The only way you can get close to using all the resources in modern processors is have flexibility with pin allocation which only happens if you solder the chip to your own board.

     

    As I explained in an earlier post I'm expecting the instrument to controllable by a simple serial protocol which can be used internally between the human interface

    and the measuring core or by external devices. Such protocols must be easy to code to and debug, which implies human readability.  CAN does not easily lend itself to this

    because it is small packet (8 bytes max unless you use FD) based. Of course you can send text streams over CAN but it's messy. The strong features of CAN (non destructive

    arbitration and the abilty to exist with many equal status nodes) don't do us any good in this application since we only envisage exactly 2 nodes in the network.

    (For clarification, the "measuring core" is the hardware and code that does the actual measuring, hard real time control and safe data storage.)

     

    The processor does have a CAN port  - so it could be done.

     

    As far as I can tell from a quick scan of the web the ESP module will average about 150mA from 3.3V when WiFi is on and connected, maybe less.

    No problem at all for transferring a few Mbytes of data but less good for continuous operation.

    The output driver will use about 900mW max when actually measuring, call that 1W when psu losses are added in.

    The rest of the works will need about 500mW (very roughly, a pretty display would double that).

    The battery  will need to be capable of at least 15 W hrs, continuous WiFi would take that up to 20W hrs,  well within reasonable lithium ion range.

    Shabaz's mega camera battery is about 40W hrs.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down