Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Audio Amplifier questions
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 328 subscribers
  • Views 1867 views
  • Users 0 members are here
Related

Audio Amplifier questions

e14 Contributor
e14 Contributor over 11 years ago

Hello everybody!

 

I am trying to make an audio amp, but I don't know which IC to use. This is problem number one.

I would liek to do something like what Ben Does with his xbox 360 laptop audio amp, which he uses buttons

to amplify the audio.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here, on the 1.35 video mark you can see that. He does not mention what is the second IC, and the

first one I can't find here in my country, any alternatives to that?

 

Also now, problem 2! I need a way to, when connecting headphones to it, it would cut the speakers sound. is that possible using only

hardware, headphone jacks only?

 

Thank you in advance everyone!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    @Enrico Miglino Thanks for the answer! I will order some new audio jacks, since in my city I can't find anything other than mono ones -.- dmaruska I didn't know about digital potentiometers, sorry for…
Parents
  • balearicdynamics
    balearicdynamics over 11 years ago

    Hey Lucy, I can answer only to the second question. What you ask in point two has a clear answer: YES image

     

    As you already say plugging the earphones in the micro jack there are some contacts that switches and only is just the signal. You can get just this signal, for example pulling it to low, nothing to do with the audio Left + Right + audio gnd and use this as a common input pin to switch automatically the speakers or the earphones.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 11 years ago

    Hey Lucy, I can answer only to the second question. What you ask in point two has a clear answer: YES image

     

    As you already say plugging the earphones in the micro jack there are some contacts that switches and only is just the signal. You can get just this signal, for example pulling it to low, nothing to do with the audio Left + Right + audio gnd and use this as a common input pin to switch automatically the speakers or the earphones.

     

    Enrico